Ultra Low Power Microcontroller Module Opens New Doors for Engineers - Part 2: Configuring Eclipse

Apr 24 2025

Read other articles in this series.

Figure 1

   

Abstract

This article continues the introduction of an ultra low power, feature rich microcontroller module and explains how to program and debug it using popular, free of charge tools. Unlike many other high end microcontroller modules, this one is available in a DIP footprint, allowing easy prototyping for professional engineers and hobbyists alike. While Part 1 describes how to create a project in Eclipse, Part 2 describes how to configure Eclipse to work with the PICO.

Reconfiguring Eclipse to Work with the PICO Hardware

The project created in Part 1was designed around the MAX32625EVKIThardware, which is different from the PICO hardware, so the file describing the hardware on the EV kit needs to be changed to reflect the hardware on the PICO. The original boards.c file is stored in:

C:\Maxim\Firmware\MAX32625\Libraries\Boards\EvKit_V1\ Source

and the new boards.c file for the PICO is stored in the zip file, which can be downloaded using the link at the end of this article. Copy the whole Boards

Authentication Required
Please fill in the form to download
809.13 K
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Resources


Software Development Kit
Secure Software Download