Calibration Implementation Techniques for Multichannel Phased Array Subsystems

Figure 1

   

Key Takeaways

  • A self-contained cross-correlation calibration method delivers ~23dB transmit combining gain and 12dB SNR improvement for a 16-channel X-band phased array—no external test equipment required.
  • Two calibration techniques, one critical tradeoff: discover how null power sweeping and cross-correlation compare for building phase correction tables across temperature and frequency in multichannel phased arrays.

Abstract

This article describes the practical implementation and comparative evaluation of two phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front end. A passive calibration board enables a fully self-contained transmit-to-receive loopback, allowing deterministic extraction of per-channel phase offsets without external instrumentation. The first technique, a null power approach, determines relative phase alignment through swept phase measurements and provides a noise-tolerant baseline solution. The second technique uses time-interleaved pulsed waveforms and cross-correlation processing to rapidly estimate transmit and receive phase errors with high precision. Experimental results show that the correlation-based method achieves near-theoretical coherent combining performance, producing approximately 23dB transmit combining gain and an additional 12dB improvement in signal-to-noise ratio when both transmit and receive channels are coherently summed. These results demonstrate a scalable and efficient calibration framework suitable for high channel count digital beamforming subsystems.

Introduction

Accurate amplitude and phase calibration is essential to achieving the theoretical performance of phased array antenna systems. Proper calibration applies the correct phase and amplitude weighting to each antenna element. This ensures that desired signals combine constructively (coherently) while noise, being uncorrelated between elements, combines less efficiently (noncoherently). The result is improved signal-to-noise ratio (SNR) and consistent antenna pattern performance across varying frequencies, temperatures, and operating conditions.

This article focuses specifically on two phase-alignment techniques used for the evaluation and characterization of the ADXBAND16EBZ reference design. Continuous-wave (CW) waveforms were employed for the analysis, leveraging the hardened digital signal processing (DSP) blocks of the AD9084. The system also utilizes prerequisite multichip synchronization to ensure phase determinism; however, the details of this synchronization process are outside the scope of this article.

Two Techniques Explained

Calibration on the subsystem platform is essential for ensuring that all 16 transmit and receive channels operate coherently. When the channels align in time, phase, and amplitude, the system achieves the expected coherent combining gain of approximately 24dB (20 × log10(16)). Two distinct calibration approaches are considered: the null power method and the cross-correlation method. The first is a traditional approach that excels in robustness, while the second is a modern, quicker alternative leveraged as the primary method for characterization. In both cases, a passive calibration board consisting of a power combiner/splitter and switch network is leveraged to enable a self-contained transmit-to-receive loopback (Figure 1). The following sections describe both methods in a detailed, engineering accurate manner and explain how the system extracts the final transmit and receive phase offsets.

ADXBAND16EBZ Connection Loopback Block Diagram Fig 01
Figure 1. (a) ADXBAND16EBZ and ADXBAND16EBZ-CAL connection and (b) combined loop back block diagram.

Null Power Calibration

The null power method is based on rotating the phase of one channel relative to a reference with fixed phase and observing the superposition magnitude of the two combined channels. The peak magnitude is recorded for each phase step and 180° is added to the phase offset corresponding to the two-channel combined minimum (null) as shown in Figure 2. The phase offset is then applied to the numerically controlled oscillator’s (NCO’s) phase shifter of the corresponding channel so that the channel aligns constructively with respect to the selected reference channel. This entire procedure must be repeated for each channel and for each frequency of interest.

Magnitude Response Null Power Method Phase Comparison Fig 02
Figure 2. Magnitude response for null power method comparing phase contributions of two combined channels.

 

Although this approach requires significant time due to its swept nature, it is extremely robust in noisy or unpredictable environments. It leverages a sinusoidal waveform and does not rely on timing alignment or correlation-based measurements. The main drawbacks are the execution time and the limited information it provides since it yields only phase offset information. Additional optimization can be implemented for quicker sweeps using this method. Instead of a fixed phase step, one could start with a coarse step size to find a general range for the null location and use a finer phase step size to dial in the exact offset for the corresponding null.

Cross-Correlation Calibration

The cross-correlation method is the standard calibration procedure leveraged because it aligns phase rapidly and with high precision. The method begins by configuring the calibration board into either combined loopback mode. All transmit and receive NCO phases, including both main and per channel adjustments, are set to zero so that any measured phase error originates solely from the hardware signal chain.

A pulsed baseband waveform is then generated with one pulse assigned to each digital-to-analog converter (DAC) channel in a time division fashion akin to time-division multiple access (TDMA). These pulses are placed in discrete time slots in a time interleaved fashion to produce a frame containing 16 non-overlapping pulses once all channels are combined. This waveform is transmitted at the operating RF frequency and serves as the reference for the correlation-based alignment.

DAC Waveforms Time Interleaved Pulsed Output Fig 03
Figure 3. All DAC waveforms combined to create time interleaved pulsed waveform. Each pulse train corresponds to an independent transmit channel.
 

The pulse corresponding to TX_CH<0> has a seven sequence Barker code, where each sinusoidal period within the pulse envelope of TX_CH<0> has a unique sequence of phase shifts. This helps distinguish the reference channel compared to the other channels by a higher SNR signature in the correlation response. Channels 1 to 15 all have a five sequence Barker code with its own unique phase shift sequence. A comparison of TX_CH<0> and TX_CH<1> can be observed in Figure 4.

TX Ch0 Ch1 Barker Code Pulse Sequences Fig 04
Figure 4. TX_CH<0> (Pulse0) with a seven sequence Barker code and TX_ CH<1> (Pulse1) with a five sequence Barker code.
 

The calibration process starts by each DAC transmitting its respective time interleaved pulsed waveform and all analog-to-digital converters (ADCs) capturing the 10 data frames of the combined waveform. Each data capture for all 16 ADCs is taken at an arbitrary time resulting in each data frame shifted by an unknown sample count relative to the others. Sample misalignment correction is done by selecting an arbitrary data frame as a reference and executing an autocorrelation against all remaining data frames. Each capture is then sample shifted by the appropriate number of samples to achieve alignment based on the autocorrelation sample delay results. Once aligned, the data frames are coherently summed, thus improving the SNR for accurate post-processing as shown in Figure 5.

Coherent ADC Captures Time Interleaved DAC Waveform Fig 05
Figure 5. Coherently summed ADC captures of the combined time interleaved waveform synthesized by all DACs. 2× the samples captured compared to transmitted.
 

The next step cross correlates the coherently summed data and the original transmitted time interleaved pulse train waveform. The resulting cross correlation matrix will aid in determining the phase offsets relative to a defined reference for all ADCs and DACs. The reference channels TX_CH<0> help identify its location in the time interleaved pulses and can be used to determine the relative phase offsets of the remaining channels. The relative difference of the complex angle of the peak correlation response for TX_CH<0> across the 16 ADC data frames will determine the ADC NCO phase offsets. The relative difference of the complex angle of the peak correlations of TX_CH<15…1> compared to TX_CH<0> within a single ADC data frame will determine the DAC NCO phase offsets. In both cases, the phase offsets are phase wrapped into the range from −180° to +180° to be compliant with the AD9084 device drivers.

Final Calibration Results

After calibration is completed and the derived phase offsets are applied, the next step is to validate the effectiveness of the phase alignment procedure. For a fully coherent 16 element array, the signal power is expected to increase by 20log10(16), while uncorrelated noise power increases by 10log10(16). Figure 6a shows the magnitude of a single transmit CW waveform digitized by one ADC channel, along with the FFT of the complex valued data frame. Figure 6b illustrates the result when all 16 transmit CW waveforms are combined and the peak magnitude is measured from the FFT of a single ADC frame; as expected, the coherent combination yields an approximately 23 dB increase in peak signal magnitude relative to Figure 6a. Finally, Figure 6c presents the FFT obtained when all 16 transmit waveforms and all 16 receive channels are coherently summed. In this case, the peak magnitude reaches the average expected level due to bit growth effects, while the uncorrelated noise combines noncoherently, resulting in an SNR improvement of approximately 12dB.

FFT Plots Single Vs Combined Tx Rx Channels Fig 06
Figure 6. (a) An FFT plot of a single transmit channel looped back into a single receiver, (b) an FFT plot of 16 combined transmit channels combined and looped back into single receiver, and (c) an FFT plot of 16 combined transmit channels and 16 combined receive channels.

Conclusion

This work demonstrates two practical calibration strategies for achieving coherent phase alignment in a 16 by 16 multichannel phased array subsystem. The null power method, while time intensive, offers a highly robust means of determining interchannel phase offsets without reliance on precise timing or correlation metrics, making it well suited for environments with elevated noise or measurement uncertainty. In contrast, the cross-correlation method provides a rapid and highly accurate calibration approach by exploiting time interleaved pulsed waveforms, Barker coded channel identification, and coherent summation of multiple captures to improve SNR and estimation stability.

Measured results confirm that the correlation-based calibration achieves near theoretical coherent combining performance, with signal power scaling as expected for a fully aligned 16 element array and noise combining noncoherently across receive channels. The ability to efficiently perform calibration across multiple frequencies enables the generation of high-resolution phase correction tables suitable for temperature and frequency dependent system characterization.

While the current implementation focuses on narrow-band CW excitation, the methodology naturally extends to wideband calibration by leveraging the integrated finite impulse response filtering and digital signal processing capabilities of the AD9084. Future work will explore broadband excitation and frequency dependent calibration to further enhance instantaneous bandwidth performance in large-scale digital beamforming systems.

References

  1. Siddhartha Das. “Quad-Apollo MxFE: A 16 Receive/16 Transmit X-Band Direct Sampling Digital Beamforming Subsystem Reference Design.” Analog Devices, Inc., January 2026.
  2. Michael Jones, Travis Collins, and Charles Frick. “Integrated Hardened DSP on DAC/ADC ICs Improves Wideband Multichannel Systems.” Analog Devices, Inc., May 2021.

About the Authors

Siddhartha Das
Siddhartha Das is a systems applications engineer on the Subsystems and Sensors Team within Analog Devices’ Aerospace, Defense, and Communications Business Unit based in Durham, North Carolina. He earned his B.S. in
Sam Ringwood
Sam Ringwood is a system platforms applications engineer for the Aerospace and Defense Business Unit located in Greensboro, North Carolina. Prior to joining Analog Devices, Sam worked in RF test and RF design roles within
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Technology Solutions
Product Categories