Tiny, Resistor-Programmable, μPower 0.4V to 18V Voltage Reference

Figure 1

   

Introduction

The LT6650 is a 0.4V to 18V adjustable voltage reference that runs from low voltage and consumes only a few microamps. It features a low-dropout (LDO) characteristic, can source or sink current, can be configured in either series or shunt mode and saves space in the tiny 5-lead ThinSOT-23 package.

Figure 1 shows a block diagram of the reference. Its 400mV internal voltage reference is connected to the non-inverting input of an operational amplifier. The inverting input is brought to a pin, thus making a series-mode reference adjustable to any output voltage from 400mV up to (VSUPPLY – 0.35V) by using two external resistors. It can also be configured as a fixed 400mV reference by simply connecting the output to the op amp inverting input. While the LT6650 is designed as a series reference, it can be used as a shunt-mode reference simply by shorting the positive rail to the output pin—it can be programmed to produce any precision “zener” voltage within the wide supply range (1.4V to 18V) by selection of the two external resistors.

Figure 1. Block diagram of 1% accurate micropower 0.4V to 18V adjustable reference.

Specifications

Table 1 summarizes the performance of the LT6650. The supply current is only 5.6μA and the supply voltage may range from 1.4V to 18V, which permits battery-powered equipment to be plugged into an unregulated wall adapter without the need for peripheral circuitry to limit the voltage input to the reference. The 400mV internal reference is ±1% accurate over the –40°C to 85°C temperature range and is also fully specified from –40°C to 125°C for extended temperature range applications. The rail-to-rail output delivers 200μA in both sourcing and sinking modes of operation.

Table 1. LT6650 Performance (Ta = 25°C, VIN = 5V, VOUT = 400mV, CL = 1μF, unless otherwise noted)
Parameter Conditions Min Typ Max Units
Input Voltage Range –40ºC ≤ TA ≤ 125°C 1.4 18 V
Output Voltage –40ºC ≤ TA ≤ 85°C 396
–1
400 404
1
mV
%
Line Regulation 1.4 ≤ VIN ≤ 18V 1 6 mV
Load Regulation 0 to –200μA (Sourcing)
0 to 200μA (Sinking)
–0.04
0.24
–0.2
1
mV
mV
Output Voltage Temperature Coefficient 12 μV/°C
Dropout Voltage VOUT = 1.4V
IOUT = 0μA
IOUT = 200μA sourcing
75 100
250
mV
mV
Supply Current 1.4V ≤ VIN ≤ 18V 5.6 12 μA
FB Pin Input Current VFB shorted to VOUT 1.2 10 nA
Turn-On Time 0.5 ms
Output Voltage Noise 0.1Hz to 10Hz 20 μVP–P
Thermal Hysteresis –40°C to 85°C 100 μV

How it Works Inside

Figure 2 shows the simplified schematic of the reference. Transistors Q1–Q7 form the band-gap-derived 400mV reference that is fed to the non-inverting input of the error amplifier formed by Q8–Q12. The resistors R1–R3 set the correct current flow into the internal reference, while R4 provides for post-package trimming capability. Transistors Q20 and Q21 form the rail-to-rail output stage and are driven by Q13–Q19. Resistors R5–R8 and the I2 current generator establish the gain and quiescent operating current of the output stage. In conjunction with the minimum recommended output capacitance of 1μF, stabilization is assured through Miller compensation inside error amplifier Q8–Q12. Pins are ESD protected by diodes D1–D3.

Figure 2. LT6650 simplified schematic showing detail of low-dropout topology.

Applications

Battery Powered Pocket Reference

The unique pocket reference shown in Figure 3 can operate for years on a pair of AAA alkaline cells or a single Lithium coin-cell, as the circuit draws just 10μA supply current. An input capacitor of 1μF as shown should be used when the LT6650 is operated from small batteries or other sources with impedance over about 50Ω. The output is adjustable from 0.4V up to the battery supply by selecting two feedback resistors (or setting a trimmer potentiometer position) to configure the non-inverting gain of the internal operational amplifier. A feedback resistor RF is connected between the OUT pin and the FB pin and a gain resistor RG is connected from the FB pin to GND. The resistor values are related to the output voltage by the following relationship:

Equation 1

Figure 3. Battery powered pocket voltage reference runs for years on a coin cell.

The worst-case FB pin bias current (IBIAS) can be neglected with an RG of 100kΩ or less. In ultra-low-power applications where current in the voltage programming resistors might be reduced to where the 1.2nA typical IBIAS becomes relatively significant loading, the relationship between the resistors then becomes:

Equation 2

The minimum allowable gain resistor value is 2kΩ established by the 400mV FB pin voltage divided by the maximum guaranteed 200μA output current sourcing capability. In applications that scale the reference voltage, intrinsic noise is amplified along with the DC level. To minimize noise amplification, a 1nF feedback capacitor (CN) as shown in Figure 3 is recommended. Any net load capacitance of 1μF or higher assures amplifier stability.

Automotive Reference

In the presence of high supply noise, such as in automotive applications or DC-DC converters, an RC filter can be used on the VIN input as shown in Figure 4. Due to the exceptionally low supply current of the LT6650, the input resistor (RIN) of this filter can be 1kΩ or higher, depending on the difference in VIN and VOUT. Figure 5 shows supply rejection better than 30dB over a wide frequency spectrum, for a minimum sourcing output current of 40μA and an input filter comprising RIN = 1kΩ and CIN = 1μF. If even higher rejection is necessary, the input filter structure presented in Figure 6 effectively eliminates any supply transients from affecting the output by the inclusion of a pre-regulating Zener diode. With this extra input decoupling and the LT6650 circuitry operating from a 12V bus, 50V transients induce less than 0.5% VOUT perturbation.

Figure 4. Simple input network for improved supply rejection.

Figure 5. Improved supply noise rejection of Figure 4 reference circuit.

Figure 6. High noise-immunity input network allows 50V transients on automotive power bus.

To obtain the micropower performance of the LT6650, quiescent currents of the internal circuitry are minute, which by nature, results in a higher output impedance than traditional references. Since output impedance is inversely related to the output stage operating current, a modest additional load current can easily reduce the output impedance by an order of magnitude from the unloaded case. Thus in applications where the output impedance and noise must be minimized, a light DC loading of the output provides enhanced performance. This loading can exist naturally in the application, or the feedback resistors can be designed to provide it. For example, setting the gain resistor value to 10kΩ establishes a moderate IOUT = –40μA and decreases the output peak resistance value from hundreds of ohms to the tens of ohms shown in Figure 7.

Figure 7. Output impedance is reduced while sourcing moderate current (40μA).

Shunt-Mode Reference

When the output voltage is tied to the input voltage, the high side of the rail-to-rail buffer amplifier is effectively disabled and only the low side remains active. In this mode of operation the LT6650 operates as a shunt reference as shown in Figure 8. Any shunt reference voltage from ±1.4V up to ±18V can be established by the feedback resistor selection. The noise and load capacitors have the same functions as in the series mode of operation. A 10μF minimum load capacitance is recommended for best stability and transient response. In shunt mode, an external biasing resistor RB is connected from the power supply to the output, and delivers all the current required for supplying the LT6650 and the load current. RB is selected to ensure the operating current of the reference (IZ in the Figure 8 zener-diode analogy) is in the range of 30μA to 220μA under all loading conditions.

Figure 8. Create you own adjustable micropower “zener” 2-terminal reference.

Conclusion

The LT6650 voltage reference incorporates a unique blend of low voltage, micropower operation and functional versatility. With the additional features of series and shunt mode configurability, source and sink output current, wide output voltage range, adjustability, and a tiny ThinSOT-23 package, the LT6650 provides an excellent solution to the many design challenges in both portable and industrial voltage control.

About the Authors

Dan Serbanescu
Jon Munson
Jon Munson is a senior applications engineer for Analog Devices, supporting their Signal Conditioning product line. Jon has a BS in electrical engineering and computer science from Santa Clara University. He has designed h...
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project