AD4696: 8 or 16 Channel Multiplexed SAR ADCs

Aug 29 2022

AD4696 family is the optimal solution, if you’re working on the next generation of wearables, medical instruments, optical communications modules, or high-density voltage and current monitors and have strict requirements on solution size and power consumption.

AD4696: 8 or 16 Channel Multiplexed SAR ADCs

Aug 29 2022

AD4696 family is the optimal solution, if you’re working on the next generation of wearables, medical instruments, optical communications modules, or high-density voltage and current monitors and have strict requirements on solution size and power consumption.

Latest Media 11
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project