Totem Pole

What is a Totem Pole?

Definition

A totem pole is a standard CMOS output structure where a P-channel MOSFET is connected in series with an N-Channel MOSFET and the connection point between the two is the output.

The P-FET sits on top of the N-FET like a "totem pole." Both gates are driven by the same signal. When the signal is low, the P-FET is on; when the signal is high, the N-FET is on. This creates a push-pull output using just two transistors.

Find a term alphabetically: