LCC
What is a LCC?
Definition
1. Leadless Ceramic Chip Carrier or Leadless Chip Carrier: An IC package, usually ceramic, that has no leads (pins). It instead uses metal pads at its outer edge to make contact with the printed circuit board. Example: Analog 20-pin LCC diagram (PDF)
2. Leaded Chip Carrier, also called PLCC or Plastic Leaded Chip Carrier: A square surface mount chip package in plastic with leads (pins) on all four sides. Example: Analog 20-pin PLCC diagram (PDF)
Synonyms
Leaded Chip CarrierFind a term alphabetically: