AN-2616: Face Identification Using the MAX78000/MAX78002
Abstract
This application note describes a method to execute the facial recognition application for the MAX78000/MAX78002 artificial intelligence (AI) microcontrollers. This application is comprised of three separate models— the Face Detection CNN model, the Face Identification CNN model, and the Dot Product model.
Introduction
The MAX78000 [1] and MAX78002 [2] are AI microcontrollers that include an ultra-low-power convolutional neural network (CNN) inference engine to run AI edge applications on a battery-powered internet of things (IoT) device. The microcontrollers can execute many complex CNN networks to achieve critical performance.
This document describes an approach to use a single facial recognition application to utilize the following three CNN models, each invoked in a different task:
- The Face Detection CNN model detects faces in the captured image and extracts a rectangular sub-image containing only one face.
- The Face Identification CNN model identifies a person from their facial images by generating the embedding for a given face image.
- The Dot Product model outputs the dot product representing the similarity between the embedding from the given image and embeddings in the database.
Using the dot product similarity as a distance metric, the image is identified as either one of the known subjects or ‘Unknown’ depending on the embedding distances.
MAX78000 Facial Recognition Application
The Facial Recognition application [4] can only run on MAX78000 Feather Board [3] because of the SD card support.
The Face Detection, Face Identification, and Dot Product models are executed sequentially.
The challenge of this application is to utilize all models when they are exceeding 432KB of 8-bit weight capacity of the MAX78000 CNN engine and MAX78000 internal flash memory storage. In this example, the Face Detection and Dot Product model’s weights are stored in the MAX78000 internal flash memory, while the Face Identification CNN model weights are stored in the external SD memory card and reloaded as soon as a face is detected.
The SDHC_weights sub-project can be used to store the Face Identification CNN weights (weights_2.h) in the SD card in binary format.
Face Detection
The Face Detection CNN model has 16 layers and uses 168x224 RGB images as input.
Face Detection CNN:
SUMMARY OF OPS
Hardware: 589,595,888 ops (588,006,720 macc; 1,589,168 comp; 0 add; 0 mul; 0 bitwise)
Layer 0: 4,327,680 ops (4,064,256 macc; 263,424 comp; 0 add; 0 mul; 0 bitwise)
Layer 1: 11,063,808 ops (10,838,016 macc; 225,792 comp; 0 add; 0 mul; 0 bitwise)
Layer 2: 43,502,592 ops (43,352,064 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 3: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 4: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 5: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 6: 173,709,312 ops (173,408,256 macc; 301,056 comp; 0 add; 0 mul; 0 bitwise)
Layer 7 (backbone_conv8): 86,779,392 ops (86,704,128 macc; 75,264 comp; 0 add; 0 mul; 0 bitwise)
Layer 8 (backbone_conv9): 5,513,088 ops (5,419,008 macc; 94,080 comp; 0 add; 0 mul; 0 bitwise)
Layer 9 (backbone_conv10): 1,312,640 ops (1,290,240 macc; 22,400 comp; 0 add; 0 mul; 0 bitwise)
Layer 10 (conv12_1): 647,360 ops (645,120 macc; 2,240 comp; 0 add; 0 mul; 0 bitwise)
Layer 11 (conv12_2): 83,440 ops (80,640 macc; 2,800 comp; 0 add; 0 mul; 0 bitwise)
Layer 12: 1,354,752 ops (1,354,752 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 13: 40,320 ops (40,320 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 14: 677,376 ops (677,376 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 15: 20,160 ops (20,160 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 275,184 bytes out of 442,368 bytes total (62%)
Bias memory: 536 bytes out of 2,048 bytes total (26%)
The corresponding CNN weights, bias, and configuration are loaded into the CNN engine every time before execution.
// Power off CNN after unloading result to clear all CNN registers
// It is needed to load and run other CNN models
cnn_disable();
// Enable CNN peripheral, enable CNN interrupt, turn on CNN clock
// CNN clock: 50MHz div 1
cnn_enable(MXC_S_GCR_PCLKDIV_CNNCLKSEL_PCLK, MXC_S_GCR_PCLKDIV_CNNCLKDIV_DIV1);
/* Configure CNN_1 to detect a face */
cnn_1_init(); // Bring CNN state machine into consistent state
cnn_1_load_weights(); // Load CNN kernels
cnn_1_load_bias(); // Load CNN bias
cnn_1_configure(); // Configure CNN state machine
The output of the Face Detection CNN model is a set of box coordinates and corresponding scores. The nonmaximum suppression (NMS) algorithm selects a bounding box with the highest confidence score, which is displayed on the TFT.
If the Face Detection CNN model detects a face, a rectangular sub-image containing only one face is resized to a 112x112 RGB image to match the Face Identification CNN model input.
Face Identification
The Face Identification CNN model consists of 17 layers with a 112x112 RGB input.
Face Identification CNN:
SUMMARY OF OPS
Hardware: 199,784,640 ops (198,019,072 macc; 1,746,752 comp; 18,816 add; 0 mul; 0 bitwise)
Layer 0: 11,239,424 ops (10,838,016 macc; 401,408 comp; 0 add; 0 mul; 0 bitwise)
Layer 1: 29,403,136 ops (28,901,376 macc; 501,760 comp; 0 add; 0 mul; 0 bitwise)
Layer 2: 58,003,456 ops (57,802,752 macc; 200,704 comp; 0 add; 0 mul; 0 bitwise)
Layer 3: 21,876,736 ops (21,676,032 macc; 200,704 comp; 0 add; 0 mul; 0 bitwise)
Layer 4: 7,375,872 ops (7,225,344 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 5: 21,826,560 ops (21,676,032 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 6: 1,630,720 ops (1,605,632 macc; 25,088 comp; 0 add; 0 mul; 0 bitwise)
Layer 7: 14,450,688 ops (14,450,688 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 8: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 9: 12,544 ops (0 macc; 0 comp; 12,544 add; 0 mul; 0 bitwise)
Layer 10: 3,261,440 ops (3,211,264 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 11: 10,888,192 ops (10,838,016 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 12: 912,576 ops (903,168 macc; 9,408 comp; 0 add; 0 mul; 0 bitwise)
Layer 13: 10,838,016 ops (10,838,016 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 14: 809,088 ops (802,816 macc; 6,272 comp; 0 add; 0 mul; 0 bitwise)
Layer 15: 7,225,344 ops (7,225,344 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 16: 22,656 ops (16,384 macc; 0 comp; 6,272 add; 0 mul; 0 bitwise)
Layer 17: 8,192 ops (8,192 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 365,408 bytes out of 442,368 bytes total (82.6%)
Bias memory: 1,296 bytes out of 2,048 bytes total (63.3%)
Before loading the Face Identification CNN configuration, weights, and bias, the CNN engine state machine and memory must be cleared from the previous CNN model execution. One way to do that is by powering down the CNN engine by calling the cnn_disable() function.
// Power off CNN after unloading result to clear all CNN registers
// It is needed to load and run other CNN models
cnn_disable();
// Enable CNN peripheral, enable CNN interrupt, and turn on CNN clock
// CNN clock: 50MHz div 1
cnn_enable(MXC_S_GCR_PCLKDIV_CNNCLKSEL_PCLK, MXC_S_GCR_PCLKDIV_CNNCLKDIV_DIV1);
/* Configure CNN_2 to recognize a face */
cnn_2_init(); // Bring CNN state machine into consistent state
cnn_2_load_weights_from_SD(); // Load CNN kernels from SD card
cnn_2_load_bias(); // Reload CNN bias
cnn_2_configure(); // Configure CNN state machine
The output of the Face Identification CNN model is an embedding vector of length 64 corresponding to the face image. Before feeding the embedding vector to the Dot Product model as an input, the vector is L2 normalized.
Dot Product
The Dot Product model has one linear layer and uses the embedding vector of length 64 as input.
Dot Product CNN:
SUMMARY OF OPS
Hardware: 65,536 ops (65,536 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 0: 65,536 ops (65,536 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 65,536 bytes out of 442,368 bytes total (14.8%)
Bias memory: 0 bytes out of 2,048 bytes total (0.0%)
Again, before loading Dot Product CNN configuration, weights, and bias, the CNN engine state machine and memory must be cleared.
// Power off CNN after unloading result to clear all CNN registers
// It is needed to load and run other CNN models
cnn_disable();
// Enable CNN peripheral, enable CNN interrupt, turn on CNN clock
// CNN clock: 50MHz div 1
cnn_enable(MXC_S_GCR_PCLKDIV_CNNCLKSEL_PCLK, MXC_S_GCR_PCLKDIV_CNNCLKDIV_DIV1);
/* Configure CNN_3 for dot product */
cnn_3_init(); // Bring CNN state machine into consistent state
cnn_3_load_weights(); // Load CNN kernels
cnn_3_load_bias(); // Reload CNN bias
cnn_3_configure(); // Configure CNN state machine
The output of the Dot Product model is 1024 dot product similarities, where each one represents the similarity between the given face and the faces recorded in the database. If the maximum of dot product similarities is higher than the threshold, the subject with the maximum similarity is declared as the identified face and displayed on the TFT. Otherwise, the output will be ‘Unknown’.
MAX78002 Facial Recognition Application
The Facial Recognition application [5] runs on the MAX78002 evaluation (EV) kit board [6].
Similar to the MAX78000 application, the Face Detection, Face Identification, and Dot Product models are executed sequentially. However, the MAX78002 features a larger internal flash memory that can store all of the model’s weights.
This application loads all weights and layer configurations only at the initialization and, with every inference, only biases are reloaded. With this approach, the overhead of switching between models is greatly reduced.
To keep all models together in the CNN memory, layer offsets must be arranged in a similar way so that models follow each other. In this example, layer offsets are arranged as shown in Table 1.
| CNN Model | Start Layer | End Layer |
| Face Identification | 0 | 72 |
| Dot Product | 73 | 73 |
| Face Detection | 74 | 89 |
To utilize this technique, the total layer count should not exceed a maximum of 128, which is the limitation of the MAX78002.
During the synthesis, for the models that are not starting from layer 0, passthrough layers must be added before the model layers in the network.yaml files. An example of network.yaml files can be found in the AI8x-Synthesis Repository [7].
Another consideration for this application is adjusting weight offsets. There are 64 parallel processors in the MAX78002, and each one has 4096 CNN kernels that can keep 9 parameters with 8-bit precision. While adjusting weight offsets, the previous model’s kernel memory usage should be considered.
In this example, weight offsets are arranged as shown in Table 2.
| CNN Model | Weight Offset | Number of Kernels |
| Face Identification | 0 | 1580 |
| Dot Product | 2000 | 114 |
| Face Detection | 2500 |
During the synthesis, “–start-layer” and “–weight-start” arguments can be used to add passthrough layers and weight offsets. Examples of synthesis scripts are provided in the AI8x-Synthesis Repository [7].
At the initialization, all model weights and configurations are loaded.
cnn_1_enable(MXC_S_GCR_PCLKDIV_CNNCLKSEL_IPLL, MXC_S_GCR_PCLKDIV_CNNCLKDIV_DIV4);
cnn_1_init(); // Bring CNN state machine into consistent state
cnn_1_load_weights(); // Load kernels of CNN_1
cnn_1_configure(); // Configure CNN_1 layers
cnn_2_load_weights(); // Load kernels of CNN_2
cnn_2_configure(); // Configure CNN_2 layers
cnn_3_load_weights(); // Load kernels of CNN_3
cnn_3_configure(); // Configure CNN_3 layers
Face Detection
The Face Detection CNN model has 16 layers and uses 168x224 RGB images as input.
Face Detection CNN: SUMMARY OF OPS Hardware: 589,595,888 ops (588,006,720 macc; 1,589,168 comp; 0 add; 0 mul; 0 bitwise)
Layer 74: 4,327,680 ops (4,064,256 macc; 263,424 comp; 0 add; 0 mul; 0 bitwise)
Layer 75: 11,063,808 ops (10,838,016 macc; 225,792 comp; 0 add; 0 mul; 0 bitwise)
Layer 76: 43,502,592 ops (43,352,064 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 77: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 78: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 79: 86,854,656 ops (86,704,128 macc; 150,528 comp; 0 add; 0 mul; 0 bitwise)
Layer 80: 173,709,312 ops (173,408,256 macc; 301,056 comp; 0 add; 0 mul; 0 bitwise)
Layer 81 (backbone_conv8): 86,779,392 ops (86,704,128 macc; 75,264 comp; 0 add; 0 mul; 0 bitwise)
Layer 82 (backbone_conv9): 5,513,088 ops (5,419,008 macc; 94,080 comp; 0 add; 0 mul; 0 bitwise)
Layer 83 (backbone_conv10): 1,312,640 ops (1,290,240 macc; 22,400 comp; 0 add; 0 mul; 0 bitwise)
Layer 84 (conv12_1): 647,360 ops (645,120 macc; 2,240 comp; 0 add; 0 mul; 0 bitwise)
Layer 85 (conv12_2): 83,440 ops (80,640 macc; 2,800 comp; 0 add; 0 mul; 0 bitwise)
Layer 86: 1,354,752 ops (1,354,752 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 87: 40,320 ops (40,320 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 88: 677,376 ops (677,376 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 89: 20,160 ops (20,160 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 275,184 bytes out of 2,396,160 bytes total (11%)
Bias memory: 536 bytes out of 8,192 bytes total (7%)
As the application starts with the Face Detection model, the corresponding bias values are loaded into the CNN engine before every execution. Then, CNN_1 and FIFO configurations are executed for Face Detection.
cnn_1_load_bias(); // Load bias data of CNN_1
// Bring CNN_1 state machine of Face Detection model into consistent state
*((volatile uint32_t *) 0x51000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x51000008) = 0x00004a59; // Layer count
*((volatile uint32_t *) 0x52000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x52000008) = 0x00004a59; // Layer count
*((volatile uint32_t *) 0x53000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x53000008) = 0x00004a59; // Layer count
*((volatile uint32_t *) 0x54000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x54000008) = 0x00004a59; // Layer count
// Disable FIFO control
*((volatile uint32_t *) 0x50000000) = 0x00000000;
Similar to the MAX78000 application, the output of the Face Detection CNN model is a set of box coordinates and their corresponding scores. The non-maximum suppression (NMS) algorithm selects a bounding box with the highest confidence score which is displayed on the TFT.
If the Face Detection CNN model detects a face, a rectangular sub-image that contains only one face is selected and resized to 112x112 RGB image to match the Face Identification CNN model input.
Face Identification
The Face Identification CNN model has 73 layers and uses a 112x112 RGB image as an input.
Face Identification CNN:
SUMMARY OF OPS
Hardware: 445,470,720 ops (440,252,416 macc; 4,848,256 comp; 370,048 add; 0 mul; 0 bitwise)
Layer 0: 22,478,848 ops (21,676,032 macc; 802,816 comp; 0 add; 0 mul; 0 bitwise)
Layer 1: 2,809,856 ops (1,806,336 macc; 1,003,520 comp; 0 add; 0 mul; 0 bitwise)
Layer 2: 231,612,416 ops (231,211,008 macc; 401,408 comp; 0 add; 0 mul; 0 bitwise)
Layer 3: 1,404,928 ops (903,168 macc; 501,760 comp; 0 add; 0 mul; 0 bitwise)
Layer 4: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 5: 6,522,880 ops (6,422,528 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 6: 1,003,520 ops (903,168 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 7: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 8: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 9: 50,176 ops (0 macc; 0 comp; 50,176 add; 0 mul; 0 bitwise)
Layer 10: 6,522,880 ops (6,422,528 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 11: 1,003,520 ops (903,168 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 12: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 13: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 14: 50,176 ops (0 macc; 0 comp; 50,176 add; 0 mul; 0 bitwise)
Layer 15: 6,522,880 ops (6,422,528 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 16: 1,003,520 ops (903,168 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 17: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 18: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 19: 50,176 ops (0 macc; 0 comp; 50,176 add; 0 mul; 0 bitwise)
Layer 20: 6,522,880 ops (6,422,528 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 21: 1,003,520 ops (903,168 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 22: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 23: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 24: 50,176 ops (0 macc; 0 comp; 50,176 add; 0 mul; 0 bitwise)
Layer 25: 13,045,760 ops (12,845,056 macc; 200,704 comp; 0 add; 0 mul; 0 bitwise)
Layer 26: 702,464 ops (451,584 macc; 250,880 comp; 0 add; 0 mul; 0 bitwise)
Layer 27: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 28: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 29: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 30: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 31: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 32: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 33: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 34: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 35: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 36: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 37: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 38: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 39: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 40: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 41: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 42: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 43: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 44: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 45: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 46: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 47: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 48: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 49: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 50: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 51: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 52: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 53: 6,472,704 ops (6,422,528 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 54: 501,760 ops (451,584 macc; 50,176 comp; 0 add; 0 mul; 0 bitwise)
Layer 55: 6,422,528 ops (6,422,528 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 56: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 57: 25,088 ops (0 macc; 0 comp; 25,088 add; 0 mul; 0 bitwise)
Layer 58: 12,945,408 ops (12,845,056 macc; 100,352 comp; 0 add; 0 mul; 0 bitwise)
Layer 59: 351,232 ops (225,792 macc; 125,440 comp; 0 add; 0 mul; 0 bitwise)
Layer 60: 3,211,264 ops (3,211,264 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 61: 1,618,176 ops (1,605,632 macc; 12,544 comp; 0 add; 0 mul; 0 bitwise)
Layer 62: 125,440 ops (112,896 macc; 12,544 comp; 0 add; 0 mul; 0 bitwise)
Layer 63: 1,605,632 ops (1,605,632 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 64: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 65: 6,272 ops (0 macc; 0 comp; 6,272 add; 0 mul; 0 bitwise)
Layer 66: 1,618,176 ops (1,605,632 macc; 12,544 comp; 0 add; 0 mul; 0 bitwise)
Layer 67: 125,440 ops (112,896 macc; 12,544 comp; 0 add; 0 mul; 0 bitwise)
Layer 68: 1,605,632 ops (1,605,632 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 69: 0 ops (0 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 70: 6,272 ops (0 macc; 0 comp; 6,272 add; 0 mul; 0 bitwise)
Layer 71: 809,088 ops (802,816 macc; 6,272 comp; 0 add; 0 mul; 0 bitwise)
Layer 72: 14,464 ops (8,192 macc; 0 comp; 6,272 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 909,952 bytes out of 2,396,160 bytes total (38.0%)
Bias memory: 7,296 bytes out of 8,192 bytes total (89.1%)
To run the Face Identification model, the corresponding bias values are loaded to CNN before every execution. Then, CNN_2 and FIFO configurations are executed for Face Identification.
cnn_2_load_bias(); // Load bias data of CNN_2
// Bring CNN_2 state machine of Face ID model into consistent state
*((volatile uint32_t *) 0x51000000) = 0x00108008; // Stop SM
*((volatile uint32_t *) 0x51000008) = 0x00000048; // Layer count
*((volatile uint32_t *) 0x52000000) = 0x00108008; // Stop SM
*((volatile uint32_t *) 0x52000008) = 0x00000048; // Layer count
*((volatile uint32_t *) 0x53000000) = 0x00108008; // Stop SM
*((volatile uint32_t *) 0x53000008) = 0x00000048; // Layer count
*((volatile uint32_t *) 0x54000000) = 0x00108008; // Stop SM
*((volatile uint32_t *) 0x54000008) = 0x00000048; // Layer count
// Enable FIFO control
*((volatile uint32_t *) 0x50000000) = 0x00001108; // FIFO control
The output of the Face Identification CNN model is an embedding vector length of 64 that corresponds to the input facial image. Before feeding the embedding vector to the Dot Product model as an input, the vector is L2 normalized.
Dot Product
The Dot Product model has one linear layer and uses an embedding vector length of 64 as an input.
Dot Product CNN:
SUMMARY OF OPS
Hardware: 65,536 ops (65,536 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
Layer 73: 65,536 ops (65,536 macc; 0 comp; 0 add; 0 mul; 0 bitwise)
RESOURCE USAGE
Weight memory: 65,536 bytes out of 2,396,160 bytes total (2.7%)
Bias memory: 0 bytes out of 8,192 bytes total (0.0%)
To run the Dot Product model, the corresponding bias values are loaded to the CNN engine before every execution. Then, CNN_3 and FIFO configurations are executed for Dot Product.
cnn_3_load_bias(); // Load bias data of CNN_3
//Dot product CNN state machine configuration
*((volatile uint32_t *) 0x51000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x51000008) = 0x00004949; // Layer count
*((volatile uint32_t *) 0x52000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x52000008) = 0x00004949; // Layer count
*((volatile uint32_t *) 0x53000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x53000008) = 0x00004949; // Layer count
*((volatile uint32_t *) 0x54000000) = 0x00100008; // Stop SM
*((volatile uint32_t *) 0x54000008) = 0x00004949; // Layer count
// Disable FIFO control
*((volatile uint32_t *) 0x50000000) = 0x00000000;
The output of the Dot Product model is 1024 dot product similarities, where each one represents the similarity between the given face and the faces recorded in the database. If the maximum of dot product similarities is higher than the threshold, the subject with the maximum similarity is declared as the identified face and is displayed on the TFT. Otherwise, the output will be ‘Unknown’.
Adding the Images of a New Subject
The application allows adding a new subject to the database. By pressing the “Record” button on the touchscreen, the subject name can be entered.
The next step is to capture the subject’s face with the camera. Press the “OK” button to add the captured image to the database or “Retry” to recapture.
The application calculates an embedding vector based on the new subject’s face and stores it in an internal flash database. The Dot Product CNN model uses an embedding database to recognize a subject and makes a final decision.
Conclusion
The ultra-low power CNN inference engine makes the MAX78000/MAX78002 microcontrollers ideal for batterypowered IoT applications. Utilizing multiple models on the MAX78000 [1] and MAX78002 [2] AI microcontrollers enables the implementation of very complex applications in an energy-efficient way.
References
[3] MAX78000FTHR Evaluation Kit Data Sheet
[4] MAX78000FTHR Facial Recognition Application
[5] MAX78002EVKIT Facial Recognition Application