AN-1374: ADE7912/ADE7913 Front-End DSP Specifications

Introduction

This application note explains several aspects of the digital filtering associated with the Σ-Δ modulators used in the ADE7912/ ADE7913. The role of the filters is to decimate the outputs of the modulators to various rates, while eliminating high frequency noise. These rates start from a high of 8 kHz and go as low as 1 kHz, allowing the user to update the rates to the microcontroller processing bandwidth.

Digital Decimation Filtering

Functional Description

Figure 1 shows the block diagram of the decimation filtering implemented in the ADE7912/ADE7913. The Σ-Δ modulator provides a bit stream with a frequency of 1 MHz when the chip is clocked at CLKIN = 4.096 MHz. The SINC4 filter uses four decimation ratios—32, 64, 128, and 256—to provide outputs at 32 kHz, 16 kHz, 8 kHz and 4 kHz. To limit the bandwidth to meaningful frequencies while also keeping the data rate as low as possible, an extra low-pass filter (LPF) with 60 dB attenuation is used. This makes the subsequent rms and power calculations more precise, reducing the bandwidth a micro-controller must reserve for the metrology calculations.

Figure 1. Block diagram of the decimation filtering implemented in the ADE7912/ADE7913.

The LPF performs another decimation by 4, and has internal flexibility, which leads to two different bandwidths. The LPF is implemented as two separate, sixth-order filters: one filter for the narrower bandwidths, one filter for the larger bandwidths.

The ADE7912/ADE7913 provide multiple output data rates (ODRs): 8 kHz, 4 kHz, 2 kHz, and 1 kHz, as well as two selectable bandwidths for each of these rates (see Table 1). The selectable ODRs help users address a wide range of scenarios to make their own trade-offs in the datapaths implemented in the microcontroller.

Table 1. CONFIG Register Settings for Obtaining Various ODRs and Bandwidths
CONFIG Register ODR (kHz) SINC4 + LPF Bandwidth (kHz)
Bits[5:4] (ADC_FREQ) Setting Bit 7 (BW) Setting
00 0 8 3.338
00 1 8 2.137
01 0 4 1.670
01 1 4 1.069
10 0 2 0.836
10 1 2 0.535
11 0 1 0.418
11 1 1 0.268

ODR and bandwidth selection is performed by Bit 7 (BW) and Bits[5:4] (ADC_FREQ) in the CONFIG register. Table 1 shows the different BW and ADC_FREQ settings required when the ADE7912/ADE7913 is clocked at CLKIN = 4.096 MHz. The bandwidth is indicated by the point at which the gain is attenuated by 3 dB.

Frequency Response and Time Delay Characteristics of the SINC4 + LPF Filters

The equivalent Z-domain formula of the SINC4 for various decimation ratios (DRs) is shown in the following equation:

Equation 1.

The Z-domain formula of the LPF that corresponds to the narrower bandwidth (BW, Bit 7 of the CONFIG register, is set to 1) is shown in the following equation:

Equation 2.

where LPF_BW1 is the LPF that corresponds to the narrower bandwidth.

The Z-domain formula of the LPF that corresponds to the larger bandwidth (BW, Bit 7 of the CONFIG register, is cleared to 0) is shown in the following equation:

Equation 3.

where LPF_BW2 is the LPF that corresponds to the larger bandwidth.

Magnitude Frequency Response and Time Delays for Various Filters

Figure 2 through Figure 25 and Table 2 through Table 32 provide detailed information about the magnitude frequency response and the time delays introduced in the signal path by the various filters. The output data rate (ODR) is the output frequency at which the analog-to-digital converter (ADC) samples are provided by the ADE7912/ADE7913. The bandwidth of the filter (BW) is the point at which the gain is attenuated by 3 dB. The full frequency response, or the response up to the −3 dB point, and the flat-band response (from 0 dB down to −0.8 dB attenuation) are shown in all ODR and BW cases.

The phase delay defines the propagation delay in the phase of a sinusoidal signal passing through the filter. Tables showing the phase delay at various frequencies are shown for all ODR and BW cases.

From the perspective of power calculations, these time delays do not affect the final results because both voltage and current signals are subject to identical time delay propagation. However, in case of transient events or events synchronous to the zero crossings, it may be useful to know the time delays.

The frequency points are selected in such a way that the intermediate values can be obtained with accuracy by piecewise linear interpolation. These frequency points may be useful, for example, if amplitude corrections are necessary.

ODR = 8 kHz and BW = 3.338 kHz

Figure 2. Full frequency response for ODR = 8 kHz and BW= 3.338 kHz.
Figure 3. 3 dB point response for ODR = 8 kHz and BW = 3.338 kHz.
Figure 4. Flat-band response for ODR = 8 kHz and BW = 3.338 kHz.
Table 2. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −0.32 −0.87 −1.66 −2.67 −3.93 −5.44 −7.21 −9.26
Table 3. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz; Frequency Range = 500 Hz to 900 Hz
Frequency (Hz)
500 550 600 650 700 750 800 850 900
Magnitude (milli_dB) −11.6 −14.22 −17.15 −20.40 −23.97 −27.87 −32.11 −36.69 −41.61
Table 4. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz; Frequency Range = 950 Hz to 1350 Hz
Frequency (Hz)
950 1000 1050 1100 1150 1200 1250 1300 1350
Magnitude (milli_dB) −46.86 −52.45 −58.37 −64.6 −71.13 −77.95 −85.05 −92.41 −100
Table 5. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz; Frequency Range = 1400 Hz to 2200 Hz
Frequency (Hz)
1400 1500 1600 1700 1800 1900 2000 2100 2200
Magnitude (dB) −0.108 −0.124 −0.141 −0.159 −0.177 −0.197 −0.218 −0.241 −0.265
Table 6. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz; Frequency Range = 2300 Hz to 3100 Hz
Frequency (Hz)
2300 2400 2500 2600 2700 2800 2900 3000 3100
Magnitude (dB) −0.291 −0.318 −0.346 −0.374 −0.402 −0.434 −0.486 −0.6 −0.859
Table 7. SINC4 + LPF Gain Response at Various Frequencies for ODR =8 kHz and BW = 3.338 kHz; Frequency Range = 3200 Hz to 3500 Hz
Frequency (Hz)
3200 3300 3338 3400 3500
Magnitude (dB) −1.414 −2.452 −3.0 −4.09 −6.27
Table 8. SINC4 +LPF Phase Delay Response at Various Frequencies for ODR = 8 kHz and BW = 3.338 kHz
Frequency (Hz)
50 500 750 1000 1500 2000 2500 3000 3300
Phase Delay (μs) 225 226 227 229 234 241 254 277 321

ODR = 8 kHz and BW = 2.137 kHz

Figure 5. Full frequency response for ODR = 8 kHz and BW = 2.137 kHz.
Figure 6. 3 dB Point response for ODR = 8 kHz and BW = 2.137 kHz.
Figure 7. Flat-band response for ODR = 8 kHz and BW = 2.137 kHz.
Table 9. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 2.137 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −0.56 −1.5 −2.77 −4.34 −6.19 −8.25 −10.51 −12.91
Table 10. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 2.137 kHz; Frequency Range = 500 Hz to 900 Hz
Frequency (Hz)
500 550 600 650 700 750 800 850 900
Magnitude (milli_dB) −15.44 −18.08 −20.82 −23.68 −26.70 −29.90 −33.36 −37.13 −41.29
Table 11. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 2.137 kHz; Frequency Range = 950 Hz to 1400 Hz
Frequency (Hz)
950 1000 1050 1100 1150 1200 1250 1300 1400
Magnitude (milli_dB) −45.90 −51.01 −56.64 −62.8 −69.41 −76.40 −83.64 −90.96 −105
Table 12. SINC4 + LPF Gain Response at Various Frequencies for ODR = 8 kHz and BW = 2.137 kHz; Frequency Range = 1500 Hz to 2200 Hz
Frequency (Hz)
1500 1600 1700 1800 1900 2000 2100 2137 2200
Magnitude (dB) −0.119 −0.140 −0.188 −0.314 −0.621 −1.274 −2.243 −3.01 −4.167
Table 13. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 8 kHz and BW = 2.137 kHz
Frequency (Hz)
50 500 750 1000 1500 1750 2000 2100
Phase Delay (μs) 294 296 299 304 322 338 365 377

ODR = 4 kHz and BW = 1.67 kHz

Figure 8. Full frequency response for ODR = 4 kHz and BW = 1.67 kHz.
Figure 9. 3 dB Point response for ODR = 4 kHz and BW = 1.67 kHz.
Figure 10. Flat-band response for ODR = 4 kHz and BW = 1.67 kHz.
Table 14. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.67 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −1.323 −3.589 −6.865 −11.234 −16.784 −23.596 −31.732 −41.222
Table 15. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.67 kHz; Frequency Range = 500 Hz to 900 Hz
Frequency (Hz)
500 550 600 650 700 750 800 850 900
Magnitude (milli_dB) −52.06 −64.199 −77.554 −92.011 −107.44 −123.73 −140.81 −158.66 −177.37
Table 16. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.67 kHz; Frequency Range = 950 Hz to 1350 Hz
Frequency (Hz)
950 1000 1050 1100 1150 1200 1250 1300 1350
Magnitude (dB) −0.197 −0.218 −0.240 −0.265 −0.291 −0.318 −0.346 −0.373 −0.401
Table 17. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.67 kHz; Frequency Range = 1400 Hz to 1900 Hz
Frequency (Hz)
1400 1450 1500 1550 1600 1670 1700 1800 1900
Magnitude (dB) −0.433 −0.486 −0.598 −0.856 −1.407 −3.01 −4.071 −8.807 −14.39
Table 18. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 4 kHz and BW = 1.67 kHz
Frequency (Hz)
50 250 500 750 1000 1250 1500 1650
Phase Delay (μs) 450 452 458 467 483 508 555 608

ODR = 4 kHz and BW = 1.069 kHz

Figure 11. Full frequency response for ODR = 4 kHz and BW = 1.069 kHz.
Figure 12. 3 dB Point response for ODR = 4 kHz and BW = 1.069 kHz.
Figure 13. Flat-band response for ODR = 4 kHz and BW = 1.069 kHz.
Table 19. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.069 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −2.19 −5.60 −9.92 −14.85 −20.23 −26.10 −32.76 −40.68
Table 20. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.069 kHz; Frequency Range = 500 Hz to 900 Hz
Frequency (Hz)
500 550 600 650 700 750 800 850 900
Magnitude (milli_dB) −50.39 −62.16 −75.77 −90.33 −104.7 −119.2 −139.8 −186.9 −311.5
Table 21. SINC4 + LPF Gain Response at Various Frequencies for ODR = 4 kHz and BW = 1.069 kHz; Frequency Range = 950 Hz to 1300 Hz
Frequency (Hz)
950 1000 1050 1069 1100 1150 1200 1250 1300
Magnitude (dB) −0.617 −1.265 −2.423 −3.015 −4.147 −6.326 −8.776 −11.343 −13.936
Table 22. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 4 kHz and BW = 1.069 kHz
Frequency (Hz)
50 250 500 750 1000 1250
Phase Delay (μs) 588 593 609 643 730 795

ODR = 2 kHz and BW = 0.836 kHz

Figure 14. Full frequency response for ODR = 2 kHz and BW = 0.836 kHz.
Figure 15. 3 dB Point response for ODR = 2 kHz and BW = 0.836 kHz.
Figure 16. Flat-band response for ODR = 2 kHz and BW = 0.836 kHz.
Table 23. SINC4 + LPF Gain Response at Various Frequencies for ODR = 2 kHz and BW = 0.836 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −5.5 −15.37 −30.27 −50.55 −76 −106 −139 −176
Table 24. SINC4 + LPF Gain Response at Various Frequencies for ODR = 2 kHz and BW = 0.836 kHz; Frequency Range = 500 Hz to 1000 Hz
Frequency (Hz)
500 550 600 650 700 750 800 836 850 900 950 1000
Magnitude (dB) −0.216 −0.263 −0.316 −0.372 −0.431 −0.594 −1.39 −3.05 −4.03 −8.75 −14.33 −20.0
Table 25. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 2 kHz and BW = 0.836 kHz
Frequency (Hz)
50 125 250 350 400 500 750 830
Phase Delay (μs) 901 904 915 930 939 965 1109 1223

ODR = 2 kHz and BW = 0.535 kHz

Figure 17. Full frequency response for ODR = 2 kHz and BW = 0.535 kHz.
Figure 18. 3 dB Point response for ODR = 2 kHz and BW = 0.535 kHz.
Figure 19. Flat-band response for ODR = 2 kHz and BW = 0.535 kHz.
Table 26. SINC4 + LPF Gain Response at Various Frequencies for ODR = 2 kHz and BW = 0.535 kHz; Frequency Range = 50 Hz to 450 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 450
Magnitude (milli_dB) 0 −7.69 −17.99 −30.48 −48.05 −73.36 −102.34 −137.17 −305.62
Table 27. SINC4 + LPF Gain Response at Various Frequencies for ODR = 2 kHz and BW = 0.535 kHz; Frequency Range = 500 Hz to 750 Hz
Frequency (Hz)
500 535 550 600 650 700 750
Magnitude (dB) −1.24 −3.01 −4.10 −8.72 −13.88 −19.01 −24.03
Table 28. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 2 kHz and BW = 0.535 kHz
Frequency (Hz)
50 125 250 350 400 500 535
Phase Delay (μs) 1177 1185 1217 1268 1309 1459 1525

ODR = 1 kHz and BW = 0.418 kHz

Figure 20. Full frequency response for ODR = 1 kHz and BW = 0.418 kHz.
Figure 21. 3 dB Point response for ODR = 1 kHz and BW = 0.418 kHz.
Figure 22. Flat-band response for ODR = 1 kHz and BW = 0.418 kHz.
Table 29. SINC4 + LPF Gain Response at Various Frequencies for ODR = 1 kHz and BW = 0.418 kHz; Frequency Range = 50 Hz to 600 Hz
Frequency (Hz)
50 100 150 200 250 300 350 400 418 450 500 550 600
Magnitude (dB) 0 −0.024 −0.070 −0.133 −0.210 −0.310 −0.424 −1.355 −2.98 −8.64 −19.95 −31.74 −45.78
Table 30. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 1 kHz and BW = 0.418 kHz
Frequency (Hz)
50 100 150 200 250 300 350 400
Phase Delay (μs) 1806 1820 1843 1879 1930 2005 2122 2349

ODR = 1 kHz and BW = 0.268 kHz

Figure 23. Full frequency response for ODR = 1 kHz and BW = 0.268 kHz.
Figure 24. 3 dB Point response for ODR = 1 kHz and BW = 0.268 kHz.
Figure 25. Flat-band response for ODR = 1 kHz and BW = 0.268 kHz.
Table 31. SINC4 + LPF Gain Response at Various Frequencies for ODR = 1 kHz and BW = 0.268 kHz; Frequency Range = 50 Hz to 400 Hz
Frequency (Hz)
50 100 150 200 250 268 300 350 400
Magnitude (dB) 0 −0.022 −0.065 −0.128 −1.20 −3.0 −8.615 −18.9 −28.91
Table 32. SINC4 + LPF Phase Delay Response at Various Frequencies for ODR = 1 kHz and BW = 0.268 kHz
Frequency (Hz)
50 100 150 200 250
Phase Delay (μs) 2363 2402 2477 2615 2913

Author

Generic_Author_image

Gabriel Antonesei