AN-1342: AD9142 to AD9142A Migration

Introduction

The AD9142 and AD9142A are pin-compatible 16-bit, dual low voltage differential signaling (LVDS) high speed digital-toanalog converters (DACs). Both products have many of the same features, but the AD9142A services wider bandwidth applications compared to the AD9142 due to its higher maximum interface speed. Therefore, the AD9142A is the recommended product for new designs. For those who currently use the AD9142, consider migrating to the AD9142A. The purpose of this application note is to describe the differences between the two products and provide a guide on upgrading to the AD9142A from the AD9142. The AD9142A has additional interface features that allow the device to operate at higher interface rates (up to 575 MHz data clock input). The AD9142A also provides interface error detection features that allow the customers to debug the system interface timing more easily.

Compared to the AD9142, the AD9142A has additional feature blocks and slight pin functionality differences. The areas of the AD9142A that differ from the AD9142 are highlighted in Figure 1. The blue highlighted delay locked loop (DLL) and sample error detection (SED) blocks correspond to the interface support differences in the block diagram. The green highlighted DCIx, DACCLKx, FRAMEx/PARITYx, and REFx/SYNCx pins are areas of the device where the data sheet specifications are slightly different. The yellow highlighted data pins (D15x through D0x) and register map have additional serial port interface (SPI) software related differences. Refer to the AD9142 or AD9142A data sheet for details regarding features not addressed in this application note.

Figure 1. Block Diagram of the AD9142A.

Figure 1. Block Diagram of the AD9142A.

Product Comparison Overview

The main differences between the AD9142 and AD9142A are related to the data interface operation. The AD9142 has a maximum of 250 MHz clock rate for the data clock input (DCIP and DCIN LVDS pin inputs). The AD9142A, by contrast, has a maximum data interface rate of 575 MHz. Table 1 through Table 3 list specific feature differences between the AD9142 and AD9142A products and include a brief description for each feature difference.

Table 1. Interface Feature Comparison
Feature AD9142 AD9142A Details
Interface Support Delay line only Delay line (bypass mode) and DLL The delay line (bypass mode) setup and hold timing is different between the two products. When using delay line mode for the AD9142A, ensure the data clock input (DCI) signal is set to dc-coupled (SPI register setting). In addition to the delay line mode, the AD9142A includes a DLL to ease interface timing constraints, especially at high data rates. The DLL operates for DCI clock rates from 250 MHz to 575 MHz. Set the DCI to ac-coupled (SPI register setting).
Interface Error Checking Support No features supported Parity and SED and automatic error detection (AED) Two types of interface error checking features are supported on the AD9142A only: SED/AED and parity. SED/AED uses a SPI-programmable pattern to check against input values that the device receives. Parity uses the frame signal as the parity bit. This feature shows errors in real time; it is not restricted to a SPI programmed repeating pattern to determine errors occurring at the interface.
Table 2. Data Sheet Specification Comparisons
Feature AD9142 AD9142A Details
Interface Timing Delay line (bypass mode) interface timing specified Delay line (bypass mode) and DLL interface timing specified The DLL interface timing is specified in the AD9142A due to the added feature on this product. Bypass mode timing is specified on both products, but the timing is slightly shifted between the AD9142 and the AD9142A. There are also slightly different SPI programming writes required for the various delay setting options.
Sync Clock vs. DAC Clock Timing Setup and hold times specified in data sheet Setup and hold times specified in data sheet The setup and hold times of the sync clock vs. the DAC clock are slightly shifted between the AD9142 and the AD9142A. The timing requirements are specified in the AD9142 and AD9142A data sheets.
Byte Mode Capabilities Byte mode can be used with both sync on and sync off Byte mode only works with sync off AD9142: Byte mode is operational when sync is off and both the SPI and frame signals can be used to reset the FIFO. However, when sync is on or when the NCO is used, only a frame FIFO request can reset the FIFO in these byte mode cases. The SPI signal cannot be used to reset the FIFO in either of these conditions in byte mode.

AD9142A: Byte mode can only be used when operating with sync off and only the SPI FIFO request can be used to reset the FIFO, not the frame signal.
DCIx Pin Input Levels DCIx levels specify a higher swing than data pins DCIx levels specified with the same swing as data pins The AD9142A does not require a special condition of a higher voltage swing level for the DCIx pins, DCIP (Pin 28)/DCIN (Pin 29), to operate, unlike the AD9142.
Table 3. Additional SPI Register Comparisons
Feature AD9142 AD9142A Details
LVDS LSB Data Bit Power-Downs Feature not supported PWR_DOWN_DATA_INPUT_BITS SPI control The AD9142A has the ability to power down the bottom 4 LSBs of the LVDS buffer to lower the resolution of the device. Use Register 0x39, Bits[3:0] to power down the corresponding data bit as desired.
Revision ID ID = 0x05 ID = 0x0B The version register (0x7F) indicates which revision of silicon is in the system.

Data Interface Features


The AD9142 interface operates at up to a 250 MHz data input clock rate. It provides a programmable delay line feature with four settings for different delay options depending on the system timing skew that needs compensation. The AD9142A has a programmable delay line feature like the AD9142. It also has a DLL that allows the data interface to operate from a 250 MHz to 575 MHz data input clock rate. The timing specifications for the programmable delay line are slightly different between the AD9142 and the AD9142A. For those who are migrating their systems from the AD9142 to the AD9142A, review these timing specifications. These timing differences and SPI delay settings are outlined in more detail in Table 5.

The DLL feature included in the AD9142A enables higher data rates and eases the interface timing constraints encountered at these higher data rates. To use this feature, program a set of registers for different controls in the feature. The DLL control bits and interrupt request (IRQ) controls related to the DLL are listed in Table 4, including the exact register addresses and some details regarding proper ways to program the device for various operation modes.

Table 4. Interface Support Details
Device Register Addresses Details
AD9142
Interface IRQs Not applicable Not applicable
Delay Line Enable Register 0x5F, Bit 3 Writing a 1 to this bit enables the programmable delay line.
Programmable Delay Line Setting Register 0x5E, Bits[7:0], Register 0x5F, Bits[2:0] The four different delay settings are programmed through these registers using valid delay setting register values, detailed in Table 5.
Device Configuration Register 0x79 = 0x18, Register 0x80 = 0xAD, Register 0xE1 = 0x1A Required writes for start-up routine are needed for proper operation.
AD9142A
Interface IRQs IRQ enables: Register 0x04, Bits[5:4]
IRQ status: Register 0x06, Bits[5:4]
IRQx pin select: Register 0x08, Bits[5:4]
Interrupt enable mask bits, status bits, and IRQ output pin select bits for DLL lock and DLL warning.
Delay Line Enable/DLL Enable Register 0x0A, Bit 7 Register location change and logic polarity change. Writing a 0 to this bit enables the straight programmable delay line (bypass mode). Writing a 1 to this bit starts the DLL state machine logic, which eases interface timing at higher input data speeds. The DLL must lock without any warnings to be stable and usable. For more information, see the AD9142A data sheet.
Programmable Delay Line Setting Register 0x5E, Bits[7:0], Register 0x5F, Bits[2:0] The four different delay settings are programmed through these registers using valid delay setting register values, detailed in Table 5.
Device Configuration Using DLL: Register 0x5E = 0xFE
Using delay line: Register 0x0D = 0x16
When using the DLL, turn off the LSB delay cell. When using the delay line, dc couple the DCI internally.
DLL Interface Controls Register 0x0A to Register 0x0E There are various interface controls for using the DLL. Follow Start-Up Sequence 1 for setting up the DLL and Start-Up Sequence 2 for setting up the delay line (bypass mode) interface. See the AD9142A data sheet for more information.
Table 5. Bypass Mode Interface Timing Support Details
Device Delay 0 Delay 1 Delay 2 Delay 3
AD9142
Register 0x5E, Bits[7:0] 0x00 0x07 0x7F 0xFF
Register 0x5F, Bits[2:0] 0x0 0x0 0x0 0x5
   Setup Time, tS (ns)1 −1.25 −1.50 −1.70 −1.93
   Hold Time, tH (ns) 2.51 2.82 3.23 3.64
   |tH + tH| (ns) 1.26 1.32 1.53 1.71
AD9142A
Register 0x5E, Bits[7:0] 0x00 0x80 0xF0 0xFE 0x00 0x80 0xF0 0xFE
Register 0x5F, Bits[7:0] 0x60 0x67 0x67 0x67
   tS (ns)1 −0.81 −0.97 -1.13 -1.28
   tH (ns) 1.96 2.20 2.53 2.79
   |tS + tH| (ns) 1.15 1.23 1.40 1.51
1 The negative sign indicates the direction of the setup time. The setup time is defined as positive when it is on the left side of the clock edge and negative when it is on the right side of the clock edge.

Example Interface Start-Up Routin Comparison

Table 6 highlights the differences between the AD9142 and AD9142A in the start-up routines needed for a specific condition. Table 6 compares the different register writes needed for the delay line mode interface scheme, which is the common interface mode for both products. A similar start-up routine is described in both product data sheets.

Table 6. Example Start-Up Routine Comparison
Register Address AD9142 Register Value AD9142A Register Value Description
0x00 0x20 0x20 Issue software reset
0x20 0x01 0x01 Device start-up configuration
0x79 0x18 Not appplicable AD9142 device start-up configuration only
0x80 0xAD Not applicable AD9142 device start-up configuration only
0xE1 0x1A Not applicable AD9142 device start-up configuration only
0x14 0xE7 0xE7 Configure PLL loop bandwidth and charge pump current
0x15 0xC2 0xC2 Configure VCO divider and loop divider
0x12 0xC0 0xC0 Enable PLL
0x12 0x80 0x80 Enable PLL autosearch mode, verify PLL is locked if Register 0x16, Bit 7 = 1
0x5E 0x00 0x00 Configure delay line interface delay setting of 0
0x5F 0x08 0x60 AD9142: enable delay line and delay setting of 0; AD9142A: delay setting of 0
0x0D Not applicable 0x16 DC couple DCI on the AD9142A only
0x0A Not appplicable 0x00 Turn off DLL and duty cycle correction on the AD9142A only
0x28 0x03 0x03 8× interpolcation
0x25 0x01 0x01 Reset FIFO, Register 0x24 reads back one of the three values: 0x37, 0x40, 0x41
0x27 0x80 0x80 Enable inverse sinc
0x01 0x00 0x00 Power up DAC outputs

Test Conditions

The test conditions used in the example start-up routine comparison in Table 6 are as follows:

  • fDCI = fDATA = 200 MHz
  • 8× interpolation
  • Phase-locked loop (PLL) enabled: fREF = 200 MHz, fDAC = 1.6 GHz
  • Voltage controlled oscillator (VCO) divider = fVCO/fDAC = 1
  • Loop divider = fDAC/fREF = 8
  • Inverse sinc enabled

Data Interfacec Error Checking


A significant advantage of the AD9142A is that it provides data interface error checking capabilities. The AD9142A has SED/AED functions, in addition to parity checking functionality, to determine whether any errors are received on the interface. These functions allow users to troubleshoot their data interface and verify that the timing constraints are met properly in their systems.

There are multiple controls available for users to program and specify the test conditions for these error checking features. The control bits and IRQ controls related to both SED/AED and parity are detailed in Table 7 and include the exact register address locations for each of the controls along with details regarding proper configuration of the feature options. For more information on the full functionality and programmability of each feature, refer to the AD9142A data sheet.

Table 7. Interface Error Checking Support Details
Device Register Addresses Details
AD9142
No Features Supported Not applicable Not applicable
AD9142A
Feature IRQs IRQ enables: Register 0x04, Bit 7 for parity, Bit 6 for SED
IRQ status: Register 0x06, Bit 7 for parity, Bit 6 for SED
IRQx pin select: Register 0x08, Bit 7 for parity, Bit 6 for SED
Interrupt enable mask bits, status bits, and IRQ output pin select bits for parity and SED failures.
Frame Signal Usage Register 0x09, Bit 5: set high when using parity
Register 0x09, Bit 4: set high when using SED or normal frame operation (when needed)
Register 0x09, Bits[1:0]: set to 1 for parity, 2 for SED or normal frame operation
A frame signal is required when running parity or when using a word depth of four for SED or AED. Certain other normal operating modes may require a frame signal, such as using byte mode interface or multichip synchronization schemes. Depending on the mode of operation, this register must be set appropriately for the type of frame signal needed.
SED/AED Control bits and status flags: Register 0x60
SED/AED pattern values: Register 0x61 to Register 0x68
The control bits allow the user to program the SED/AED depth, select between SED and AED operation, clear any error flags, and enable the SED/AED comparison. The pattern sent to the device is programmed in the pattern value registers for the device to compare the bits actually received and raise any error flags in the status flag bits as well as the IRQ bits. For more information, see the AD9142A data sheet.
Parity Control bits and status flags: Register 0x6A
Error counters: Register 0x6B to Register 0x6C
The control bits allow the user to select between even and odd parity, clear any error flags, and enable the parity operation. If any errors occur on either the rising or falling edges of the clock, the error counters increment appropriately and raise corresponding error flags in the status flag bits as well as the IRQ bits. For more information, see the AD9142A data sheet.

Sync vs. DAC Clock Timing


In addition to the interface timing differences, there is a slight sync clock to DAC clock tS and tH shift between the AD9142 and AD9142A. The details of this shift are shown in Table 8. The timing details are included in each product data sheet. If using the multichip sync function on the AD9142, note these slight timing differences to adjust user systems accordingly when migrating from the AD9142 to the AD9142A.

Table 8. Sync Clock and DAC Clock Timing Support Details
Falling Edge Sync Timing (default) AD9142 Max (ps) AD9142A Max (ps)
tS (ns) 246 324
tH (ns) -11 -92
|tS + tH| (ns) 235 232

Author

Generic_Author_image

Michelle Viani

Michele Viani, Applications Engineer, has worked in the High Speed Converter Group at Analog Devices for 6.5 years. Michele has worked as both a Product Engineer and Applications Engineer, responsible for evaluating high speed digital-to-analog converter products and providing technical support to customers in solving implementation issues. Michele holds a Bachelor’s Degree in Electrical Engineering from Rensselaer Polytechnic Institute.