AN-1143: ADV7511 HDCP 1.1 Enable/Disable Option
HDCP 1.1 Features
The ADV7511 HDMI® transmitter supports HDCP 1.1 features; however, there has been some misunderstanding within the industry as to the proper implementation of some of these HDCP 1.1 features, specifically the enhanced link verification (Pj checking). Because there have been different interpretations of the proper implementation, Analog Devices, Inc., has added a disable option to the ADV7511 for the HDCP 1.1 features. This option is available on ADV7511 devices with a Revision ID (Register 0x00 of the main register map) of 0x14. In previous revisions of the ADV7511, if the Rx indicated within its HDCP responses that it supported HDCP 1.1 features, the ADV7511 automatically invoked this (Pj checking) protocol. The HDCP 1.1 features disable option allows the user to disable this Pj checking with the assertion of an I2C register bit.
For users not wishing to employ this option, no changes to software or hardware are necessary.
The default setting leaves HDCP 1.1 features fully enabled so that ADV7511s with a Revision ID of 0x14 performs the same as the ADV7511s with a Revision ID of 0x12. With the new silicon, users can disable support for Pj checking.
By default, if the HDCP sink supports the HDCP 1.1 feature set, the DDC controller enables the following functions:
- Enhanced link verification (Pj checking)
- Advance cipher mode
- Enhanced encryption status signaling (EESS)
The ADV7511 now has the option to disable the HDCP 1.1 feature implementation, using the HDCP 1.1 features disable bit (Register 0xCF, Bit 0). The HDCP 1.1 feature implementation is typically only disabled in situations where there is a compatibility issue with the HDCP sink. It is not recommended to disable the feature if the HDCP sink supports it due to the enhanced security that this feature affords. In HDMI mode, the implementation of EESS is mandatory and, therefore, is enabled regardless of this bit setting. However, in DVI mode, implementation of EESS is disabled if the HDCP 1.1 features disable option is set to 1. Refer to the HDCP specification for further details regarding the implementation of the HDCP 1.1 features.
HDCP 1.1 Features ADV7511 Disable Option
The ADV7511s with a Revision ID (Register 0x00) = 0x14 can disable the HDCP 1.1 features, and the ADV7511s with a Revision ID (Register 0x00) = 0x12 cannot disable the HDCP 1.1 features.
| HDCP 1.1 Features ADV7511 Disable Option | Rev ID |
| No | 0x12 |
| Yes | 0x14 |
Pj Checking Problem Detection
When the HDCP 1.1 features are selected and an error interrupt occurs with an error code (main map, Register 0xC8, Bits[7:4]) of 0b0011, it indicates a Pj mismatch. If this occurs, it is recommended that the HDCP 1.1 features be disabled by writing 1 to Register 0xCF, Bit 0.