The future of manufacturing is smarter, faster, and more connected than ever before. As factories scale up and digitalize, the need for integrated networks that effectively manage operations and enable precise control is paramount. As today’s factories grow larger and embrace smarter technologies, it’s more important than ever to create integrated networks that keep operations running smoothly and allow for precise control. This involves collecting real-time data from every piece of equipment, analyzing it instantly, and quickly sending back control signals to optimize performance.
Integrating Networks for Smarter Operations
The ADIN6310 and ADIN3310 Industrial Ethernet Time-Sensitive Networking (TSN) switch ICs from Analog Devices, Inc. (ADI) have achieved a major milestone by becoming the first ADI products to pass the CC-Link IE TSN Recommended Network Wiring Parts Test: Switch Certification Class B and Class A from the CC-Link Partner Association (CLPA).
Why CC-Link IE TSN Matters
CC-Link is an open network specification that has enabled data communication among devices from diverse manufacturers since 2000. The CC-Link IE TSN standard, which now certifies ADI’s switches, is the Industrial Ethernet specification that brings Time-Sensitive Networking to the factory floor. TSN delivers the precise time synchronization that standard Ethernet cannot, enabling the integration of IT and OT networks by supporting a single network for both critical, real-time data and non-real-time data. This enables remote monitoring of production lines and real-time operational coordination among multiple devices, with the result of increasing productivity, efficiency, and safety. This means manufacturers can gather real-time data from every piece of equipment, analyze it instantly, and send control signals back with minimal delay. The result? Enhanced productivity, efficiency, and safety—hallmarks of the smart factory revolution.
Inside the ADIN6310 and ADIN3310: Certified for Performance
ADI’s ADIN6310 (6-port) and ADIN3310 (3-port) Industrial Ethernet TSN-compliant network switch ICs stand out for their flexible Ethernet port count and robust multi-speed operation. Both have secured CC-Link IE TSN certification for 100 Mbps and 1 Gbps connectivity, supporting core TSN functions like time synchronization, traffic scheduling, and preemption.
For system manufacturers, ADI offers evaluation boards that integrate the switch IC, PHYs, host processor, and power supply units—making it easier to design fully CC-Link IE TSN-compliant systems. These products and boards are already in mass production and shipping worldwide.
Accelerating Global Adoption of Smart Factory Standards
CLPA anticipates that this major product certification will accelerate the global adoption of CC-Link IE TSN, driving the advancement of smart factories around the world.
About the CC-Link Partner Association
Headquartered in Japan, CLPA operates through active bases in 11 regions globally. As an open network promotion organization, CLPA has pioneered the worldwide adoption of the CC-Link family, with a special focus on CC-Link IE TSN—a 1Gbps Ethernet-based industrial network that is among the first in the industry to adopt time-sensitive networking technology.
Ready to learn more?
Check out CCLink’s press release for additional details about ADI’s first-ever CC-Link IE TSN Compliance Certification. Learn more about ADI’s ADIN6310 and ADIN3310 Industrial Ethernet Time-Sensitive Networking (TSN) switch ICs.