SDARS MAX2140 XM Radio Tuner Solution
Abstract
The following note introduces the SDARS XM radio tuner solution using MAX2140, including basic RF to demodulator block, signal path from antenna to demodulator, features of the MAX2140 tuner and some critical RF specifications of an SDARS receiver.
Introduction
Satellite digital audio radio service (SDARS) is a satellite-based direct-broadcast radio service. In SDARS, digitally encoded audio entertainment material, is broadcast to earth-based receivers either directly from an orbiting satellite, or in cases in which the receiver is in a shielded location from the satellite, to the receiver via a repeater station. Maxim's MAX2140 is a complete RF to base-band SDARS receiver.
Complete SDARS Receiver MAX2140
MAX2140 complete receiver is designed for SDARS, and includes the following features:
- Integrated receiver requiring only one SAW filter
- Self-contained RF AGC Loop
- Differential I/Q interface
- Complete integrated frequency generation
- Bias supply for external LNAs
- Over-current protection
- Low power standby mode
Figure 1 shows the MAX2140 block diagram.
Figure 1. MAX2140 Block diagram/pin configuration.
XM Radio Tuner Block Diagram
An RF input to Demodulator block diagram is shown as the following Figure 2.
Figure 2. SDARS radio tuner block diagram.
- The audio signal is first received by antenna, and in order to satisfied the sensitivity requirement an external low-noise amplifier (LNA) is required, which can be controlled by a base-band controller;
- This tuner includes a self-contained RF AGC loop and baseband-controlled IF AGC loop, effectively providing a total dynamic range of over 92dB. The operation of IF AGC and RF AGC is shown as Annex A;
- Channel sensitivity is ensured by SAW filter and by on-chip monolithic low-pass filters. High-pass filters are also inserted in the back-end signal paths, which removes DC offset;
- In order to achieve sufficient image rejection, this IC includes an image reject mixer which also ensures good half IF rejection;
- The fractional-N PLL allows a very small frequency step, making possible the implementation of an AFC loop. Additionally, the reference is provided by external XTAL and on-chip oscillator. A reference buffer output is also provided.
Specifications of SDARS Tuner
1. Frequencies and Channel Bandwidth
XM is assigned 12.5MHz of spectrum range from 2332.5 to 2345MHz centered on 2338.75MHz. This spectrum is roughly divided into sixths. Four bands are assigned to the transmitting satellite and two are assigned to a terrestrial repeater network.
Figure 3. SDARS frequency bands.
2. Modulation
Satellites use QPSK modulation and Repeaters use COFDM modulation to realize the requirements of terrestrial broadcasting.
3. RF Specifications for the MAX2140
| PARAMETER | CONDITIONS | TYPICAL | UNITS |
| Frequency | SDARS Band | 2320 to 2345 | MHz |
| Channel Bandwidth | 12.5 | MHz | |
| Input Power Range | Over RF and IF AGC Range | -91 to +3 | dBm |
| Noise Figure | RF AGC is at maximum gain. IF AGC is at reference |
8.5 | dB |
| Out-of-Band Input IP3 | At Maximum Gain | -9 | dBm |
| Out-of-Band Input IP2 | At Maximum Gain | +38 | dBm |
Annex A : the operation of IF AGC and RF AGC