ADI Commercial Aviation Solutions
ADI Commercial Aviation Solutions
With its profound experience in optimizing system grade signal processing and diverse array of products, ADI is able to offer developers solutions designed exclusively for commercial aviation. ADI solutions include access to a series of related applications, such as aircraft navigation subsystems, communication subsystems, radar and monitoring subsystems, power and propulsion subsystems, and cabin entertainment subsystems.
ADI offers:
- SDR-based communication solutions
- Full signal chain radar solutions
- High temperature and scalable products
- High precision MEMS products
- Audio/video products
To Learn more about the comprehensive and flexible Analog Devices system solutions and main products,click here to get the complete solutions for free.
Enhanced Products
At present, ADI has over 100 EP products in its catalog and over 600 with nickel-palladium-gold leadframes. ADI contiues to releasing new EP devices in support of the commercial aviation market. ADI will continue to convert legacy devices to EP where practival.
• Products available with temperature ratings of –55°C to +125°C.
• Lead finishes will be NiPdAu by default or with SnPb for some
packages.
• Our EP devices will have separate data sheets.
• Controlled manufacturing baseline including one assembly site, one test site, and one fab site.
Design Resources
Circuits from the Lab® Reference Circuits for Radar and SDR
• AD-FMCOMMS6-EBZ: A 400 MHz to 4.4 GHz receiver based on the
AD9652 dual, 16-bit analog-to-digital converter, the ADL5566 high
dynamic range RF/IF dual differential amplifier, and the ADL5380
quadrature demodulator. This is an I and Q demodulation approach
to direct convert (also known as a homodyne or zero IF) receiver
architecture — wiki.analog.com/resources/eval/user-guides/
ad-fmcomms6-ebz
• AD-FMCOMMS5-EBZ: An FMC board for the AD9361, a highly
integrated RF Agile Transceiver™ , which demonstrates how to design a
platform which shows how to connect and synchronize (at the RF side)
multiple AD9361s for SIMO/MISO/SU-MIMO/MU-MIMO applications. For many broadband wireless access (BWA) systems, multi-input, multi-output (SIMO/MISO/SU-MIMO/MU-MIMO) operation and RF
beamforming are proven techniques for maximizing throughput and
efficient spectrum utilization — wiki.analog.com/resources/eval/
user-guides/ad-fmcomms5-ebz
• MEMS evaluation system — www.analog.com/en/eval-adis2
• AD-FMCDAQ2-EBZ evaluation board — www.analog.com/en/eval-ad-fmcdaq2-ebz
• More reference circuits are available at analog.com/circuits
Technical Articles/Application Notes
• Advanced Technologies Pave the Way for New Phased Array Radar
Architectures — www.analog.com/en/advanced-technologies-pave-the-way-for-new-phased-array-radar-architectures
Software-Defined Radio Solutions — www.analog.com/en/software-defined-radio-solutions-from-adi
Design Tools/Forums
If you need more ADI radar applications and products information, please visit: analog.com/en/applications/markets/aerospace-and-defense/radar.html| CUSTOMER INTERACTION CENTER Email : cic.asia@analog.com EngineerZone : ez.analog.com Free Sample : analog.com/sample |