Nanopower is a unique technology that enables single-function analog and mixed-signal ICs to consume less than 1 μA of supply current or quiescent current (IQ), resulting in dramatically reduced power consumption and increased battery life. Analog Devices’ nanoPower Technology™ products allow designers to utilize smaller batteries or extend the guaranteed product operation time between battery recharges or replacements.
Battery-powered applications continue to grow exponentially, including the vast array of Internet of Things (IoT) devices, wearables, health monitors, and field sensors. These devices push the limits of technology, requiring extended run time, less heat dissipation, and smaller form factors. Quiescent current (IQ) dominates in duty cycled systems and reducing IQ unlocks system benefits. ADI’s nanoPower Technology products operate with less than 1 μA of quiescent current, giving your system the highest performance, lowest heat dissipation, and longest operational life.
Maximize Battery Life
Typical battery-powered applications operate mostly in an idle state, waiting for something to happen. This something could be a timed event that occurs at regular intervals, or an event enabled by a user. The system takes the appropriate action, such as reading a sensor and displaying the results, then goes back into a sleep state waiting for the next event. By having ultralow current consumption in the operating and idle states, the system can function longer with smaller batteries. Consider real-world, day-to-day examples:
- A remote environmental sensor monitoring weather and air quality
- A wireless mouse is not in use but is not switched off
- A car is turned off, but the head unit is still running
Nanopower enables single-function analog and mixed-signal ICs to consume less than 1 μA of supply current or IQ while in waiting mode. Below, learn more about how nanopower ICs—from voltage regulators and supervisors to op amps and comparators—can transform your system design.

nanoPower Technology for IoT
Internet of things (IoT) sensor circuits need long lives and must often operate in the field, where they are powered by a battery or a renewable power source, such as light. Often these devices have steady, low loads combined with high power consumption peaks when measuring and transmitting data. nanoPower Technology solutions optimize both the light load and peak consumption requirements of these applications.

AI at the Edge
On-device artificial intelligence (AI) is revolutionizing machine learning. Devices that incorporate AI at the edge reduce the need for low latency timing decisions and circumvent bottlenecks in data transmission to the cloud. The challenge is that they need to operate at very low power.

Medical Applications
As healthcare extends from the hospital to the home and outside world, the needs of medical equipment change and expand. Low power measurement and communication have become critical for monitoring and delivering treatment. nanoPower Technology products preserve battery life and allow for smaller battery sizes, making equipment lighter, easier to use, and more likely to produce the right outcome.

Portable Instrumentation
Deploying personnel to take measurements in the field is time-consuming and expensive. Measurements must also be accurate the first time to avoid energy-consuming repetition. Further, portable instruments must be light and easy to carry. nanoPower Technology products resolve the dilemma of performance and power consumption with a shot-in-the-arm for creative designers who need to solve the latest technology challenges.

Consumer
Consumer devices are prime real estate for integrating nanoPower Technology. Its building block approach allows system architects and designers to select unique features and optimize overall system performance. Many nanopower products, such as supervisors and comparators, consume so little power that their inclusion in a system may be considered energy free.

Industrial Applications
Even line-powered devices benefit from nanoPower Technology with reduced heat dissipation, especially in space-constrained systems without forced cooling. Further, these systems reduce vampire power and overall system power consumption for a smaller carbon footprint.
MAXESSENTIAL02: Essential Analog Power Toolkit
This sample box allows for a hands-on evaluation of an array of power conversion solutions before purchasing a full-featured evaluation board, including LDOs, buck, boost, and buck-boost controllers with representative products from the nanopower, uSLIC™ module, and Continua™ families for line and battery-powered applications.
Key Features and Benefits
- Rapid testing and prototyping
- nanoPower Technology reduces standby (quiescent) current to nanoampere levels, extending battery life in portables and wearables
- Continua backup power solutions combine buck and boost functions to power devices from a single supercapacitor

Featured Products
Featured Videos
Extend Battery Life in Space-Constrained Applications with ADI’s Nanopower Modules
Find out more about the MAXM38643 and MAXM17225—power modules that feature the lowest quiescent current compared to competitive solutions and discover how to get started with their evaluation (EV) kits.
Nanopower Boost Converter Demo
Watch a demonstration of the extremely low quiescent current and True Shutdown™ capabilities of our nanopower boost converter using the MAX17222 EV kit.
Fundamentals of nanoPower Technology
Watch a demonstration of the extremely low quiescent current and True Shutdown™ capabilities of our nanopower boost converter using the MAX17222 EV kit.