Abstract
This document describes two firmware improvements that were applied to the Demo Code version 4.8p for Maxim's Teridian™ 71M6521 family of energy meter ICs. These improvements make transitions between power modes on the 71M6521 more reliable and support proper correction of the real-time clock (RTC) after return to mission mode. This document isolates the changes and describes details so that the updates can be retrofitted into customer firmware, if needed.
Introduction
Trim Fuses
Trim fuses are a form of nonvolatile (NV) memory used in the production of Maxim's Teridian energy metering ICs to adjust analog and digital characteristics of the ICs. After the production stage, the contents of the trim fuses cannot be changed. Some examples are the fuses used to trim the VREF voltage to within ±1mV of 1.195 VDC and the fuses used to trim the VBIAS internal voltage to the target value.
During operation of the IC, the contents of the trim fuses are read and refreshed by hardware on the IC at regular intervals, and the values obtained by the trim fuse read are provided to both the hardware controlled by the fuse values and to the fuse register locations in I/O RAM (see Figure 1). In the 71M6521 family, a total of seven individual trim fuse values can be read by first writing any number from 1 to 7 to I/O RAM register 0x20FD (TRIMSEL
) and then reading the corresponding fuse value from I/O RAM register 0x20FF (TRIM
).
Figure 1. Trim fuse mechanism.
Misread of the Trim Fuses
The 71M6521 ICs support three low-power modes (sleep mode, LCD only mode, and brownout mode). In the low-power modes, regular operating currents are not available to the IC.
Extreme electromagnetic interference (EMI) or severe and repeated disruptions of the supply voltage can sometimes affect the trim read/refresh cycle, resulting in the IC misreading one of its trim fuses. If this occurs, a number of failures can result. The likelihood of potential failures is increased when the power supply rapidly "oscillates" the 71M6521 between mission and brownout modes, which can occur when the AC mains voltage is ramped up or down slowly in conjunction with a "soft" power supply. This oscillation causes the 71M6521 to switch rapidly and repeatedly between regular current consumption (mission mode) and low current consumption (brownout mode). Failures based on trim fuse misreads are extremely rare and can only be seen when large numbers of meters are power-cycled over days or weeks.
IC failures caused by a misread of the trim fuses can cause various symptoms, depending on which trim fuse read is affected. Symptoms include the following:
- Unexpected MPU software execution. Depending on the firmware, the unpredictable software execution can in some instances cause the internal clock to stop, preventing the watchdog timer from resetting the meter.
- Unexpected changes to internal power supply voltages and detection thresholds. This failure could cause the external power supply voltage applied to the V1 pin to be misread, causing an unexpected transition to sleep mode when the wake timer has not been set. In some instances, operating with an improperly initialized internal power supply for an extended period of time can corrupt the RTC.
Eliminating all EMI in a meter is not practical, but firmware can detect and avoid the above issues by testing the trim fuses of the IC when it enters brownout mode.
Another issue addressed by this new demo code version is faulty RTC drift correction. Older codes contained RTC code that integrated long term jitter into the RTC's drift correction after reset.
Application Cases for the Improved Code
The code described in this application note should be used for all versions of the 71M6521, including the 71M6521BE, 71M6521DE, and 71M6521FE. Maxim recommends including the firmware correction in all existing designs that contain batteries, and in all new designs.
Possible Failure Events at Power Mode Transition
Trim fuses are read by the fuse logic in the 71M6521 in a loop. Extensive repeated power mode transitions and severe EMI could occasionally affect the proper function of the trim fuse read. The failure mechanism is as follows:
- The meter undergoes multiple power transitions or EMI events in rapid succession.
- A trim fuse misread can occur on a mission-to-brownout mode transition in meters with a new lithium bat-tery. The fact that the battery voltage (typically 3.6 VDC) is different from the regular operating voltage of the 71M6521 (typically 3.3 VDC) contributes to the failure.
- Meters equipped with batteries tend to be affected to a larger degree. This is because a meter without a battery is off when no mains voltage is present and experiences a clean power-on-reset (POR) when the mains voltage returns.
- After the power mode transition, the failure symptoms described above could occur. The exact form of a failure is unpredictable and intermittent, because it depends on the nature of the power disruption or EMI, the firmware of the meter, the battery selection, the power supply design, and on the exact trim fuse that is affected by the misread. Most meter designs exhibit no symptoms, even in extensive qualification.
- When the meter returns to mission mode, higher operating currents are available, and the trim values self-correct from the fuse refresh. However, the meter state may be corrupted.
The RTC Failure Event
The RTC code adjusts the time to compensate for the drift while the meter was in low-power mode. However, the adjustment is not synchronized to the start of a second, and therefore accumulates jitter into the drift.
Details of Demo Code Revision 4.8p
Testing of the Code
A practical test is to attach new batteries to the meter of demo board, set the display defaults to display a clock value from the RTC, then cycle AC power every 10 seconds for eight meter-weeks. The meters can be tested by briefly stabilizing the power supply to nominal AC voltage. Successful code will resume operation and display a reasonable clock time. Code that passes eight meter-weeks is unlikely to fail in full qualification. New code should be checked at increasing intervals, starting with a half meter-hour.
Code Side Effects
Demo Code Revision 4.8p enables the PLL_OK interrupt very early, before running main(). This assures that a brownout mode transition during firmware initialization will be tested and handled. Other interrupts must be carefully managed to avoid creating spurious failures.
Demo Code Revision 4.8p also keeps a nonzero value in the wake timer at all times. In mission mode, the wake timer value does not count or cause an event unless the IC unexpectedly enters sleep or LCD only mode. In that case, the wake timer will trigger, waking the meter, and recover the IC from the error. This method may affect code that depends on using a zero reset value of the wake timer.
Code Location
The linker should be commanded to put the corrective code in the first 8KB of flash memory. In the Keil® IDE, the linker command can be changed by hovering the mouse over the project workspace, and by then selecting <right click>options
BL_51 Locate Tab
Code Space. In the demo code, this command puts the segments as low in memory as possible:
?C_C51STARTUP,?PR?_?PLL_ISR?BATMODES_20,?PR?_?BATMODE_CHANGE?BATMODES_20, <rest of the link commands for code space>
?C_C51STARTUP is the segment that contains the demo code's startup code.
?PR?_?PLL_ISR?BATMODES_20SAFE,?PR?_?BATMODE_CHANGE?BATMODES_20SAFE are the segments needed to run the demo code's PLL_OK interrupt routine.
PLL_OK Interrupt
The following code should be placed in the PLL_OK interrupt routine, which runs when brownout mode is detected. A tested copy of the code is in 4.8p in main\batmodes_20.c
extern void trim_test(void) small reentrant; EA = 0; CONFIG0 = 0; // Make sure we are running as fast as we can. IFLAGS = (~IE_PLLFALL_) & (~IE_PLLRISE_); // force an edge to occur WAKE = 0x81; // force a wake timer wake if sleep is forced trim_test(); // From start-up code.
Startup Code
The following startup code should be used in place of startup.a51. A tested copy of the code is available from Maxim (in the version 4.8p code build, the startup code can be found in util\startup_n_safe.a51). The code listing is provided on the following pages.
When this code first runs in the factory, it copies the trim registers to a location in flash memory. After that, it tests the trim registers. When the test fails, it forces a reread of the trim values by briefly putting the IC to sleep mode. After the wake occurs, the trim fuses are automatically read again. Calling the fuse test during reset assures that even in severe EMI situations, the trim fuses will be reread until they are correct.
;/*************************************************************************** ; * This code and information is provided "as is" without warranty of any * ; * kind, either expressed or implied, including but not limited to the * ; * implied warranties of merchantability and/or fitness for a particular * ; * purpose. * ; * * ; * Copyright (C) 2011 Maxim Integrated All Rights Reserved. * ; ***************************************************************************/ ;//************************************************************************** ;// ;// DESCRIPTION: 71M652x POWER METER - STARTUP Code. ;// ;//************************************************************************** ;// ;// File: STARTUP_N_SAFE.A51. ;// $NOMOD51 ;------------------------------------------------------------------------------ ; This file is part of the C51 Compiler package ; Copyright (c) 1988-2002 Keil Elektronik GmbH and Keil Software, Inc. ;------------------------------------------------------------------------------ ; STARTUP.A51: This code is executed after processor reset. ; ; To translate this file use A51 with the following invocation: ; ; A51 STARTUP_N_SAFE.A51 ; ; To link the modified STARTUP_N_SAFE.OBJ file to your application use the following ; BL51 invocation: ; ; BL51 <your object file list>, STARTUP_N_SAFE.OBJ <controls> ; ;------------------------------------------------------------------------------ ; ; User-defined Power-On Initialization of Memory ; With the following EQU statements the initialization of memory ; at processor reset can be defined: ; ; ; the absolute start-address of IDATA memory is always 0 IDATALEN EQU 100H ; the length of IDATA memory in bytes. ; XDATASTART EQU 0H ; the absolute start-address of XDATA memory XDATALEN EQU 000H ; the length of XDATA memory in bytes. ; PDATASTART EQU 0H ; the absolute start-address of PDATA memory PDATALEN EQU 0H ; the length of PDATA memory in bytes. ; ; Notes: The IDATA space overlaps physically the DATA and BIT areas of the ; 8051 CPU. At minimum the memory space occupied from the C51 ; run-time routines must be set to zero. ;------------------------------------------------------------------------------ ; ; Reentrant Stack Initialization ; ; The following EQU statements define the stack pointer for reentrant ; functions and initialized it: ; ; Stack Space for reentrant functions in the SMALL model. IBPSTACK EQU 1 ; set to 1 if small reentrant is used. IBPSTACKTOP EQU 0FFH+1 ; set top of stack to highest location+1. ; ; Stack Space for reentrant functions in the LARGE model. XBPSTACK EQU 0 ; set to 1 if large reentrant is used. XBPSTACKTOP EQU 07FFH+1; set top of stack to highest location+1. ; ; Stack Space for reentrant functions in the COMPACT model. PBPSTACK EQU 0 ; set to 1 if compact reentrant is used. PBPSTACKTOP EQU 07FFH+1; set top of stack to highest location+1. ; ;------------------------------------------------------------------------------ ; Page Definition for Using the Compact Model with 64 KByte xdata RAM ; ; The following EQU statements define the xdata page used for pdata ; variables. The EQU PPAGE must conform with the PPAGE control used ; in the linker invocation. ; PPAGEENABLE EQU 1 ; set to 1 if pdata object are used. ; PPAGE EQU 7 ; define PPAGE number. PUBLIC PPAGE_SFR PPAGE_SFR DATA 0BFH ; SFR that supplies uppermost address byte ; (most 8051 variants use P2 as uppermost address byte) ;------------------------------------------------------------------------------ ; Switch to M6520 when chip is available. ; Standard SFR Symbols ACC DATA 0E0H B DATA 0F0H SP DATA 81H DPL DATA 82H DPH DATA 83H USER1 DATA 90H DIR1 DATA 91H FCTRL DATA 0B2H IPH DATA 0B9H IPL DATA 0A9H IRCON DATA 0C0H IEN0 DATA 0A8H IEN1 DATA 0B8H NAME ?C_STARTUP ?C_C51STARTUP SEGMENT CODE ?STACK SEGMENT IDATA RSEG ?STACK DS 1 EXTRN CODE (?C_START) PUBLIC ?C_STARTUP PUBLIC _?TRIM_TEST CSEG AT 0 ?C_STARTUP: LJMP STARTUP1 RSEG ?C_C51STARTUP STARTUP1: CLR IEN0^7 ; Disable interrupts ; To enable secure mode, remove the semicolon of the next line ; ORL FCTRL,#40H ; set secure bit MOV 0E8h,#0FFh ; Refresh nonmaskable watchdog. ; Set system interrupt priorities; more frequent are higher priority. MOV IPH,#01DH ; From code in options_gbl.h, main.c MOV IPL,#00AH ; From code in options_gbl.h ; Clear PLL_OK interrupt (bit3), and others MOV IRCON,#0 ; Enable PLL_OK interrupt MOV DPTR,#2007H ; Set EX_PLL MOV A,#20H MOVX @DPTR,A ; Enable interrupts MOV IEN1,#08H ; Enable INT4, the PLL_OK interrupt MOV IEN0,#80H ; Enable all interrupts ACALL _?TRIM_TEST ; Test 6521's trims IF IDATALEN <> 0 MOV R0,#IDATALEN - 1 CLR A IDATALOOP: MOV @R0,A DJNZ R0,IDATALOOP ENDIF IF XDATALEN <> 0 MOV DPTR,#XDATASTART MOV R7,#LOW (XDATALEN) IF (LOW (XDATALEN)) <> 0 MOV R6,#(HIGH (XDATALEN)) +1 ELSE MOV R6,#HIGH (XDATALEN) ENDIF CLR A XDATALOOP: MOVX @DPTR,A INC DPTR DJNZ R7,XDATALOOP DJNZ R6,XDATALOOP ENDIF IF PPAGEENABLE <> 0 MOV PPAGE_SFR,#PPAGE ENDIF IF PDATALEN <> 0 MOV R0,#LOW (PDATASTART) MOV R7,#LOW (PDATALEN) CLR A PDATALOOP: MOVX @R0,A INC R0 DJNZ R7,PDATALOOP ENDIF IF IBPSTACK <> 0 EXTRN DATA (?C_IBP) MOV ?C_IBP,#LOW IBPSTACKTOP ENDIF IF XBPSTACK <> 0 EXTRN DATA (?C_XBP) MOV ?C_XBP,#HIGH XBPSTACKTOP MOV ?C_XBP+1,#LOW XBPSTACKTOP ENDIF IF PBPSTACK <> 0 EXTRN DATA (?C_PBP) MOV ?C_PBP,#LOW PBPSTACKTOP ENDIF MOV SP,#?STACK-1 LJMP ?C_START ; Read a trim whose index is in A. Return the trim in A. CSEG AT 100H FUSE_TABLE: DB 0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff ; Trim test. Prefix "_?" tells Keil C it's reentrant. _?TRIM_TEST: PUSH IEN0 PUSH PSW ; Save registers, so it's reentrant. MOV PSW,00H ; Select registers before saving them PUSH DPL PUSH DPH PUSH ACC MOV A,R7 ; Save R7 from the current register set. PUSH ACC MOV A,R6 ; Save R6 from the current register set. PUSH ACC CLR IEN0.7 ; Wait for all fuses to be read once before checking fuses ; Complete fuse read takes 45 xtal clock cycles (1 fuse per xtal clock) MOV R7,#21 ; Wait 21x4 = 48 cycles loop_inner: DJNZ R7,loop_inner ; 4 cycles (in brownout, 1 cycle/clk) mov DPH, #HIGH(FUSE_TABLE) fuse_test_frst: ; check if values previously stored mov DPL,#LOW(FUSE_TABLE) clr a movc a,@a+dptr ; read fuse table xrl a,#55H jnz fuse_save MOV DPTR,#2003H ; Check if in brownout mode MOVX A,@DPTR JB ACC.6,PASS ; Mission mode, so don't check. fuse_test: mov r7,#8 ; byte counter fuse_test_lp1: mov DPTR,#FUSE_TABLE ; load pointer to fuse table mov a,r7 movc a,@a+dptr ; read fuse table mov r6,a mov a,r7 MOV DPTR,#20FDH ; TRIMSEL address MOVX @DPTR,A ; load reg to read trim MOV DPL,#0FFH ; TRIM value address MOVX A,@DPTR ; Get trim value cjne a,06H,FAIL ; test if flash read and trim == djnz r7,fuse_test_lp1 JMP PASS fuse_save: MOV DPTR,#2003H ; Check if in brownout mode MOVX A,@DPTR ; If brownout mode, don't save them and enter sleep. JNB ACC.6,FAIL ; mov 84H,#LOW(FUSE_TABLE) mov r7,#8 ; byte counter fuse_save_lp1: mov a,r7 MOV DPTR,#20FDH ; TRIMSEL address MOVX @DPTR,A ; load reg to read trim MOV DPL,#0FFH ; TRIM value address MOVX A,@DPTR ; Get trim value mov r6,a mov a,r7 mov dptr,#FUSE_TABLE add a,DPL mov DPL,a mov a,r6 orl 0B2H,#01H ; set to flash write movx @dptr,a ; write fuse table byte djnz r7,fuse_save_lp1 mov a,#55H ; control byte to mark mov dptr,#FUSE_TABLE orl 0B2H,#01H ; set to flash write movx @dptr,a ; write fuse table byte jmp PASS FAIL: MOV DPTR,#20A9H ; WAKE address MOV A,#0C1H ; SLEEP forces wake and fuse re-read MOVX @DPTR,A PASS: CLR A ; Select 0 MOV DPTR,#20FDH ; TRIMSEL address MOVX @DPTR,A ; clear trim select register. POP ACC MOV R6,A ; Restore R7 in this register set POP ACC MOV R7,A ; Restore R7 in this register set POP ACC POP DPH POP DPL POP PSW ; Restore registers, so it's reentrant. POP IEN0 RET END
RTC Code
At reset, the code should not adjust the clock to correct for the drift during sleep mode. The code that sets the clock after calculating the drift should be removed.