AN-2555: True Bipolar Input, Fully Differential Output, ADC Driver Design
Introduction
Precision signal chains used in data acquisition and general-purpose test and measurement equipment must accommodate a wide range of input levels. The signal chain may need to offer high input impedance, support both gain and attenuation, and adjust the common-mode level to ensure that the signal falls within the appropriate input range for the ADC. The schematic in Figure 1 illustrates two-stage signal conditioning that scales and level shifts a differential, bipolar ±10 V signal to a fully differential ±4.096 V signal with a 2.048 V common-mode level required by the ADC. The design goal is to achieve this conditioning while not degrading the ADC noise and distortion performance. The ADC driver typically needs to have supply voltages that exceed the input range of the ADC, to allow for input and output swing voltage headroom. The driver usually must scale and shift the first stage output voltage to match the input voltage range of the ADC (or example, changing a true bipolar differential signal into a differential signal that swings from ground to VREF).
The schematic in Figure 1 was created from LTspice®, a high performance SPICE III simulator, schematic capture, and waveform viewer with enhancements and models for easing the simulation of switching regulator, linear, and signal chain circuits. For additional information about the devices shown in Figure 1, see the LTC6373, ADA4945-1, and LTC2387-18 data sheets.

KEY DESIGN SPECIFICATIONS
For a true bipolar input signal range of ±10 V, the key design specifications are listed in Table 1. For a differential, ±10 V peak sinewave, this circuit outputs a ±4.096 V differential output signal.
| Parameter | Value |
| Input Differential | ±10 V |
| Output Differential | ±4.096 V |
| Output Common-Mode Voltage (VOCM) | 2.048 V |
| +VS/−Vs Supplies | ±15 V, +5 V/−1 V |
| ADC Fully Differential | 18 bits |
| Reference Voltage (VREF) | 4.096 V |
| Input Frequency Range | 0 kHz to 100 kHz |
| Total Harmonic Distortion (THD) | −117 dB |
| Single-to-Noise Ratio (SNR) | 95.7 dB |
DESIGN DESCRIPTION
The circuit is an ADC driver circuit that has a very high input impedance and can be tailored to drive a wide range of input voltages, both single-ended and differential. The output signal of the circuit is capable of driving ADCs with less than 30 ns acquisition times. The circuit accomplishes this while maintaining optimal noise and distortion performance. The circuit in Figure 1 is composed of the LTC6373 programmable gain-instrumentation amplifier as the input stage, the ADA4945-1 fully differential amplifier (FDA) as the second stage ADC driver, and the LTC2387-18, an 18-bit, 15 MSPS ADC. Additionally, there is a 100 kHz filter between the LTC6373 output and the ADA4945-1 input to reduce noise and a glitch suppression/noise reduction filter between the ADA4945-1 output and the LTC2387-18 input. The LTC6373 is configured as a differential-to-differential amplifier with a gain of 0.5 and output common-mode voltage of 2.048 V. The ADA4945-1 is configured as an attenuating differential-to-differential driver with a gain of 0.8. The ADA4945-1 has an output common-mode voltage of 2.048 V to be compatible with the LTC2387-18 input range. The LTC2387-18 has an input signal range of 0 V to 4.096 V at each input, resulting in a differential input signal range of ±4.096 V when using its internal 4.096 V reference.
DESIGN TIPS
If greater or less signal range is necessary, the gain of the LTC6373 and the ratio of RF/RG can be changed. For example, if a ±100 mV signal range is required, RF can be increased while keeping RG at its original value. The following formula can be used to recalculate RF:

where:


Because of the greater gain bandwidth of the ADA4945-1, it is recommended to increase its gain rather than the LTC6373.
The filters composed of R5, C6, R6, and C7 reduce the bandwidth of the ADA4945-1. The lower bandwidth results in lower noise at the LTC2387-18 input. The values of C6 and C7 were experimentally determined by gradually increasing the value until the SNR stopped improving.
The filter composed of Resistors R7 and R8 and Capacitors C4 and C5 helps to isolate the ADA4945-1 output from the sampling glitches generated by the ADC inputs if they are not buffered. It limits the bandwidth of the signal provided to the ADC inputs and helps to reduce the noise seen at the ADC inputs.
If the filter between the driver and ADC does not have time to settle, the result is a gain error. Depending on the application, a small gain error may be tolerable but the inability to settle can also cause distortion, which must be avoided. The Precision ADC Driver Tool can be used to check filter settling and estimate circuit SNR and THD performance.
DESIGN PROCEDURE
Initial Conditions and Assumptions
The power supplies for the LTC6373 are set at ±15 V and the power supplies for the ADA4945-1 are set at +5 V/−1 V. Given the input range of 20 V p-p (±10 V) and the output range of 8.192 V p-p (into the ADC), the total gain distributed across the analog front end (AFE) is as follows:

Allowing some headroom to accommodate component tolerances and a small variation in common mode, the total gain target is set at 0.4 V/V. The LTC6373 supports a fixed selection of gain values: {0.25, 0.5, 1, 2, ..., 16}. Selecting the gain of both stages to be < 1 allows the use of the smaller power supply range for the ADA4945-1 and lowers the noise gain of each stage. Setting the gain of the LTC6373 to 0.5 results in a gain of 0.8 for the ADA4945-1.
The common mode for both the LTC6373 and ADA4945-1 is set to 2.048 V.

-
For the ADC (LTC2387-18), set the full scale input of ±4.096 V with VREF = 4.096 V and ±VFS = ±4.096 V.
-
Set the driver amplifier (ADA4945-1) VOCM.
VOCM is biased to 4.096 V/2 = 2.048 V. Check this against the data sheet output common-mode requirement.

For this application,

where VOCM is within the allowed range. VOCM is supplied by the VOCM pin of the LTC2387-18.
-
Set the input amplifier (LTC6373) input and output limits.
Because the gain is set to 0.5, the output swing is

The output swing is

For the reversed signal polarity, the value of ±DIN is simply reversed (0.452 V, −4.548 V).
Figure 3 shows the input and output swing limits for the LTC6373 with a gain of 0.5. Looking at the VS = ±15 V curve, it can be seen that with an input common-mode voltage of 2.048 V and an output differential voltage swinging between ±4.548 V, the LTC6373 is easily capable of supporting this application. However, if ±5 V supplies are used, the LTC6373 may operate outside of its differential output voltage range. The common-mode range vs. differential output voltage curves for all LTC6373 gains are available in the data sheet.
The VOCM of the LTC6373 is also set to 2.048 V using the VOCM pin of the LTC2387-18 to eliminate having to generate another bias point.

Figure 3. Input Common Mode Range vs. Differential Output Voltage -
Set the amplifier gain as follows:

For this application,

For optimal noise, the ADA4945-1 data sheet recommends 499 Ω for RF and RG in a unity-gain setup. In this instance, RG is scaled to 402 Ω for the desired gain. RG is composed of the 49.9 Ω and 453 Ω resistors. If THD is more important than SNR, 2 kΩ can be used for RG and 1.62 kΩ for RF with a potential 3dB improvement in THD at the expense of 4 dB in SNR.
-
Set the driver amplifier (ADA4945-1) output swing.
Because the driver amplifier has a differential output swinging about VOCM, when observing +VFS, the op amp outputs are reversed voltages for −VFS. The VREF (4.096 V) is used for the range, even though the actual maximum range is limited to 4 V by the circuit gain. The ADA4945-1 outputs must be able to swing from 0.0 V to 4.096 V for this application.

For VOUTdm = +VFS,

-
Check the driver amplifier (ADA4945-1) output voltage swing against the data sheet requirements for the supply rails.
According to the ADA4945-1 data sheet at 1 kΩ load,

For this application,

-
Set the driver amplifier (ADA4945-1) input swing.
For VOUTdm = +VFS, compute the input common mode voltage as follows:

For VOUTdm = −VFS, compute the input common mode voltage as follows:

The ADA4945-1 inputs must be able to swing from 2.02 V to 2.07 V for this application.
-
Check the driver amplifier (ADA4945-1) input common mode.
According to the ADA4945-1 data sheet,

Data sheet requirements are met.
For this application,

Application requirements are met.
DESIGN SIMULATIONS
The Precision ADC Driver Tool provides a specialized simulation environment where the engineer can quickly determine the impact of the drive amplifier and R-C filter selection on the overall performance of an ADC signal chain.
Using the Precision ADC Driver Tool as shown in Figure 4, settling time, noise, and THD performance are estimated. The Precision ADC Driver Tool does not currently allow the LTC6373 to be added to the schematic. Therefore, only the ADA4945-1 performance driving the LTC2387-18 is simulated. The driver tool suggests the minimum supply voltages to be +4.6 V and −0.5 V. The driver tool warns that the driver selected significantly degrades the overall noise performance. RF and RG are the largest contributors to driver noise. The driver tool does not allow capacitors to be added across RF as in the application shown. The capacitors reduce driver noise. The summary of design goals vs. simulated results is shown in Table 2.
| Parameter | Design Goal | Simulation |
| SNR THD |
95.7 dB −117 dB |
91.9 dB −116 dB |

MEASURED RESULTS
The measured ADC SNR performance is 0.4 dB lower than the ADA4945-1 data sheet typical specification of −95.7 dB, and the THD performance is 3.8 dB lower than the data sheet typical specification of −117 dB, as shown in Figure 5.

The summary of design goals vs. simulated results is shown in Table 3. THD performance can potentially be improved by up to 3 dB by increasing the ADA4945-1 RG to 2 kΩ and RF to 1.62 kΩ. This increase results in a degradation of SNR performance by 4 dB according to the ADC driver tool. It is up to the user to determine whether THD or SNR performance is more important. All data taken is at a 14 MSPS data rate. At 15 MSPS, THD is degraded significantly due to the small ADC acquisition period.
| Parameter | Design Goal | Measured |
| SNR THD |
95.7 dB −117 dB |
95.3 dB −113.2 dB |
As shown in Figure 6, THD exceeds −100 dB when the input frequency goes above 15 kHz. SNR goes below 90 dB when the input frequency goes above 90 kHz. This data was taken at 25°C. At lower or higher temperatures, performance may start to degrade earlier. Variations in circuit processing may also result in a different voltage where performance starts to degrade.

DESIGN DEVICES
| Parameter | Value |
| Input Offset Voltage Maximum | 50 μV |
| Bias Current Maximum | −2.5 μA |
| Gain Bandwidth Product Typical | 145 MHz |
| Noise Voltage Typical | 5 nV/√Hz |
| Quiescent Current per Amplifier Typical | 180 μA |
| Supply Voltage Span Minimum/Maximum | 3 V/10 V |
| Parameter | Value |
| Input Offset Voltage Maximum | 464 μV |
| Bias Current Maximum | 0.0005 μA |
| Gain Bandwidth Product Typical | 7 MHz |
| Noise Voltage Typical | 26.4 nV/√Hz |
| Quiescent Current per Amplifier Typical | 4.4 mA |
| Supply Voltage Span Minimum/Maximum | 9 V/36 V |
| Parameter | Value |
| Resolution | 20 bits |
| Sampling Frequency Maximum | 1 MSPS |
| Input Type (Single-Ended or Differential) | Fully differential |
| VIN Span VMIN/VMAX | 5 V |
| SNR Typical | 104 dB |
| THD Typical | −125 dB |
| Data Interface (I2C, Serial Peripheral Interface (SPI), Parallel) | SPI |