Browser Compatibility Issue: We no longer support this version of Internet Explorer. For optimal site performance we recommend you update your browser to the latest version.Update Microsoft Internet Explorer
APR 2018
VOL 52
ADALM1000 SMU Training Topic 4: Transient Response of RC Circuit
Formats the Html codes.FormatFix the Html to be XHtml compliantFix
Write
Validate that the text is XHtml compliant.Validate
Proofing
After the introduction of the SMU ADALM1000 in our Analog Dialogue December 2017 article, we want to continue with the fourth part of our series with some small, basic measurements. You can find the first ADALM1000 article here.
Figure 1. A schematic of the ADALM1000.
Now let’s get started with the next experiment.
Objective:
The objective of this lab activity is to study the transient response of a series RC circuit and understand the time constant concept using pulse waveforms.
Background:
In this lab activity, you will apply a pulse waveform to the RC circuit to analyze the transient response of the circuit. The pulse width relative to a circuit’s time constant determines how it is affected by an RC circuit.
Time Constant (τ): A measure of time required for certain changes in voltages and currents in RC and RL circuits. Generally, after four time constants (4 τ), the capacitor in the RC circuit is virtually fully charged and the voltage across the capacitor is now approximatively at 98% of its maximum value. This interval is considered to be the transient response of the circuit. When the elapsed time exceeds five time constants (5 τ) after switching has occurred, the currents and voltages have reached their final value, which is also called steady-state response.
Table 1 shows the voltage and current percentage values for the capacitor in the RC charging circuit at a given time constant while charging.
Table 1. Voltage and Current Percentage Values for Given Time Constant
Time Constant (τ)
Percentage of Maximum
Voltage
Current
0.5 τ
39.3%
60.7%
0.7 τ
50.3%
49.7%
τ
63.2%
36.8%
2 τ
86.5%
13.5%
3 τ
95.0%
5.0%
4 τ
98.2%
1.8%
5 τ
99.3%
0.7%
Note that the capacitor will never become 100% charged in reality. Therefore, five time constants are used to consider a capacitor fully charged for all practical purposes.
The time constant of an RC circuit is the product of equivalent capacitance and the Thévenin resistance as viewed from the terminals of the equivalent capacitor.
A pulse is a voltage or current that changes from one level to another and back again. If a waveform’s high time equals its low time it is called a square wave. The length of each cycle of a pulse is its period (T).
The pulse width (tp) of an ideal square wave is equal to half the time period.
The relation between pulse width and frequency is then given by,
Figure 2. Series RC circuit.
From Kirchhoff’s laws, it can be shown that the charging voltage VC (t) across the capacitor is given by:
where V is the applied source voltage to the circuit for τ = 0, and RC = τ is the time constant.
The response curve increases and is shown in Figure 3.
Figure 3. Capacitor charging for series RC circuit to a step input with time axis normalized by τ.
The discharge voltage for the capacitor is given by:
Where Vo is the initial voltage stored in capacitor at t = 0, and RC = τ is time constant. The response curve is a decaying exponential as shown in Figure 4.
Figure 4. Capacitor discharging for series RC circuit.
Materials:
ADALM1000 hardware module
Resistors (2.2 kΩ, 10 kΩ)
Capacitors (1 μF, 0.01 μF)
Procedure:
Set up the circuit shown in Figure 5 on your solderless breadboard with the component values R1 = 2.2 kΩ and C1 = 1 μF. Open the ALICE Oscilloscope software.
Set the Channel A arbitrary waveform generator (AWG) Min value to 0.5 V and the Max value to 4.5 V to apply a 4 V p-p square wave centered on 2.5 V as the input voltage to the circuit. From the AWG A Mode drop down menu, select the SVMI mode. From the AWG A Shape drop down menus select Square. From the AWG B Mode drop down menu, select the Hi-Z mode.
Figure 5. Breadboard diagram of an RC circuit.
Figure 6. Breadboard connections for RC circuit R1 = 2.2 kΩ and C1 = 1 μF.
From the ALICE Curves drop down menu, select CA-V and CB-V for display. From the Trigger drop down menu, select CA-V and Auto Level. Adjust the time base until you have at approximately two cycles of the square wave on the display grid.
Figure 7. Oscilloscope configuration.
This configuration uses the oscilloscope to look at the input of the circuit on Channel A and the output of the circuit on Channel B. Make sure you have checked the Sync AWG selector.
Observe the response of the circuit for the following three cases and record the results.
Pulse width » 5 τ: Set the frequency of AWG A output such that the
capacitor has enough time to fully charge and discharge during each
cycle of the square wave. Let the pulse width be 15 τ and set the
frequency according to Equation 2. The value you have found should
be approximately 15 Hz. Determine the time constant from the
waveforms obtained on the screen if you can. If you cannot obtain
the time constant easily, explain possible reasons.
Pulse width = 5 τ: Set the frequency such that the pulse
width = 5 τ (this should be approximately 45 Hz). Since the pulse
width is 5 τ, the capacitor should just be able to fully charge and
discharge during each pulse cycle (see Figure 3 and Figure 4).
Figure 8. Measuring the time constant t approximately by counting the number of squares.
Pulse width « 5 τ: In this case the capacitor does not have time to charge significantly before it is switched to discharge, and vice versa. Let the pulse width be only 1.0 τ in this case and set the frequency accordingly.
Repeat the procedure using R1 = 10 kΩ and C1 = 0.01 μF and record the measurements.
Questions:
Calculate the time constant (τ) using Equation 1 and compare it to the measured value from 4b (R = 2.2 kΩ and C = 0.01 μF).
Repeat this for another set of values, R = 10 kΩ and C = 0.01 μF.
As in all the ALM labs, we use the following terminology when referring to the connections to the ALM1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the ADALM1000 analog I/O connector. The analog I/O channel pins are referred to as CA and CB. When configured to force voltage/measure current, –V is added (as in CA-V) or when configured to force current/measure voltage, –I is added (as in CA-I). When a channel is configured in the high impedance mode to only measure voltage, –H is added (as in CA-H).
Scope traces are similarly referred to by channel and voltage/current, such as CA-V and CB-V for the voltage waveforms, and CA-I and CB-I for the current waveforms.
We are using the ALICE Rev 1.1 software for those examples here.
Note: You need to have the ADALM1000 connected to your PC to use the software.
Figure 9. ALICE desktop 1.1 menu.
Authors
Doug Mercer
Doug Mercer received his B.S.E.E. degree from Rensselaer Polytechnic Institute (RPI) in 1977. Since joining Analog Devices in 1977, he has contributed directly or indirectly to more than 30 data converter products and holds 13 patents. He was appointed to the position of ADI Fellow in 1995. In 2009, he transitioned from full-time work and has continued consulting at ADI as a fellow emeritus contributing to the Active Learning Program. In 2016, he was named engineer in residence within the ECSE department at RPI.
Antoniu Miclaus
Antoniu Miclaus is a software engineer at Analog Devices, where he works on embedded software for Linux and no-OS drivers, as well as ADI academic programs, QA automation, and process management. He started working at ADI in February 2017 in Cluj-Napoca, Romania. He holds an M.Sc. degree in software engineering from the Babes-Bolyai University and a B.Eng. degree in electronics and telecommunications from the Technical University of Cluj-Napoca.