How to Build an Uninterruptible Power Supply for Home Devices

QUESTION:

How can you use Wi-Fi and other at-home devices during a power outage?

How to Build an Uninterruptible Power Supply for Home Devices

Answer:

Design a home uninterruptible power supply (UPS) by using a car battery as a backup power source. This is connected to a buck-boost converter that generates a stable 12 V/5 A supply to power the Wi-Fi router, as well as a 6.5 V/1.5 A buck converter to power a cordless telephone.

Introduction

As the world becomes more advanced, our dependence on electricity becomes more acute. Power outages can reduce the most sophisticated homes to quite primitive ones and this article describes the design of an uninterruptible power supply for the home that keeps alive the home’s most essential service: Wi-Fi.

An Uninterruptible Power Supply (UPS) for the Home

The circuit in Figure 1 was designed out of necessity. With the threat of an energy crisis looming in early 2022 and world peace on a knife’s edge, it was designed to keep home Wi-Fi alive in the case of a power outage. While this might be seen as a First World problem, it takes over 2 minutes for the average Wi-Fi router to reboot, and this can seem like an eternity if the power disappears in the middle of a conference call. Even minor dips can cause major problems. This home uninterruptible power supply design provides a 12 V/5 A power supply for the Wi-Fi access point (and any other electronics) and an additional 6.5 V/1.5 A supply for a cordless telephone. This is enough to keep most laptops communicating with the outside world.

Figure 1. The uninterruptible power supply (UPS) schematic.

Figure 1 shows the circuit. The backup power source for this design was a preloved car battery purchased from a scrapyard for £20. The LTC3789 is a four switch buck-boost converter that provides a constant 12 V supply, with extremely high efficiency, from an input that could be above or below this voltage. Its evaluation kit provides 12 V at 5 A from a 5 V to 36 V input voltage, so it could be used with no modification. Since the Wi-Fi router only needed 1 A, this evaluation kit could be used to power many other applications that require 12 V.

The cordless telephone required 6.5 V at about 600 mA, so the LT8608 was chosen to provide this rail with low noise and high efficiency with an extremely low quiescent current of 2.5 μA. The LT8608 and LTC3789 have maximum input voltages of 42 V and 38 V, respectively, so they were connected directly to the car battery for the highest circuit efficiency. Some lower cost battery chargers can generate high voltages if they are not connected to the battery correctly, so the battery does not adequately absorb the charging current. Therefore, if the charger has a good connection to the circuit, but a poor connection to the battery, a voltage can be generated that might damage the electronics. The wide input voltage range of the LTC3789 and the LT8608 alleviated concern of high voltages being generated when the battery charger was connected. The circuit can be operated either with the battery charger permanently connected or not. However, the safety aspect of keeping the battery charger permanently connected in an unventilated room depends on the type of the battery and charger used.

The clever part of the circuit was provided by the LTC4416. This is a dual ideal diode and was responsible for switching between the main supply voltages and the backup supplies. The LTC4416 contains a precision comparator that detects when the main supply has failed and switches over to its backup supply using four external P-channel MOSFETs (PFETs).

A simpler form of this circuit is a dual diode OR configuration where the cathodes of two diodes are joined and the main and backup supplies are connected to the anodes. However, this circuit only feeds the highest of the two supplies to the output at the cathode as well as incurring a loss of 0.6 V across the diode. A more efficient circuit can be designed using PFETs to replace the diodes. The voltage drop across the body diode of the PFET is measured and if this exceeds a certain threshold, the FET is switched on, thus shorting out the body diode. If this voltage drop goes negative, the drive to the PFET is removed and the body diode blocks the reverse current; thus, an ideal diode has been created that has a low forward voltage drop and blocking in the reverse direction. This is shown in Figure 2.

Figure 2. An ideal diode implementation of the diode OR circuit.

With this circuit, the body diode of each PFET points from the input to the output, so if one input voltage is higher than the other by more than 600 mV, this body diode will conduct. Therefore, if the backup supply happens to be higher than the main supply, the load’s power will be supplied by the backup supply, which is undesirable. Reversing the PFET stops this problem, but then the body diode conducts if the output voltage is higher than the input voltage by more than 600 mV.

A cleaner solution is to add an additional PFET to each path as shown in Figure 3. In this circuit, the two body diodes oppose each other so this circuit provides a bidirectional open circuit when the FETs are switched off and isolates each channel regardless of the input or output voltages.

Figure 3. A diode OR circuit with bidirectional disconnect.

For the 12 V circuit, the evaluation kit of the LTC4416 (DC1059A) was modified to give a switch over voltage of 11.17 V, using a 100 kΩ resistor for R3 and a 10 kΩ + 2.2 kΩ resistor for R1. This worked well, but it was found that the Wi-Fi access point needed a precise 12 V supply and sometimes it rebooted when the main 12 V was switched back on again. This was due to the voltage step (from 11.17 V to 12 V) upsetting the router electronics. Changing R1 to 11.47 kΩ increased the switch over voltage to 11.8 V, thus decreasing the step size.

The cordless telephone circuit was much more sympathetic to power supply steps, so R15 comprised of a 22 kΩ + 10 kΩ resistor, giving a switch over voltage of 5 V.

The waveforms can be seen in Figure 4. The green trace shows the always on 12 V output from the LTC4416, the red trace shows the 12 V output from the wall cube, and the blue trace shows the car battery voltage. The disturbance to the green trace could not be seen when the oscilloscope was DC coupled. Changing to AC coupling shows little disturbance when the mains 12 V is connected (at 600 ms) and disconnected (at 5.8 s). Ironically, the noise on this rail was significantly higher when the mains 12 V was connected, showing that the noise from the wall cube output was higher than that from the LTC3789.

Figure 4. 12 V (green trace) is hardly disturbed when the mains (red trace) is disconnected.

A photograph of the UPS electronics is shown in Figure 5 with the complete circuit shown in Figure 6.

Figure 5. The power supplies and ideal diodes mounted to the side of the UPS box.
Figure 6. The complete circuit with a battery.

Future Modifications

The circuits previously mentioned require the cables from the wall cubes to be cut to allow the UPS to be inserted in series. A neater solution would be to generate, say, 340 V DC from the car battery and feed this into an extension socket, then plug the wall cubes into the extension socket. Since the circuitry inside all wall cubes contains a rectifier, it would not matter if this voltage was AC or DC. However, the losses incurred in generating 340 V from a 12 V battery as well as the losses incurred in reducing that voltage down inside the wall cube meant that a low voltage circuit would be far more efficient and simpler, even if it did mean cutting the wall cube cables.

The LTC4416 evaluation kits included LEDs to indicate whether the main or backup power supply was being used and these could easily be brought to the outside casing. Another useful addition would be a push button switch to artificially pull the LTC4416’s enable pins low to test the switch over functionality.

The circuit was tested extensively and found to give excellent performance. For higher currents, N-channel ideal diodes are available. The LTC4416 is part of a wide range of ideal diodes and hot swap devices available from Analog Devices.

Conclusion

The circuit described in this article illustrates the design of a simple home uninterruptible power supply that can be built to keep various home appliances alive in the event of a power failure. There is no reason why this circuit cannot be modified to use more powerful MOSFETs and a larger battery to give an increased output power and a longer backup life.

Author

Simon Bramble

Simon Bramble

Simon Bramble graduated from Brunel University in London in 1991 with a degree in electrical engineering and electronics, specializing in analog electronics and power. He has spent his career in analog electronics and worked at Maxim and Linear Technology (both now part of Analog Devices).