AN-1536: ADuM4135 Gate Driver Performance Driving APTMC120AM20CT1AG SiC Power Switches
Introduction
In solar photovoltaics (PV) and energy storage applications, there is a trend towards increased power density, along with the ever present need of improved efficiency. A solution to this problem comes in the form of silicon carbide (SiC) power devices. SiC devices are wide band-gap devices that can operate at an increased voltage of >1000 V dc and tend to have a low drain source impedance (RDSON). SiC devices also fill the need for reduced conduction and, therefore, increased efficiency. SiC devices can also exhibit fast switching speeds of >100 kHz with low parasitic capacitance and associated charge during switching. However, disadvantages include a requirement for higher common-mode transient immunity (CMTI) greater than 100 kV/μs required for gate drivers. Another disadvantage is that higher switching across the drain source of the SiC can lead to ringing at the gate of the device. These disadvantages can cause problems when driving higher voltage SiC devices, where significant power density improvement can be achieved by their implementation. One combination of gate driver and SiC that can solve these problems is the ADuM4135 and the Microsemi APTMC120AM20CT1AG module. The ADuM4135 gate driver is a single-channel device with a typical drive capability of 7 A source and sink at a 25 V operating voltage (VDD to VSS). It has a minimum CMTI of 100 kV/μs. The APTMC120AM20CT1AG power module is a half bridge SiC device with a 1200 V collector emitter voltage rating, RDSON of 17 mΩ, and a continuous current capability of 108 A. Its gate source voltage (VGS) rating is −10 V to +25 V.
Test Setup
Electrical Setup
The system test circuit setup is shown in Figure 2. A dc voltage is applied to the inputs across the full half bridge, where a decoupling capacitor of 900 µF is added to the input stage. The output stage is an inductor capacitor (LC) filter stage of 83 µH and 128 µF, filtering the output into the load, R1, of 2 Ω to 30 Ω.
Table 1 shows a list of the test setup power components. A physical setup is shown in Figure 3, and Table 2 details the setup equipment used for testing.
| Equipment | Value |
| U1 | 200 V to 900 V |
| C1 | 900 μF |
| L1 | 83 μH |
| C2 | 128 μF |
| R1 | 2 Ω to 30 Ω |
| Equipment | Manufacturer | Type |
| Oscilloscope | Keysight | DSO-X 3024T |
| DC Supply | Delta Elektronika | SM 660-AR-11 (two in serial) |
| Gate Driver Board | Watt&Well | ADUM4135-WW-MS-01 SN001 |
| Waveform Generator | Agilent | 33522A |
| Current Probe | Hioki | 3275 |
| Passive Voltage Probe | Keysight | N2873A 500 MHz |
| Passive High Voltage Probe | Elditest | GE3421 100 MHz |
Test Result
No Load Testing
| Test | VHV (V)1 | Switching Frequency, fSW (kHz) | Duty Cycle (%) | IIN (A)2 | Figures |
| 1 | 600 | 50 | 50 | 0.26 | Figure 4 and Figure 5 |
| 2 | 600 | 100 | 50 | 0.22 | Figure 6 and Figure 7 |
| 3 | 900 | 50 | 50 | 0.37 | Figure 8 and Figure 9 |
1 VHV is the differential voltage between HV+ and HV−.
2 IIN is the input current through U1.
| Test | VHV (V) | fSW (kHz) | Ambient Temperature (°C) | Heatsink Temperature (°C) | DC-to-DC Power Supply Temperature, High-Side (°C) | DC-to-DC Power Supply Temperature, Low-Side (°C) | Gate Driver Temperature, High-Side (°C) | Gate Driver Temperature, Low-Side (°C) |
| 4 | 600 | 50 | 20 | 21.3 | 25.4 | 25.4 | 34 | 33.5 |
| 5 | 600 | 100 | 20 | 23.5 | 31.5 | 31.5 | 42 | 42 |
| 6 | 900 | 50 | 20 | 23 | 29 | 29 | 37 | 37 |
In the latest revision of ADuM4135, some changes include: a capacitor of 2.2 nF was added on the gates of the power metal oxide semiconductor field effect transistors (MOSFETs), Q1, and Q2. C0G decoupling capacitors of 15 nF have been added to VHV. Table 3 and Table 4 summarize of the results observed, and Figure 4 through Figure 9 show the proof of results. Test 1 and Test 2 were carried out at 600 V, respectively, at 50 kHz and 100 kHz switching frequencies, whereas Test 3 was carried out at 900 V at a switching frequency of 50 kHz.
Load Testing
| Test | VHV (V) | fSW (kHz) | Duty Cycle (%) | IOUT1 (A) | VOUT2 (V) | POUT3 (W) | IIN4 (A) |
Figures |
| 4 | 200 | 50 | 25 | 1.7 | 48 | 83 | 0.55 | Figure 10 and Figure 11 |
| 5 | 600 | 50 | 25 | 6.9 | 145 | 1000 | 1.66 | Figure 12 and Figure 13 |
| 6 | 900 | 50 | 25 | 8.7 | 215 | 1870.5 | 2.47 | Figure 14 and Figure 15 |
| 7 | 900 | 100 | 25 | 8.2 | 200 | 1640 | 2.13 | Figure 16 and Figure 17 |
1 IOUT is the output current in Load Resistor R1.
2 VOUT is the output voltage across R1.
3 POUT is the output power (IOUT × VOUT).
4 IIN is the input current through U1.
Board configuration is similar to the test setup of the No Load Testing section.
Table 5 is a summary of the results observed for load testing, and Figure 10 through Figure 17 show the proof of results.
Output voltage (VOUT) was measured as the voltage across R1. The test results show some Miller feedback on VGS, but VGS remains at the −5 V level at the gate of the SiC. At 900 V, some ringing is seen on VDS, but it is <100 V of the input dc voltage. This design shows how the ADuM4135 can drive SiC MOSFETs with clean performance.
High Current Testing
| Test | VHV (V) | fSW (kHz) | Duty Cycle (%)1 | IOUT2 (A) | VOUT3 (V) | PIN4 (W) | IIN5 (A) | Figures |
| 4 | 300 | 50 | 25 | 21.8 | 70.14 | 1526 | 5 | Figure 18 and Figure 19 |
| 5 | 400 | 50 | 25 | 27.1 | 93.8 | 2640 | 6.6 | Figure 20 and Figure 21 |
| 6 | 600 | 50 | 25 | 40.5 | 141 | 6000 | 10 | Figure 22 and Figure 23 |
1 Duty cycle high side.
2 IOUT is the output current in Load Resistor R1.
3 VOUT is the output voltage across R1.
4 PIN is the input power (IIN × VHV).
5 IIN is the input current through U1.
Board configuration is similar to the test setup of the No Load Testing section. A Regatron power supply was used in this test.
Table 6 is a summary of the results observed for high current testing, and Figure 18 through Figure 23 show the proof of results.
VOUT was measured as the voltage across R1.

PWM Delay
The ADuM4135 input and output PWM measures the delay between the two signals. The measures have been made directly on the input and output pins of the ADuM4135. The delay is to 59.4 ns.
Schematic
Conclusion
The ADuM4135 gate driver has the current drive capability, the correct power supply range, and a strong CMTI capability of >100 kV/µs to deliver clean performance when driving SiC MOSFETs.
The test results provide data showing a solution is available for isolated power supply, high voltage gate drivers driving SiC.