Design and Layout of Planar RF Front Ends for X/Ku Band Phased Array Radars
Integrated beam-former ICs (BFICSs) are making it easier to design planar RF front ends for phased array radar systems. The appeal of a design where RF electronics and patch antennas are located on opposite sides of the same PCB is obvious. While BFICs and integrated TR modules can ease layout challenges, the task is still far from trivial due to the physical bounds imposed by the lattice spacing of lambda over two. On the simulation side, large element counts challenge traditional approaches and require improved speed and accuracy of modeling.
Using real-world design and simulation examples, this webcast will focus on challenges such as RF amplifier biasing and sequencing, circuit layout, thermal management, power management, part-to-part performance variations and calibration. The webcast will also highlight how Analog Devices’ hardware and Keysight’s Pathwave design software can simplify and de-risk the prototyping process.
-
Joel Dobler
joel.dobler@analog.com
产品应用工程师
Joel Dobler于2006年加入ADI公司,在俄勒冈州Beaverton市的西北实验室作为RF产品工程实习生工作。他于2005年获得华盛顿州立大学电气工程学士学位(BSEE),并于2007年获得波特兰州立大学电气工程硕士学位(MSEE)。从2007年至2010年,他一直担任产品工程师。从2010年开始,他一直担任RF应用工程师,为各种RF产品提供支持,包括可变增益放大器、可编程低通滤波器以及RF和光学探测器。他目前在航空航天与防务部门工作,负责为波束成形、矢量调制器和可编程低通滤波器产品提供支持。
-
Weston Sapia
weston.sapia@analog.com
Weston Sapia是位于美国科罗拉多州斯普林斯市的ADI公司的高级RF应用工程师。最初,他在凌力尔特公司工作,负责所有的RF混频器产品。自加入ADI公司后,他主要负责未来毫米波成像产品。2010年,Weston毕业于圣路易斯奥比斯波的加州理工州立大学,获得电气工程学士学位。主要从事模拟和RF产品工作。