This installer contains USB drivers that are both 32- and 64-bit compatible. Note: Older AD9520 evaluation boards will need to have the USB controller EEPROM re-flashed in order to use this driver.
This handy tool will automatically calculate divider values based on the user’s input/output frequencies, as well as assist with designing the loop filter based on the user’s parameters. Be sure to install the MATLAB runtime installer first.
Note: The USB driver requires 32-bit Windows XP (or a 32-bit Windows XP virtual machine). However, the software can be run in standalone mode on newer versions of Windows.