ADI公司与英特尔携手开发应对5G网络设计挑战的无线电平台

2020-08-04 - 中国,北京
  • Analog Devices Collaborates with Intel on Radio Platform for Addressing 5G Network Design ChallengesAnalog Devices, Inc. (ADI) 宣布与 英特尔公司 携手开发应对5G网络设计挑战的灵活无线电平台,这款平台有助于客户以更低的成本更迅速地扩展其5G网络规模。新型无线电平台集成了ADI射频(RF)收发器的先进技术和英特尔Arria 10现场可编程门阵列(FPGA)的高性能和低功耗特性,为开发人员提供了一套新的设计工具,使其能够更轻松地创建优化的5G解决方案。

    随着人们越来越多地采用数字化方式进行商业活动,以及随时随地获取和传输数据,通信市场也在加速发展,以应对带宽和延迟方面的挑战。私有网络和公共空间的现有无线网络流量显著增加,因此无线网络运营商希望能够缩短开发时间,同时以经济高效的方式实现可提高5G网络容量、性能和可靠性的新型解决方案。通过结合开放标准和现有通信链路,移动网络运营商正在制定一套更加广泛的技术规范,同时支持越来越多的用例。

    ADI公司无线通信事业部副总裁Joe Barry表示:"这款新型无线电平台可降低设计总成本,并缩短客户的产品上市时间,同时又不会降低系统性能。通过集成ADI收发器所具有的先进数字前端(DFE)功能和英特尔的领先FPGA技术,我们能够满足客户对解决方案的高性能要求,同时提高其灵活性,以更高效地方式解决新出现的网络问题。"

    这款符合O-RAN规范的高性能解决方案采用了ADI领先的软件定义收发器(包括创新的DFE功能)以及英特尔的Arria A10 FPGA,以创建高度灵活的架构。通过此次协作,使设计人员能够进行频率、频段和功率定制,从而以更低的成本实现更高的系统性能。

    英特尔可编程解决方案事业部无线接入业务主管、高级总监CC Chong表示:"ADI与英特尔的此次协作有助于开发适用于5G网络的新型无线电解决方案。我们非常期待与ADI公司合作,通过提供FPGA平台加快硬件的开发。FPGA平台易于使用,可满足不断变化的需求,并且能够解决射频和数字化产品开发的许多复杂问题。"

  • 关于ADI公司
    • Analog Devices (Nasdaq: ADI)是全球领先的高性能半导体公司,致力于解决艰巨的工程设计挑战。凭借杰出的检测、测量、电源、连接和解译技术,搭建连接现实世界和数字世界的智能化桥梁,从而帮助客户重新认识周围的世界。
      详情请浏览ADI官网 www.analog.com/cn 。


  • Intel、Intel标志、Xeon和Arria是英特尔公司或其子公司的商标 。

    This release may be deemed to contain forward-looking statements intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, among other things, our statements regarding the expected opportunities, benefits, cost savings, product and service offerings and developments associated with the collaboration between Analog Devices, Inc. and Intel Corporation relating to the new radio platform that addresses 5G network challenges, that are based on current expectations, beliefs, assumptions, estimates, forecasts, and projections about the industry and markets in which the companies operate. The statements contained in this release are not guarantees of future performance, are inherently uncertain, involve certain risks, uncertainties, and assumptions that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed in such forward-looking statements, and such statements should not be relied upon as representing Analog Devices' expectations or beliefs as of any date subsequent to the date of this press release. Important factors that could cause actual results to differ materially from the results described, implied or projected in any forward-looking statements include difficulty or delay in our design, development, production and marketing of products, technologies and solutions, including those associated with the collaboration between Analog Devices and Intel, the course, impacts and uncertainty of the COVID-19 global pandemic, and other risk factors described in the most recent filings of Analog Devices with the Securities and Exchange Commission. Analog Devices does not undertake any obligation to update forward-looking statements made by us.


  • 联络方式