ADP8860SHIELD-EVALZ
Overview
Features and Benefits
- Arduino compatible
- Backlight array
- Keypad backlight array
- Ambient light sensor
- Dedicated reset button
- Dedicated header for I2C communications
Product Details
The ADP8860SHIELD-EVALZ and the ADP8861SHIELD-EVALZ incorporate light emitting diodes (LEDs) for quick and easy evaluation of the ADP8860 and the ADP8861. Note that only the ADP8860SHIELD-EVALZ has dual light intensity sensors. The ADP8860SHIELD-EVALZ and the ADP8861SHIELD-EVALZ follow the form factor of a regular Arduino® shield to allow compatibility with microcontroller boards that use the same interface. These evaluation boards also incorporate a separate header dedicated to I2C communications.
The ADP8860 and the ADP8861 are 7-channel LED drivers that utilizes a charge pump with selective gain for maximum efficiency. The LEDs driven by either device are programmable for maximum current and fade in and out times via the I2C interface. Only the ADP8860 has a programable light intensity threshold that can be set via the I2C interface of the device. Each channel can handle up to 30 mA (typical), except for the seventh channel, which can handle 60 mA (typical). Each channel can be unified to have the same fade in time and fade out time, or each channel can have an individual fade in time and fade out time for greater flexibility.
For full details on the ADP8860 and the ADP8861, see the ADP8860 and the ADP8861 data sheets, which should be consulted in conjunction with the user guide when using these evaluation boards.
Markets and Technologies
Applicable Parts
Getting Started
EQUIPMENT NEEDED
- Micro USB to USB cable
- EV-COG-AD3029LZ and EV-GEAR-EXPANDER1Z
- Windows 7 or Windows 10 PC
- EV-COG-BLEINTP1Z (optional)