对增益大于等于10时保持稳定的放大器进行补偿以在较低增益下工作

本文说明如何补偿一个增益为9倍以上时通常保持稳定的放大器(如 ADA4895-2,以使其在增益低至2时工作,提供比等效内部补偿放大器更高的压摆率和更快的建立时间。本文将提出两种方法并突出每种电路的优缺点。

ADA4895-2与ADA4896-2, ADA4897-1, 和 ADA4897-2同属一个系列,是一款双通道、低噪声、高速、电压反馈、轨到轨输出型放大器。它在增益为10时可保持稳定,增益带宽积为1.5 GHz,压摆率为940 V/µs,0.1%建立时间为26 ns,10 Hz时1/f噪声为2 nV/√Hz,宽带噪声为1 nV/√Hz,2 MHz时无杂散动态范围为−72 dBc。这款器件采用3 V至10 V电源供电,每个放大器的静态功耗为3 µA。

Figure 1
图1. 方法1:补偿ADA4895-2实现增益为+2时保持稳定

方法1如图1所示,在反相输入端增加一个简单的RC电路(RC = 28 Ω 且 CC = 56 pF) ,且反馈电阻并联一个反馈电容(CF = 5 pF)。该电路在高频时的噪声增益为+9,在谐振频率(1/2πRCCC = 100 MHz)以下的频率时噪声增益为+2。虽然高频时的噪声增益接近+9,但只要由RO 和 CL构成的低通滤波器能够阻隔高频成分,总输出噪声就能保持在低水平。这种情况下,放大器可以在增益为+2时工作,而总输出噪声则非常低(3.9 nV/√Hz)。

可以扩展这种配置以支持+2到+9之间的任何增益。表1显示了各种增益设置的元件值和总宽带输出噪声

表1. 用于增益低于+10的元件值, RT = RO = 49.9 Ω.
增益 RC (Ω) CC (pF) RG (Ω) RF (Ω) CL (pF)  总输出噪声1 (nV/√Hz)
+2 28.6 56 200 200 330 3.88
+3
33.3 56
100 200
270 5.24
+4
40 56
66.7 200
200 6.60
+5
50 56
50 200
150 7.96
+6
66.7 40 40 200
150
9.32
+7
113 30 37.5 226 120 10.82
+8
225 20 32.1 226 120
12.18
+9
N/A N/A 31.1 249 100 13.67
1完整的总噪声公式见下文。
Figure 2
图2. 方法2:补偿ADA4895-2实现增益为+2时保持稳定

方法2如图2所示,在反相输入端与同相输入端之间增加一个电阻(R1 = 28 Ω) ,将放大器的噪声增益提高到+9。R1上无电压,因而无电流通过其中。因此,R1 与同相输入端并联所得的输入阻抗仍然非常高。输入至输出信号增益等于1 + RF/RG,本例中即为+2。补偿电路未使用电容,因而不存在频率依赖性。这意味着,与第一种方法相比,低频时的宽带输出噪声始终较高。

可以扩展这种配置以支持+2到+9之间的任何增益。表2显示了各种增益设置的元件值和总宽带输出噪声。

表2. 用于增益低于+10的元件值, RT = RO = 49.9 Ω, CL = 120 pF.
增益 R1 (Ω) RG (Ω) RF (Ω) 总输出噪声1 (nV/√Hz)
+2 28.6 200 200 13.39
+3 33.3 100 200 13.39
+4 40 66.5 200 13.39
+5 49.9 49.9 200 13.39
+6 66.5 40 200 13.39
+7 113 37.4 226 13.53
+8 225 32.4 226 13.53
+9 N/A 30.9 249 13.67
1完整的总噪声公式见下文。

图3显示了图1和图2所示电路的小信号和大信号频率响应,采用50 Ω分析仪,G = +5 V/V或14 dB。如图所示,两个电路均非常稳定,峰化略高于1 dB。只要使用表1和表2中的值,增益范围在+2至+9时均可保持稳定。

为降低总输出噪声,可以调整输出端的低通RC滤波器以将此电路的带宽降至50 MHz或更低,具体取决于应用。

Figure 3
图3. G = +5时的频率响应

为什么方法1中的输出噪声优于方法2中的输出噪声?

方法1中的输出噪声远低于方法2,尤其是在增益低于+7时,这是因为方法1中的噪声增益仅在高频时较高。高频时,可以利用低通滤波器来消除高频噪声成分。但在方法2中,放大器始终在噪声增益为+9时工作,即便在低频时亦如此。因此,总输出噪声不随增益而变化,如表2所示。下面是这两种方法对应的公式(注意:RE = RG//R1).

方法1的公式:总输出噪声=

Equation 1

方法2的公式:总输出噪声 =

Equation 2

每种方法的优缺点

我们给出了两种不同的方法,说明如何利用若干外部元件来使高增益稳定型放大器能在低增益下稳定地工作。与方法2相比,方法1采用了更多的无源元件,因而可能会占用更多的电路板空间,成本更高。作为回报,第一种电路的总输出噪声低于第二种电路。因此,选择何种电路取决于具体应用及其要求的规格。

如图4所示,与增益大于等于+1时保持稳定的内部补偿放大器ADA4897-2相比,去补偿的ADA4895-2提供更高的压摆率(300 V/µs对100 V/µs)和更快的建立时间。随着电路增益提高,这些优势还会扩大。

Figure 4
图4. G = +2时对比补偿与去补偿放大器

结论

ADA4895-2去补偿放大器在增益大于9时保持稳定,可以通过补偿来实现低增益工作。本文提出的两种方法通过提高复杂度来降低总宽带噪声。与增益大于等于+1时保持稳定的内部补偿放大器ADA4897-2相比,两种方法均能提供更高的压摆率和更快的建立时间。

I invite you to comment on amplifier compensation in the Analog Dialogue Community on EngineerZone.


作者

charly-el-khoury-new

Charly El-Khoury

Charly El-Khoury是ADI公司高速产品部门的一名应用工程师。2007年2月加入ADI公司,负责低噪声、低失真放大器和精密ADC驱动器产品。他拥有伍斯特理工学院的电气与计算机工程(MSECE)学硕士学位。