2008年8月第42卷 阻抗测量监控血液凝固 引言 ADI公司是生物医学诊断学院(BDI)3的合作伙伴。BDI是爱尔兰科学基金会4资助的科学、工程与技术中心,是一家致力于开发下一代生物医学诊断设备的多学科研究机构。在BDI整体计划的其中一项中,ADI公司正与都柏林大学5以及一家全球专业制药与药物输注公司合作开发一种凝固监控设备,用于在重症监护环境下的病人治疗。该系统将提供有关病人凝血状况的快速、自动化信息,提高病人安全、流程以及决策支持水平,从而改善病人治疗结果。 血液凝固的电子测量 通过监控凝血样本的整个阻抗,可以测量与凝血形成有关的传导率变化。为了评估仪器性能,根据数据确定的凝血时间要与临床测量的凝血时间这个“黄金标准”进行相关比较。 利用AD5933进行阻抗测量
图1. 阻抗测量系统功能框图 AD5933的功能框图展示了完全集成的阻抗测量系统。本地数字处理支持测试电路的复数阻抗计算。这个系统要求初始校准:用一个精密电阻替代被测量的阻抗,并计算出后面测量的比例系数。对于1 kHz~100 kHz的激励频率,AD5933可以测量100 Ω~10 MΩ之间的阻抗,系统精度为0.5%。 血液凝固与阻抗变化的相互关系已经确定很长时间,详见文献9,10,11,12,13。不过,最近推出了复数阻抗测量的集成器件,这意味着测量凝血时间的仪器可以小型化。它在节能、便携性、仪器外观方面具有重大的优势,这在重症监护设备中是需要重点考虑的因素。 单电源器件,如AD5933,通常信号摆幅的中心在固定直流偏置值附近。在大多数阻抗测量中,这不是一个需要着重考虑的问题,但当直流电压超过特定门限值时,会使水导电媒质在与电极接触时发生电化学反应,从而改变样本。在当前利用AD5933进行血样测量项目中,为了防止出现这种电解反应,电压激励和电流测量都采用交流耦合,使用如图2所示的信号调理电路。
图2. 具有输出信号调理功能的AD5933 血液凝固测量系统
图3. 阻抗测量系统示意图,系统包含被测血样的聚合体微通道。系统允许血样与调节凝血的特定试剂相互作用,并在血样与AD5933测试仪器之间创建一个接口。 测量阻抗响应
图4. 未凝固(黑色)与凝固(红色)血样的阻抗比较 图5的阻抗响应曲线说明,随着血样中肝磷脂浓度的增加,血液凝固时间也随着增加。图中箭头表示不同血样的凝血时间。
图5.凝血时间增加时的阻抗比较:从最短(蓝色)到最长(黑色) 通过上面介绍的系统,对大量临床捐赠血样的凝固时间进行了测量,并利用临床黄金标准测量系统对血样抽样的凝固时间进行测量,对两种测量结果进行相关对比(图6)。
图6. 利用AD5933测量系统测量的凝固时间与临床黄金标准测量的凝固时间的相关对比, 结束语 致谢 参考文献 2Kost, Gerald, J., ed. Principles and Practice of Point-of-Care Testing. Lippincott, Williams and Wilkins. 2002. 3www.bdi.ie 4www.sfi.ie 5www.dcu.ie 6Guest, M.M. “Circulatory Effects of Blood Clotting, Fibrinolysis, and Related Hemostatic Processes.” Handbook of Physiology, Circulation III, American Physiological Society. Washington, DC. 1964. 7Brummel-Siedins, K., T. Orfeo, Jenny N. Swords, S.J. Everse, and K.G. Mann. “Blood Coagulation and Fibrinolysis.” Chapter 21 in Wintrobe’s Clinical Hematology. 11th edition. Volume 1. M.M. Wintrobe and J.P. Greer, eds. Lippincott, Williams, and Wilkins. 2004. 8ADI website: www.analog.com (Search) AD5933 (Go) 9Ur, A. “Changes in the electrical impedance of blood during coagulation.” Nature 226. 1970a. 269–270. 10Ur, A. “Determination of blood coagulation using impedance measurements.” Biomedical Engineering 5 (7). 1970b. 342–345. 11Ur, A. “Detection of clot retraction through changes of the electrical impedance of blood during coagulation.” American Journal of Clinical Pathology 56 (6). 1971. 713–717. 12Ur, A. “Analysis and interpretation of the impedance blood coagulation curve.” American Journal of Clinical Pathology 67 (5). 1977. 470–476. 13Theiss, W. and A. Ulmer. “Comparative and direct measurement of the electrical impedance in blood coagulation.” Thrombosis Research 13. 1978. 751–765.
Copyright 1995-
Analog
Devices, Inc. All rights reserved. |
||||||||