![]() |
|
| Home Analog Devices Feedback Subscribe Archives 简体中文 日本語 | |
|
|
|
|
Detecting and Distinguishing Cardiac Pacing Artifacts When heart patients with implanted pacemakers undergo electrocardiogram (ECG) testing, a cardiologist must be able to detect the presence and effects of the pacemaker. The electrical signature—or artifacts—of the pacing signal consists of small, narrow pulses. Buried in noise and larger cardiac signals, these artifacts can be difficult to detect. This article describes the nature of pacing artifacts and introduces a device and methodology to detect them. The heart, a biochemical-electromechanical system, develops an electrical impulse that travels from the sinoatrial (SA) node in the upper right atrium to the atrioventricular (AV) node. The SA node acts as the pacemaker for the system (Figure 1).
Figure 1. Heart muscle showing SA (1) and AV (2) nodes.1 This electrical impulse generates the P wave, which can be seen on the ECG capture in Figure 2. From the AV node, the electrical signal propagates, via the His-Purkinje system, to the ventricles, causing the ventricle muscles to contract. Their contraction (the R wave) moves oxygenated blood from the left ventricle into and through the body—and deoxygenated blood from the right ventricle to the lungs.
Figure 2. Graphical ECG representation of electrical action during heart muscle contractions.2 When the electrical system doesn’t work perfectly, many different heart conditions can occur. For example, bradycardia occurs when the heart beats too slowly or misses beats. A typical surgical intervention for this condition would be to implant a pacemaker device (pulse generator) just under the skin of the patient’s chest, with endocardial leads routed through the veins directly to the heart, as shown in Figure 3.
Figure 3. Positions of implanted pacemaker and leads for different types of pacemakers In another class of arrhythmias, called tachycardia, the heart beats too fast. This very serious condition is treated with implantable cardiac defibrillators (ICDs). Modern ICDs can also treat many bradycardia arrhythmias. Heart failure can occur when the heart becomes enlarged, lengthening its conduction paths and upsetting the timing of the ventricular contractions. This forms a positive feedback system, further aggravating the heart. Implantable cardiac resynchronization (ICR) devices retime the ventricles by pacing both ventricles and usually one atrium. These devices actually improve cardiac output, allowing the heart to recover to a certain degree. Cardiac resynchronization therapy (CRT) devices include an ICD as part of the system. A CRT device is seen in the fluoroscopic image of Figure 4(a). This is the image that physicians use to place the leads. Such images are difficult for lay persons to interpret. You can see a light outline of the heart—a static view of a beating heart. It is lying on the right atrium with the apex of the heart pointing to the right and downward. In this typical lead placement, the black arrow points to the right atrium lead. The dashed black arrow points to the right ventricle lead. The partially seen lead, indicated by the red arrow, is the left ventricle lead (the red arrow points to the tip of the electrode). Figure 4(b) shows a fluoroscopy image of typical lead placement for a dual-chamber pacemaker. The right atrium lead is pointing up and is placed in the right atrium. The right ventricle lead is positioned at the apex of the right ventricle.
Figure 4. Fluoroscopy images showing pacemaker lead placement.3 Implantable pacemakers (Figure 5) are typically lightweight and compact. They contain the circuitry necessary to monitor the electrical activity of the heart through implanted leads and to stimulate the heart muscle when required to ensure a regular heartbeat. Pacemakers must be low-power devices, as they operate with a small battery that typically has a 10-year lifespan. As of 2010, the National Academy of Engineering states that over 400,000 pacemakers are implanted in patients every year.4
Figure 5. Example of a pacemaker device.5 Pacing Artifacts Their small amplitude, narrow width, and varying wave shape make pacing artifacts very difficult to detect, especially in the presence of electrical noise that can be many times their amplitude. Furthermore, pacing therapy has become extremely advanced, with dozens of pacing modes available—from single-chamber pacing to three-chamber pacing. To further complicate the detection of pacing artifacts, pacemakers produce lead-integrity pulses, minute-ventilation (MV) pulses, telemetry signals, and other signals that can be incorrectly identified as pacing artifacts. The use of real-time pacemaker telemetry has made the display of pacing artifacts on an ECG strip less important than it used to be, but an individual skilled in pacing therapies can look at the strip to infer the type of pacing therapy being administered to the patient and determine whether the pacemaker is working properly. In addition, all pertinent medical standards, including the following, require the display of pacing artifacts. They do vary somewhat in their specific requirements regarding the height and width of the pacer signal that needs to be captured.
For example, IEC60601-2-27 states: Equipment shall be capable of displaying the ECG signal in the presence of pacemaker pulses with amplitudes of ±2 mV to ±700 mV and durations of 0.5 ms to 2.0 ms. An indication of the pacemaker pulse shall be visible on the display with an amplitude of no less than 0.2 mV referred to input (RTI); whereas, AAMI EC11 states: The device shall have the capability of displaying the ECG signal in the presence of pacemaker pulses with amplitudes between 2 mV and 250 mV, durations between 0.1 ms and 2.0 ms, a rise time of less than 100 µs, and a frequency of 100 pulses/minute. For pacemaker pulses having durations between 0.5 ms and 2.0 ms (and amplitude, rise time, and frequency parameters as specified above), an indication of the pacemaker pulse shall be visible on the recording; this indication shall be visible on the display with an amplitude of at least 0.2 mV RTI. These may be subtle differences, but they’re differences nonetheless, in terms of the heights and widths to be captured. How Pacemakers Pace In unipolar pacing, the pacing leads consist of an electrode at the tip of a single pacing lead and the metal wall of the pacemaker housing (can) itself, so just one lead is inserted into the heart. The pacing artifacts caused by this mode of pacing can be several hundred millivolts at the skin surface with a width of a couple of milliseconds. Unipolar pacing is no longer commonly used. In bipolar pacing, the heart is paced from the electrode at the tip of the pacing lead. The return electrode is a ring electrode located very close to the tip electrode. Most pacing artifacts are now created by bipolar pacing. The artifacts produced by this type of lead are much smaller than those produced by unipolar pacing; pulses on the skin surface can be as small as a few hundred microvolts high and 25 μs wide, with average artifacts 1 mV high and 500 μs wide. The amplitude of the artifact can be much smaller when the detection vector does not line up directly with the pacing lead vector. Many pacemakers can be programmed for pulse widths as short as 25 μs, but these settings are typically used only in pacemaker threshold tests performed in an electrophysiology laboratory. Setting the lower limit to 100 μs eliminates the problem of falsely detecting minute ventilation (MV) and lead integrity (LV lead) pulses as valid pacing artifacts. These subthreshold pulses are usually programmed to be between 10 μs and 50 μs. Various types of available pacemakers pace different chambers:
Pacing Artifact Waveforms Figure 6 shows an example of an ideal pacing artifact. The positive pulse has a fast rising edge. After the pulse reaches its maximum amplitude, a capacitive droop follows, and then the trailing edge occurs. The artifact then changes polarity for the recharge portion of the pacing pulse. This recharge pulse is required so that the heart tissue is left with a net-zero charge. With a monophasic pulse, ions would build up around the electrodes, creating a dc charge that could lead to necropsy of the heart tissue.
Figure 6. Ideal pacing artifact. Introducing cardiac resynchronization devices adds another degree of complication in detecting and displaying pacing artifacts. These devices pace the patient in the right atrium and both ventricles. The pulses in the two ventricles can fall close together, overlap, or occur at exactly the same time; and the left ventricle can even be paced before the right ventricle. Currently, most devices pace both ventricles at the same time, but studies have shown that adjusting the timing will benefit most patients by yielding a higher cardiac output. Detecting and displaying both pulses separately is not always possible, and many times they will appear as a single pulse on the ECG electrodes. If both pulses occur at the same time, with the leads oriented in opposite directions, the pulses could actually cancel each other out on the skin surface. The probability of this occurring is very remote, but one can envision the appearance of two ventricle pacing artifacts on the skin surface with opposite polarities. If the two pulses were offset by a small time interval, the resulting pulse shape could be very complex. Figure 7 shows scope traces of a cardiac resynchronization device pacing in a saline tank. This is a standard test environment for pacemaker validation; it is believed to be similar to the conductivity of the human body. The close proximity of the scope probes to the pacing leads causes the amplitudes to be much larger than what would be expected on the skin surface. In addition, the low impedance presented by the saline solution to the ECG electrodes results in much less noise than would normally be seen in a skin surface measurement.
Figure 7. Pace signal capture from resynchronization device in saline tank. The first pulse is the atrial, the second pulse is the right ventricle, and the third pulse is the left ventricle. The leads were placed in the saline tank with vectors optimized to see the pulses clearly. The negative-going pulse is the pace and the positive-going pulse is the recharge. The amplitude of the atrial pulse is slightly larger than the other two pulse amplitudes because the lead was in a slightly better vector than the ventricle leads, but in actuality, all three pacing outputs in the resynchronization device were programmed to have the same amplitude and width. With real patients, the amplitudes and widths are often different for each pacemaker lead. Detecting Pacing Artifacts The pacing leads for cardiac resynchronization devices will not all have the same vector. The right atrium lead usually aligns with Lead II, but it can sometimes point straight out of the chest, so a Vx vector may be needed to see it. The right ventricle lead is usually placed at the apex of the right ventricle, so it usually aligns well with Lead II. The left ventricle pacing lead, threaded through the coronary sinus, is actually on the outside of the left ventricle. This lead usually aligns with Lead II but may have a One of the major noise sources is the H-field telemetry scheme used by most implantable heart devices. Other sources of noise include transthoracic impedance measurements for respiration, electric cautery, and conducted noises from other medical devices connected to the patient. To further complicate the problem of acquiring pacing artifacts, each pacemaker manufacturer uses a different telemetry scheme. In some cases, a single manufacturer may use many different telemetry systems for different implantable device models. Many implantable devices can actually communicate using both H-field telemetry and either MICS- or ISM-band telemetry. The variability of H-field telemetry from one model to the next makes filter design very difficult. ECG devices have to be Class CF, but other medical devices may be Class B or BF, and their higher leakage currents may interfere with the performance of ECG acquisition devices. ADAS1000 ECG Analog Front End Includes Pacing Artifact Detection Algorithm
Figure 8. ADAS1000 block diagram. In addition to supporting the essential ECG signal-monitoring elements, the ADAS1000 is equipped with functions such as respiration measurement (thoracic impedance measurement), lead/electrode connection status, internal calibration, and capabilities for pace artifact detection—as discussed above. One ADAS1000 supports five electrode inputs, facilitating a traditional 6-lead ECG measurement. By cascading a second ADAS1000-2 (companion) device, the system can be scaled up to a true 12-lead measurement; and by cascading multiple devices (three and above), the system can be scaled to measurements with 15 leads and beyond. See Table 1 for details on the different variants of the ADAS1000. Table 1. Overview of Available Models of the ADAS1000
The respiration feature of the ADAS1000 provides the ability to measure thoracic impedance variations of the patient, indicating the extent, or absence, of breathing. At the heart of the respiration function is an integrated DAC (digital-to-analog converter) respiration drive at a programmable frequency (46 kHz to 64 kHz), and a dedicated analog-to-digital measuring circuit that simplifies this difficult measurement. The signal is demodulated and provided as magnitude and phase information, from which the corresponding respiration can be determined, given the specific cable parameters. The circuit is capable of detecting resolutions as small as 200 mΩ, using the internal capacitor—with even more-precise resolution, using an external capacitor—and has a flexible switching scheme, allowing measurement on one of three leads (I, II, III). Pace Detection Algorithm The pace-detection algorithm runs three instances of a digital algorithm on three of four possible leads (I, II, III, or aVF). It runs on the high-frequency ECG data, in parallel with the internal decimation and filtering. Designed to detect and measure pacing artifacts with widths ranging from 100 μs to 2 ms, and amplitudes of 400 μV to 1000 mV, it returns a flag that indicates pace was detected on one or more of the leads, and also the measured height and width of the detected signal. For users who wish to run their own digital pace algorithm, the ADAS1000 provides a high-speed pace interface that provides the ECG data at a fast data rate (128 kHz), while the filtered and decimated ECG data remains unchanged on the standard interface. The ADAS1000 ECG IC has a minute-ventilation filter built into its algorithm. Minute-ventilation pulses, which are conducted from the ring of a bipolar lead to the can of the pacemaker, detect respiration rates to control the pacing rate. They’re always less than 100 μs wide, varying from about 15 μs to 100 μs. Many implantable devices are capable of being programmed for pacing pulses as narrow as 25 µs, but physicians almost never program implantable devices with pulses that narrow because there would not be enough of a safety margin of energy above the pacing threshold. This pacing artifact system was developed by a team of engineers and pacing experts who worked in conjunction with the pacing industry. The result of this collaboration is a simultaneous three-vector pacing-artifact system that can detect pacing artifacts despite electrical noise that is significantly larger that the artifacts. Each of the three instances of the pace algorithm can be programmed to detect pace signals on different leads (I, II, II, or aVF). Programmable threshold levels allow it to be tailored to detect the range of pulse widths and heights presented, with internal digital filters designed to reject heartbeat, noise, and minute-ventilation pulses. When a pace has been validated in an individual instance of the pace signal, the device outputs a flag so that the user can mark or identify the pace signal in the ECG capture strip. A simplified flowchart of the pacemaker algorithm is shown in Figure 9.
Figure 9. Flowchart of the pace algorithm. The choice of sample rate for the pacing artifact algorithm is significant because it cannot be exactly the same frequency as those used by Medtronic, St. Jude, and Boston Scientific for the H-field telemetry carrier. All three corporations use different frequencies, and each has many different telemetry systems. Analog Devices believes that the sampling frequency employed by the ADAS1000 does not line up with any of the major telemetry systems of these three pacing companies. As mentioned above, the ADAS1000 also includes respiration measurement and ac leads off. These features both inject ac signals at different frequencies onto the patient electrodes, but they don’t interfere with the acquisition of pacing artifacts. Electric cautery signals can be filtered ahead of the ADAS1000 inputs for ECG, but performance of the pacing artifact detection algorithm may be degraded by the filtering, so care must be taken with its design. Conclusion We invite you to comment on pacing artifacts in the Analog Dialogue Community on EngineerZone. References 2http://en.wikipedia.org/wiki/File:SinusRhythmLabels.svg. 3(a) http://en.wikipedia.org/wiki/File:Cardiac_resynchronisation_therapy.png. 4http://www.nae.edu/page20019090/WhatisaPacemaker.aspx. 5http://en.wikipedia.org/wiki/File:St_Jude_Medical_pacemaker_with_ruler.jpg.
|
||||||||||||||||||||||||||||||||||||||||||||||||||