content here.
content here.

CAPACITANCE-TO-DIGITAL CONVERTER FROM ANALOG DEVICES ENABLES GREATER TOUCH-CONTROL SENSITIVITY IN PORTABLE ELECTRONIC DEVICES

AD7147 CapTouch™ controller provides accurate measurement and improved responsiveness for user interface controls.
AD7147

Norwood, MA (06/11/2007) - Cell phones, multimedia players, digital cameras, and other rapidly shrinking mobile devices increasingly require new user interfaces to replace mechanical switches. Analog Devices’ new capacitance-to-digital converter (CDC) is a highly integrated touch controller that allows designers to quickly and easily add responsive user controls, such as scroll wheels and touch pads, to portable electronic devices.

As the newest addition to Analog Devices’ family of CapTouch™ controllers for consumer applications, the AD7147 provides highly accurate measurement and responsiveness, and features the addition of an active shield feature for improved noise performance. Requiring only a single PCB (printed-circuit board) for full implementation, the new CDC is ideal for ultra-thin mobile electronic devices.

About the AD7147
The configurable AD7147 CDC features 13 capacitance inputs and femto farad resolution, allowing mobile electronics designers to implement a touch pad, scroll wheel, slider, or up to 36 buttons per device. The addition of integrated active shield technology protects the AD7147 from capacitance-to-ground pickup and other noise sources in the system, allowing designers the freedom to place the sensor away from the main system IC.

The analog front-end of the AD7147 has been improved, yielding a threefold improvement in sensor response compared to previous AD714x products. The improved response allows end-users to experience more accurate finger navigation and improved device performance, while continuing to offer designers per-channel sensitivity adjustment for sensor-response fine tuning. The AD7147 includes on-chip sensitivity algorithms that compensate for changes in temperature and humidity, and ensure that users with different finger sizes receive the same responsive sensor performance.

The AD7147 typically consumes 1 mA in full power mode, and just 50 μA in low-power mode, a 20% reduction compared to competitive products on the market. Additionally, the AD7147 has the industry’s lowest shutdown power consumption at only 2 μA.

Availability and Pricing
The AD7147 includes an SPI (serial peripheral interface)-compatible serial interface, while the AD7147-1 features an I²C (inter-integrated circuit)-compatible serial interface. Both devices are sampling now and will be available in full production quantities in July 2007. Priced at $1.30 per unit in 1,000-unit quantities, both products are housed in 24-pin 4 mm × 4 mm LFCSPs (lead-frame chip-scale packages).

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

CapTouch is a trademark of Analog Devices Inc.

Editor's Contact Information:

Linda Kincaid
781-937-1472
781-937-1078
linda.kincaid@analog.com