content here.
content here.

ANALOG DEVICES ENABLES SECURE AND ROBUST TRANSMISSION OF REMOTE DATA FOR SMART GRIDS AND HOME AND BUILDING AUTOMATION

- ADI’s new RF transceivers address short-range ISM-band and io-homecontrol® protocols.
New RF transceivers address short-range ISM-band and io-homecontrol® protocols

Norwood, MA (05/27/2009) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications and a leading provider of RF (radio frequency) technology, today announced the introduction of two new RF transceivers that deliver the best-in-class performance, low power consumption and high integration effective for smart grid and home and building automation applications. Smart grid technology measures how much power is consumed and at what time and price to save energy, reduce cost and increase reliability for the delivery of electricity from utility companies to consumers. RF transceivers are needed for the secure and robust transmission of this information over short distances, for storing measurement data, and communicating with utility computers over wireless networks. Over the next five years, analysts report that more than 150 million smart meters will be installed worldwide to support the growing number of smart grids coming online.

ADI’s new ADF7022 RF transceiver and ADF7023 RF transceiver are effective for smart grid and other applications operating on the short-range ISM-band (industrial, science and medical) for remote data measurement. These applications include industrial monitoring and control, wireless networks and telemetry systems, security systems, medical devices and remote controls. In addition, the ADF7022 RF transceiver is the industry’s first transceiver with an integrated communications processor to support the io-homecontrol® protocol, which is a technology that enables homeowners to control remotely home systems, such as roller blinds and shutters, awnings, garage doors, roof windows and heating systems.

“Wireless technology is becoming more pervasive as a mechanism to control and monitor energy, as well as control home and business systems,” said Peter Real, vice president, RF Group, Analog Devices, Inc. “Short-range RF transceivers offering robust radio performance are paramount for these applications, and Analog Devices’ new transceivers offer a complete radio solution with the performance, integration and low power consumption required to ensure the transfer of critical data.”

Complete Short-Range Transceiver with Support for io-homecontrol® Standard
Available to member companies of the io-homecontrol consortia, the new ADF7022 short-range RF transceiver is a low-power, high-performance, highly integrated FSK/GFSK transceiver designed for operation at the three io-homecontrol channels of 868.25 MHz, 868.95 MHz and 869.85 MHz in the license-free ISM band. The ADF7022 is fully compliant to ETSI-300-200 and has enhanced digital baseband features specifically designed for the io-homecontrol standard. This enables the device to perform complex tasks typically performed by a microprocessor, such as media access, packet management/validation and packet retrieval to and from data buffer memory, thereby allowing the host microprocessor to remain in power-down mode. As a result, this capability significantly lowers power consumption and eases both the computational and memory requirements of the host microprocessor. More details can be found at www.analog.com/pr/ADF7022.

Complete Short-Range Transceiver for ISM Bands at 433 MHz, 868 MHz and 915 MHz
The ADF7023 short-range RF transceiver is a low-power, low-IF transceiver designed for operation in the license-free ISM bands at 433MHz, 868MHz and 915MHz. The ADF7023 includes enhanced baseband features and offers a low transmit-and-receive current, as well as data rates in 2FSK/GFSK up to 250 kbps. It offers industry-leading blocking resistance and receive sensitivity with very low receive and transmit currents, allowing the radio to operate in environments where interfering signals are greater than four times stronger and more than double the operating range. It operates with a power supply range of 1.8 V to 3.6 V and has lower power consumption in both transmit and receive modes, enabling longer battery life. Other features integrated on-chip include an extremely low-power, 8-bit RISC communications processor; patent-pending, fully-integrated image rejection scheme; VCO (voltage controlled oscillator); Fractional-N PLL (phase locked loop); 10-bit ADC (analog-to-digital converter); digital RSSI (received signal strength indication); temperature sensors; AFC (automatic frequency control) loop; and battery voltage monitor. For more information, please visit www.analog.com/pr/ADF7023.

Pricing, Availability, and Complementary Products
The ADF7022 and ADF7023 RF transceivers are compatible with ADI’s AD8353 RF gain block, ADF4360 PLL/VCO, ADM6320 supervisory circuits and the ADL5542 driver amplifier. Furthermore, the ADF7022 and ADF7023 are supported by Analog Devices’ ADIsimSRD Design Studio, which is a free downloadable design tool that allows real-time simulation and optimization of many of the parameters in a typical wireless system. For information on samples, availability and pricing, please visit the ADI sales webpage: http://www.analog.com/salesdir/continent.asp.

Product
Price Each Per 1,000
Packaging
ADF7022
$2.88
5 x 5 mm 32-pin LFCSP
ADF7023
$2.88
5 x 5 mm 32-pin LFCSP

ADI's RF IC Portfolio Covers Entire RF Signal Chain
Using a unique combination of design skills, system understanding, and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain. Individual devices range from industry-leading, high-performance RF function blocks to highly-integrated, short-range, and WiMAX transceivers. The RF function blocks include DDS and PLL synthesizers; TruPwr™ power detectors and logarithmic amplifiers; X-Amp® VGAs; power amplifiers, LNAs and other RF amplifiers, mixers, and direct-conversion modulator and demodulator products. For more information, visit: http://www.analog.com/pr/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Colleen Cronin
781/937-1622

colleen.cronin@analog.com