Norwood, MA (11/17/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced the ADP1048, the first interleaved digital power factor correction (PFC) controller with highly accurate AC power metering capability. Similar to the ADP1047 single-phase digital PFC controller (announced March, 2011), the interleaved (or dual-phase) ADP1048 uses conventional, continuous-conduction-mode PFC techniques to reduce harmonic distortion. The ADP1048 can be configured as an interleaved design to reduce inductor size and replace the ACDC rectifier to improve efficiency in bridgeless boost mode. These techniques convert all signals to the digital domain and allow parameters to be adjusted and reported over a PMBus™-compliant interface, including accurate measurement of input voltage, current and power. The ADP1048 is extremely versatile and easy-to-use enabling ACDC designers and system architects to tweak their design in real-time and optimize efficiency at system level.
As with the ADP1047 single-phase controller, the ADP1048 interleaved PFC controller is easily programmed using an intuitive graphical-user interface (GUI), which enables customers to design and optimize their systems without the complex code programming required by alternative digital signal processor (DSP)-based devices. Designed specifically for high reliability AC/DC power-factor correction systems and motor control applications, the ADP1048 is suited to communications infrastructure, industrial and instrumentation systems, such as motor control, and high-power medical imaging applications.
The ADP1048 provides power metering accuracy of ±3 percent at full load current with further improvements to ±1 percent with customer calibration. The new digital controller also offers enhanced transient response through non-linear control algorithms, programmable inrush control to reduce start-up over-stress, real-time programming to maximize efficiency and extensive fault detection and reporting for improved reliability. The ADP1048 can be frequency synchronized to eliminate “beat” frequency noise, or alternatively, the switching frequency spread spectrum feature can be enabled to further improve EMI.
| Product | Full Production | Temperature Range | Price Each Per 1,000 | Packaging |
|---|---|---|---|---|
| ADP1048 | Now | -40°C to +85°C | $3.60 | 24-lead QSOP |
| ADP1048-600-EVALZ | Now | -- | $600.00 | -- |
The ADP1048 and ADP1047 digital PFC controllers are designed to complement the ADP1043A digital controller for isolated systems, high-speed MOSFET drivers and iCoupler® digital isolators, which also are available from Analog Devices. These devices facilitate easy implementation of intelligent power management for greater energy efficiency.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue
iCoupler® is a registered trademark of Analog Devices, Inc.
PMBus is a trademark of the System Management Interface Forum (SMIF), Inc.
Howard Wisniowski
781-937-1571
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved