Norwood, MA (07/20/2011) - Analog Devices, Inc. introduced today the ADP5034 regulator/LDO, a highly integrated power management IC that combines two 3-MHz, high efficiency, 1.2-A step down regulators with two 300-mA LDO (low drop out) regulators in a small LFCSP (lead-frame chip-scale) package. Also today, Analog Devices introduced the ADP5024 regulator/LDO, which is identical to the ADP5034 but features a single 300-mA LDO regulator. Occupying a total board area of only 69mm2, the ADP5034 and ADP5024 step-down regulators/LDOs are designed to meet the shrinking board space and increasing performance requirements of processors and FPGAs.
The integrated step-down regulators are used 180 degrees out of phase to reduce input filtering, which allows smaller input capacitors to be used while reducing input noise. A dedicated mode pin places both regulators in forced PWM operation or auto PWM/PSM operation for higher efficiency. The low quiescent current, low dropout voltage, and wide input voltage range of the ADP5034 and ADP5024 also enable more efficient power management. The integrated LDOs feature high 65-dB PSRR (power-supply rejection ratio) performance that ranges from 1 kHz to 10 kHz, lowering output noise to 80 μV/rms for powering sensitive analog circuitry.
The ADP5034 and ADP5024 step down regulators/LDOs are flexible, highly integrated power management components that can be used in applications including USB-powered portable devices, handheld medical products and multi-voltage power applications for processors, ASICs, FPGAs and RF chipsets. Each component has dedicated enable pins for each of the step down regulators and LDOs and supports adjustable output voltages on all four regulator outputs, allowing the output voltages to be easily set using an external resistor divider network. Adjustable output voltage allows the ADP5034 and ADP5024 to be easily and quickly modified to work with different output voltage requirements, which reduces design time and time to market. The ADP5034 and ADP5024 are fully specified over the junction temperature range of −40 °C to 125 °C and both are available in a 24-lead, 4 mm × 4 mm LFCSP packages
| Product | Sample Availability | Full Production | Price per 1k units | Packaging |
|---|---|---|---|---|
| ADP5024 | Now | August 2011 | $1.79 | 4mm x4 mm 24-lead LFCSP |
| ADP5034 | Now | Now | $1.99 | 4mm x4 mm 24-lead LFCSP |
| ADP5024-1-EVALZ | -- | Now | $100.00 | -- |
| ADP5034-1-EVALZ | -- | Now | $100.00 | -- |
Other products which may be used with the ADP5034 and ADP5024 regulators include Analog Devices’ SHARC® and Blackfin® processors and the ADF7023 and ADF7020 transceivers.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
All trademarks are the property of their respective owners.
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved