RAQs

What shall we do with an unused op-amp?

Q. In the RAQ on op-amps as comparators you mentioned an unused op-amp in a quad as being possible justification for using it as a comparator. What do you do if you've an unused op-amp and don't need a comparator?

What shall we do with an unused op-amp?


A.  This is a trickier than it looks. If an opamp is overdriven, the output stage will saturate at one of the supply rails, and the op-amp will consume excess power. Many common configurations of an unused upamp will overdrive it.

If the terminals are all left unconnected, there is a real risk that stray electrostatic fields will cause an input to go outside the supply rails. This can cause latch-up and destroy the whole chip. Even if latch-up does not happen, a dc field may cause saturation and power waste. In addition, the amplifier may amplify an ac field and, if overdriven, will heavily modulate its own supply current and cause crosstalk to other amplifier(s) on the chip.

Some users connect one input to the positive supply and the other input to the negative supply. This again saturates the output and wastes power; it may also exceed the differential input voltage rating and damage the device. Even if damage does not occur, some input stages draw several tens of milliamps under these conditions, wasting even more power.

Grounding both inputs, or shorting them together at some other potential, also causes the output stage to saturate, since the offset voltage of an op-amp is never exactly zero; shorting them together and not biasing them has the same latch-up risks that we have already mentioned.

What we should do is connect the device as a follower (output to inverting input1) and connect the non-inverting input to a potential somewhere between the supply rails. With a dual-supply system, ground is ideal, but connecting to the positive or negative supply of a single supply system will cause saturation and the resulting power waste if the offset voltage has the wrong polarity. The "potential somewhere between the supply rails" may be any point in the circuit with a suitable potential, since the loading caused by the op-amp input is minimal. For diagrams see the linked article.

Or you might use it as a buffer amplifier in a part of your system that does not need one but might perform slightly better if it had one.

1 If the op-amp is a current-feedback type, or has a minimum stable Acl >1 the connection should be made with a 100 kΩ resistor rather than a short-circuit to ensure stability and prevent possible oscillation.

Download this article (pdf) back to top

James Bryant Offers Intrigue, Interest and Technological Troubleshooting Ideas... engineer, applications manager, philosopher, humorist, columnist and radio ham (G4CLF), only a man with such an eclectic dossier could make the often drab world of semiconductors come to life with such color and imagination. James Bryant


For more information:

Unused Op-Amps
MT-036 (pdf)
MT-069 (pdf)
Comparators & Op Amps – May They Never Meet
Op Amps as Comparators (ppt)
Amplifiers and Linear
Parametric Search - Operational Amplifiers
Op-Amp Noise can be Deafening Too
Op-Amp Noise
Many of the noise coupling mechanisms described in this article apply to hum coupling
Low Noise from DC/DC Switching Supplies

Product Links:

ADG465: Single Channel Protector in SOT-23/µSOIC Packages
ADG467: Octal Channel Protector in SOIC Package

Analog Dialogue:

Protecting Off Amps
Amplifier Input Protection ... Friend or Foe?
ESD Diode Doubles as Temperature Sensor

Press Releases:

Analog Devices Unveils OP Amp With Over-Voltage Protection For Industrial Process Controls

Webcasts:

Operational Amplifiers (Op Amps) - Webcasts

Useful Analog Devices Links:

Analog Dialogue

Webcasts from Analog Devices

Sign up for Analog Devices eNewsletters

Analog Devices Homepage

back to top

Send Feedback X
content here.
content here.

Send Feedback

Close