High Efficiency Synchronous PWM Controller Boosts 1V to 3.3V or 5V

2001年02月01日

Figure 1

   

Introduction

CPU power supplies continue to fall toward the 1V level, although other circuits still require the traditional 3.3V or 5V rails. Since the LTC1700 is capable of operating at an input voltage as low as 0.9V, it can boost the latest CPU power supply voltages to provide the missing 3.3V or 5V rail. The LTC1700 uses a constant frequency, current mode PWM architecture but does not require a current sense resistor; instead, it senses the VDS across the external N-channel MOSFET. This reduces component count and improves high load current efficiency. Efficiency is further increased at high load currents through the use of a synchronous P-channel MOSFET. With Burst Mode operation selected, efficiency at low load currents is enhanced, thereby providing high efficiency over the entire load current range. The LTC1700 operates at 530kHz but can be externally synchronized to frequencies between 400kHz and 750kHz. During continuous mode operation, the LTC1700 consumes 540µA; it drops to 180µA in Sleep mode. In shutdown, the quiescent current is just 10µA. The LTC1700 is available in the 10-lead MSOP package.

3.3V to 4.2V Input, 5V/2A Output Regulator

Figure 1 shows a 10W output application circuit. Since the LTC1700 is operating at 530kHz, a small valued inductor is sufficient for this circuit. The input capacitors consist of a small 22µF ceramic capacitor in parallel with a B-case size tantalum capacitor. The ceramic capacitor provides a low overall ESR while the tantalum provides the bulk capacitance. In applications where the input is connected very close to a low impedance supply, the input tantalum capacitor may not be needed. A Sanyo POSCAP capacitor is used for the output capacitor because of its high ripple current rating. Once again, a ceramic capacitor is used in parallel with the POSCAP for reduced ESR and high frequency decoupling.

Figure 1. 3.3 to 4.2V input, 5V/2A output converter.

Figure 2 shows the efficiency curves for input voltages of 3.3V and 4.2V. Note that the maximum efficiency reaches 95% at a load current of 2A. A load step from 100mA to 1.75A was applied and its response is shown in Figure 3.

Figure 2. Efficiency of Figure 1’s circuit.

Figure 3. Load-step response of Figure 1’s circuit.

Start-Up and MOSFET Selection

When the voltage at the VOUT pin is below 2.3V, the LTC1700 operates in the start-up mode. In this mode, only the start-up circuitry in the LTC1700 is active and both of the external MOSFETs are turned off. Figure 4 shows the components that control start-up. In this mode, the current limit is set at 60mA and the internal MOSFET is used to bring the output voltage up. The start-up oscillator, which is different from the main oscillator, runs at 210kHz at a duty cycle of 50%. Due to the low current limit, the output should not be heavily loaded during the start-up phase, as this will cause the output to “hang.” Once the output rises above 2.3V, the rest of the internal circuitry of the LTC1700 comes alive and the external MOSFETs begin switching. The start-up circuitry will then be shut down.

Figure 4. Start-up components of the LTC1700.

In some applications, the input voltage is high enough that start-up mode is not needed, resulting in the circuit being able to power up at full load current. Figure 1 shows an example of this. The required input voltage to power up with full load current is:

VIN > 2.3 + VF

where VF is the forward voltage of the parasitic diode across the external P-channel MOSFET, which is dependent on the load current. For a load current less than 3A, a VF of 0.75V can be used.

Since the switchover from the internal MOSFET to the external MOSFETs occurs at VOUT = 2.3V, the MOSFETs selected should have a threshold of 2.5V or lower. This will guarantee a smooth transition out of the start-up mode.

3.3V Input, 5V/3A Output Regulator

Figure 5 shows a 3.3V input to 5V output circuit that can provide a maximum of 3A output current. Like the circuit in Figure 1, this circuit will bypass the start-up mode and therefore is capable of starting up at full load. Figure 6 shows that its efficiency reaches 88% at load currents of 2A to 3A. Figure 7 shows the load step response.

Figure 5. 3.3V input to 5V/3A output regulator.

Figure 6. Efficiency of Figure 5’s circuit.

Figure 7. Load-step response of Figure 5’s circuit.

3.3V Input, 5V/4A Output Regulator

The circuit shown in Figure 8 is capable of supplying 4A of load current. To obtain this output current capability, two IRF7811A N-channel MOSFETs are paralleled to obtain the required peak inductor current. Two Si9803DY are used for the synchronous P-channel MOSFET because of the amount of RMS current through these devices. The Si9803DYs are mounted on an area of copper adequate to effectively remove the maximum amount of heat. Due to the high RMS ripple current going into the output capacitors, two Panasonic SP capacitors are required. The maximum efficiency of 92% occurs at load currents between 2A to 3A. This circuit has no problem starting up into a load that exhibits a resistive characteristic.

Figure 8. 3.3V input, 5V/4A output regulator.

2.5V Input, 3.3V/1.8A Output Regulator

Figure 9 shows a circuit that takes an input of 2.5V and steps it up to 3.3V. Both MOSFETs are selected with a guaranteed threshold voltage of 3V. Its efficiency and load step response are shown in Figures 10 and 11, respectively. Due to its low input voltage, this circuit cannot start up into a heavy load.

Figure 9. 2.5V input, 3.3V/1.8A output regulator.

Figure 10. Efficiency of Figure 9’s circuit.

Figure 11. Load-step response of Figure 9’s circuit.

Conclusion

Through the use of VDS sensing and a synchronous topology, the LTC1700 provides high efficiency at high load currents. Selectable Burst Mode operation allows high efficiency to be obtained at low load currents. With its low operating voltage, the LTC1700 can easily be used to step up low voltages to the traditional 3.3V or 5V supply rails.

著者について

Sanhwa Chee
San-Hwa Cheeは、アナログ・デバイセズのパワー製品グループに所属するスタッフ・サイエンティストです。Linear Technology(現在はアナログ・デバイセズに統合)で、長年にわたり数多くの製品を設計し、リリースしてきました。そのキャリアの中で複数の特許を取得しています。
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して

製品