FAQ
AD7715 - FAQ
How do I get the best performance from the AD7714, AD7715 ADC?
The AD7714, AD7715 Sigma Delta ADC's performance considerations.
What are some general design considerations when using the AD7714, AD7715 ADC?
AD7714, AD7715 general design considerations.
What are the calibration options on the AD7714, AD7715 ADC?
AD7714,AD7715 Sigma Delta ADC Calibration Options.
How do I use the serial interface on the AD7714, AD7715 ADC?
Using the AD7714, AD7715 ADC serial interface.
What Architecture is used in the AD7714, AD7715 ADC?
The AD7714, AD7715 ADC Archetecture.
未使用ロジック入力は?
Q: /CONVSTやALERT、/BUSY信号を使用しない場合の処理を教えてください。
A: 未使用ロジック入力はノイズの影響でエッジが発生することを避けるためPull upなどでLOGIC high固定してください。