faqs
よくある質問(FAQ)
What is the compression rate of the ADV202/ADV212?
The compression rate is not defined in the JPEG2000 ISO/IEC15444-1 standard which is implemented on the ADV202/212.
Any compression rate can be programmed with the ADV202/212 encode parameters.
The part can be configured to provide a fixed compression rate with a variance of +5% of the programmed value, down to -100% of the programmed value.
The compression rate is programmed with the RCType and RCVal encode parameters [refer to Programming Guide].