よくある質問(FAQ)

What is the ADV202/ADV212?

The ADV2x2 is designed to provide a hardware solution for JPEG2000 compression. The ADV2x2 doesn't provide JPEG or MPEG compression.

The ADV2x2 allows seamless input of most common video formats such as NTSC, PAL, 1080i, or 720p.

The ADV2x2 provides JPEG2000 output compliant to the ISO/IEC1544-1 standard in JP2 and J2C formats.

An overview of ADV2x2 operation and operational requirements can be found in the AN-790 application note.