よくある質問(FAQ)

Should I be concerned about ESD?

The AD714x ESD Human Body Model is specified at 2.5kV.The AD714x sensors have been subjected to the ESD air discharge up to 15kV under both contact and non-contact conditions without any failures. Note: ESD events have to be carefully considered during development in order to prevent the ESD charge from coupling directly onto the AD714x sensor board circuits.