faqs
よくある質問(FAQ)
Can all sensors connected to the AD7147 be active at the same time?
The AD7147 takes a measurement on all sensors connected to it in a round robin fashion. All sensors can be measured within 36 ms. In practice, this allows the AD7147 to detect if sensors are active at the same time, as it is very unlikely the end user can activate/deactive a sensor within 36 ms.