faqs
よくある質問(FAQ)
I require a compression system with extreme low latency
The ADV202/212 has a latency of approx. 1.5 fields/frame/image in encode and approx. the same latency in decode mode.
This means, if a field, frame or image has an input rate of 10ms/field,frame or image then the latency will be approx. 15 ms in encode mode.