よくある質問(FAQ)

How to input RGB data to the ADV202/212

The ADV202/212 does not support direct input of RGB data on the VDATA or HDATA bus.

It does support input in single component format, so that either R or G or B can be input on the VDATA or HDATA bus.

For RGB applications it is therefore recommended to use the ADV202/212 in single component mode or to convert RGB to YCbCr 4:2:2 prior to encoding.