Chips to Measure ECG and PPG with Temporal Correlation | Maxim Integrated
要約
Pulse Arrival Time (PAT) is a useful medical parameter which can be correlated to physical attributes like artery hardness and changes in blood presser. Accurate PAT measurements require good temporal correlation between Electrocardiography (ECG) and Photoplethysmography (PPG) data. This application note presents a two chip solution using the MAX30003 ECG analog front end and the MAX86171 PPG optical pulse oximeter.
Introduction
To accurately measure pulse arrival time (PAT) using synchronized electrocardiography (ECG) and photoplethysmography (PPG) measurements, the two-chip solution described in this application note establishes a ±5µs temporal correlation between the ECG and PPG signals. This document discusses the hardware configuration and detailed register configuration settings that allow the two chips to acquire data synchronously. Also covered in detail is how to adjust for temporal-sampling offsets between the ECG and PPG data samples with respect to a selected ECG-filter group delay and PPG settling and integration times.
This two-chip solution uses the MAX30003 as the ECG analog front end (AFE) and the MAX86171 to optically obtain a PPG signal. The MAX30001 can also be used.
System Overview
Figure 1 shows the PAT measurement system, which consists of a 32,768Hz crystal input to the MAX30003 ECG AFE, a MAX86171 PPG with sampling triggered by a MAX30003 synchronization output pulse, and a microcomputer unit (MCU) to configure registers and read data from the FIFOs over a 3-wire SPI.
Figure 1. PAT measurement system.
To achieve system temporal synchronization, configure the MAX30003 interrupt registers to generate a synchronization pulse after each ECG sample is placed in its data FIFO. The MAX86171 wakes up with each ECG synchronization pulse and acquires a sample. After the PPG completes a measurement and sets its FIFO interrupt, the MCU reads the ECG and PPG FIFO data registers over the SPI. This process is repeated at the sample rate selected for the MAX30003 ECG.
Figure 2 shows the system timing. Although the MAX86171 internal timing is driven by its internal fast (10MHz) and slow (32kHz) clock signals, these clocks systematically reset each time a synchronization pulse wakes up the device. The one sigma clock jitter between the ECG sync out signal and the PPG clock system is measured at less than 300ns.
Figure 2. System timing.
Hardware Configuration
A single synchronization signal and the shared 3-wire SPI signals connect the ECG and PPG devices. Each device also has its own SPI chip-select signal from the MCU and a FIFO ready signal connected to the MCU. The MAX30003 FIFO interrupt signal uses INTB, and the synchronization output signal is setup on INTB2. Connecting the synchronization pulse to the MCU can be useful depending on how you set up the firmware. The MAX86171 has the synchronization signal connected to its TRIG input, and the FIFO interrupt signal is set up on INT1.
The MAX86171 is also configured for SPI communications by pulling the I2C_SPI pin high. For the scope of this application note, a single LED is driven by LED1_DRV, and the photodiode is connected to PD1_IN. Different LED and photodiode configurations can also be used but require different register configuration settings than the settings used here. Refer to the MAX30003 and MAX86171 data sheets for application-specific capacitor values. Figure 3 shows the hardware configuration, but power-supply decoupling caps are not shown in the circuit.
Figure 3. Hardware configuration.
ECG
The MAX30003 is a single-biopotential channel that provides ECG waveforms and detects heart rate.
The MAX30003 ECG AFE can be configured for different sample frequencies, signal gain, digital high- and low-pass filter corner frequencies, and input impedance. For this application note, the following parameters have been selected:
- Sample Rate = 512sps
- Gain = 20V/V
- Digital high-pass filter (DHPF) = bypass
- Digital low-pass filter (DLPF) = bypass
- Input Impedance (RBIAS) = 100MO
Lead-on and lead-off detection are also disabled for simplicity.
ECG Measurement Considerations
The most important consideration in using the MAX30003 ECG AFE in a synchronized data-acquisition system is understanding how the digital filter-group delay affects the time delay associated with each data sample placed in the ECG FIFO. For each of the different sampling rates listed in Table 1, the digital filter-group delay is a set number of 32kHz clock cycles. The number of 32kHz clock cycles is also different depending on weather the DHPF is active or in bypass mode. Depending on what clock is selected, there is also a systematic delay of 1.003ms or 1.020ms associated with the ADC sampling when the FMSTR clock is configured for 32,768Hz or 32,000Hz, respectfully.
Table 1 lists the calculated ECG sample delays (tECG_DELAY). These delays are referenced to the falling edge of the synchronization pulse, which occurs immediately after an ECG sample is placed in the FIFO (30µs) and immediately before the ECG FIFO flag is set (15µs). In practice, these delays have a measured typical standard deviation of 3µs.
Table 1. ECG Sample Delay (tECG_DELAY)
| DLPF Setting | FMSTR CLOCK = 32000Hz | FMSTR CLOCK = 32768Hz | ||||||
|---|---|---|---|---|---|---|---|---|
| 500sps Delay (ms) | 250sps Delay (ms) |
200sps Delay (ms) |
125sps Delay (ms) |
512sps Delay (ms) |
256sps Delay (ms) |
204.8sp Delay (ms) |
128sps Delay (ms) |
|
| Bypass | 21.333 | 92.333 | 39.833 | 106.333 | 20.839 | 90.172 | 38.906 | 103.844 |
| 40Hz | 33.333 | 116.333 | 69.833 | 154.333 | 32.558 | 113.610 | 68.203 | 150.719 |
| 100Hz | 33.333 | 116.333 | X | X | 32.558 | 113.610 | X | X |
| 150Hz | 33.333 | X | X | X | 32.558 | X | X | X |
X = Setting not allowed.
The ECG time-delay values in Table 1 were determined and verified by generating an input pulse and then looking at the output data. To obtain a measurement accuracy greater than the sample rate, multiple sets of pulses can be generated that have an additional 5µs delay with respect to the ECG synchronization pulse. Using the data, a set of output data is constructed with 5µs time steps to calculate the time from the center of the input pulse to the center of the output pulse. This can be done for several pulse widths in each configuration. The standard deviation of the delay for different pulse-width measurements is less than 5µs for all ECG configurations.
Table 2 shows the data for an ECG sample rate of 512sps with the DLPF set to bypass. The input-pulse-center-to-output-pulse-center data is averaged to obtain the average delay of 20.839ms with a standard deviation of 4.1µs.
Table 2. ECG Pulse Delay Measurement Data
| Input Pulse Width (µs) | Input-Pulse-Center-to-Output-Pulse-Center Delay (ms) |
|---|---|
| 100 | 20.835 |
| 500 | 20.834 |
| 1000 | 20.835 |
| 1953 | 20.842 |
| 3906 | 20.843 |
| 5859 | 20.844 |
| 7812 | 20.843 |
| 9765 | 20.842 |
| 15624 | 20.837 |
ECG Register Configuration
Table 3 lists the MAX30003 registers to configure to set up the ECG to generate the signaling for synchronous operation with the MAX86171. Any registers not listed are assumed to be in their default state after a software reset.
If the state of the registers is unknown, send a software reset before configuring the registers. For the MAX30003, write 0x000000 to register 0x08 (SW_RST).
To start the ECG data sampling, there are three register commands that must be sent after the PPG has been configured. See the Startup Sequence section for more details.
Table 3. ECG Register Configuration
| Address | Data | Configuration | Description |
|---|---|---|---|
| 0x02 | 0x800001 | EN_EINT = 1b | Set INTB to EINT (ECG FIFO Interrupt) |
| INTB_TYPE = 01b | CMOS driver | ||
| 0x03 | 0x000201 | SAMP = 1b | Set INTB2 to Sync pulse out. |
| INTB2_TYPE = 01b | CMOS driver | ||
| 0x04 | 0x000000; | EFIT = 0000b | FIFO interrupt when one word in FIFO |
| SAMP_IT = 00b | Generate one sync pulse for each data sample | ||
| 0x10 | 0x000007 | FMSTR = 00b | Master clock frequency set to 32768Hz |
| EN_ECG = 0b | Disable ECG (this bit starts the ECG sampling when set) | ||
| RBIASV = 1b | RBIAS = 100MO | ||
| RBIASP = 1b | ECGP is connected to VMID through RBIAS | ||
| RBIASN = 1b | ECGN is connected to VMID through RBIAS | ||
| 0x14 | 0x000000 | OPENP = 0b | Close ECGP mux switch |
| OPENN = 0b | Close ECGN mux switch | ||
0x15* |
0x000000 | RATE** = 00b | Sample at 512sps |
| GAIN = 00b | Gain set to 20V/V | ||
| DHPF = 0b | Digital high-pass filter set to bypass | ||
| DLPF = 00b | Digital low-pass filter set to bypass |
*The settings for register 0x15 differ depending on the sample rate, gain, and filter settings chosen.
**The MAX30001 uses the bits ECG_RATE[1:0] and the MAX30003 uses the bits RATE[1:0] for this configuration.
PPG
The MAX86171 optical pulse oximeter is an ultra-low-power, dual channel, optical data-acquisition system with 9 LED drive outputs. In addition, two independent 19.5-bit ADCs utilize internal ambient-light cancelation circuitry, which is ideal for measuring PPG.
In this application note, the MAX86171 is configured to sample each time a falling edge occurs at the TRIG input pin. When in external trigger mode, the MAX86171 measurement circuity is in sleep mode until a trigger input is received. When a trigger occurs, the device wakes up, takes a measurement, puts the data in the FIFO, generates an interrupt, and then goes back to sleep.
The MAX86171 measurement circuity does not need to be awake while communicating over SPI.
PPG Measurement Considerations
The MAX86171 PPG is configured to wake up and acquire a sample after each synchronization pulse is generated by the ECG. A random clock jitter occurs between the ECG and PPG because the internal clocks of the PPG run asynchronously to the 32,768Hz crystal that drives the ECG. This clock jitter between the ECG and PPG has been measured to be less than ±0.3µs. The clock jitter is systematically related to the start of the PPG 10MHz fast clock after the ECG synchronization pulse triggers the PPG to wake up and is typically less than two PPG fast-clock cycles or 0.2µs.
In central difference mode (CDM), the PPG reads the ambient background light immediately before and after the LED measurement. The average of these two ambient light measurements is subtracted from the LED measurement.
The PPG expected time delay (tPPG_DELAY) is the time between the falling edge of the ECG synchronization trigger pulse and the center of the LED integration time. The PPG internal clocks have a maximum accuracy error of less than 1%. So if the maximum tPPG_DELAY is 526µs, the maximum accuracy error is 5.26µs. The actual error varies from device to device and, if desired, can be measured and corrected to be 0.2% accurate using the FR_Clock_Frequency_Select (0x15) register settings. When properly tuned, the maximum error during the longest integration setting is less than 1.1µs. Figure 4 shows the tPPG_DELAY timing.
Figure 4. tPPG_DELAY timing.
Table 4 shows the tPPG_DELAY for each possible combination of LED settling and LED integration times. The times are based on the required number of internal fast and slow clock cycles by the internal PPG state machine for measuring, and a clock accuracy of 0% error is assumed. In this application note, only the registers for measurement 1 are used, and the pulse width is the sum of the settling time and the integration time set by the MEAS1 configuration registers. The register (0x19) MEAS1_Configuration_1 is used to configure the integration time, MEAS1_TINT, and the register (0x1B) MEAS1_Configuration_3 is used to configure the settling time, MEAS1_LED_SETLNG.
Table 4. PPG Expected Time Delay (tPPG_DELAY)
| Measurement 1 Configuration Register Settings | Settling Time (µs) | Integration Time (µs) | Pulse Width (µs) | tPPG_Delay (µs) | |
|---|---|---|---|---|---|
| (0x1B) Meas1 Configuration 3 | (0x19) Meas1 Configuration 1 | ||||
| 0x00 | 0x00 | 6 | 14.6 | 20.6 | 354 |
| 0x00 | 0x08 | 6 | 29.2 | 35.2 | 377 |
| 0x00 | 0x10 | 6 | 58.6 | 64.6 | 420 |
| 0x00 | 0x18 | 6 | 117.1 | 123.1 | 508 |
| 0x50 | 0x00 | 12 | 14.6 | 26.6 | 360 |
| 0x50 | 0x08 | 12 | 29.2 | 41.2 | 383 |
| 0x50 | 0x10 | 12 | 58.6 | 70.6 | 426 |
| 0x50 | 0x18 | 12 | 117.1 | 129.1 | 514 |
| 0xA0 | 0x00 | 18 | 14.6 | 32.6 | 366 |
| 0xA0 | 0x08 | 18 | 29.2 | 47.2 | 388 |
| 0xA0 | 0x10 | 18 | 58.6 | 76.6 | 432 |
| 0xA0 | 0x18 | 18 | 117.1 | 135.1 | 520 |
| 0xF0 | 0x00 | 24 | 14.6 | 38.6 | 372 |
| 0xF0 | 0x08 | 24 | 29.2 | 53.2 | 364 |
| 0xF0 | 0x10 | 24 | 58.6 | 82.6 | 438 |
| 0xF0 | 0x18 | 24 | 117.1 | 141.1 | 526 |
PPG Register Configuration
Table 5 lists the MAX86171 registers to configure to properly slave the MAX86171 to the MAX30003 synchronization pulse with minimum ECG-to-PPG sample time jitter. Any registers not listed are assumed to be in their default state after a software reset.
If the state of the registers is unknown, send a software reset before configuring the registers by writing 0x01 to register 0x0C (System Configuration).
Table 5. PPG Register Configuration
| Address | Data | Configuration | Description |
|---|---|---|---|
| 0x09 | 0xFF | FIFO_A_FULL = 0xFF | Set for FIFO full flag when there is one byte in the FIFO |
| 0x0A | 0x18 | FLUSH_FIFO = 1b | Reset PPG FIFO |
| FIFO_STAT_CLR = 1b | Clear FIFO full flag on FIFO data read | ||
| 0x0C | AND with 0xCF |
Clear SYNC_MODE by ANDing with 0xCF, leave all other bits in the previous state, and then set the following bits. | |
| SYNC_MODE = 01b | Sync on external pulse | ||
| PPG2_PWRDN = 1b | Power down Optical Channel 2 | ||
| SHDN = 1b | Set PPG in shutdown mode | ||
| 0x0D | 0x01 | MEAS1_EN = 1b | Enable Measurement 1 |
| 0x0E | 0x00 | ALC_Disable = 0b | ALC (ambient light correction) is enabled |
| COLLECT_RAW_DATA = 0b | Do not collect dark current | ||
| MEAS1_CONFIG_SEL = 0b | MEAS1 used only for MEAS1, not MEAS2 thru MEAS9 | ||
| 0x0F | 0x55 | PD4_BIAS = 01b PD3_BIAS = 01b PD2_BIAS = 01b PD1_BIAS = 01b |
Set all photodiode bias to a range of 0pF to 125pF (POR default) |
| 0x10 | 0x00 | INT2_FCFG = 00b | Disable INT2 |
| TRIG_ICFG = 0b | Set TRIG input triggers on falling edge | ||
| 0x11 | 0x04 | INT2_OCFG = 00b | Set INT2 output to open drain |
| INT1_OCFG = 10b | Set INT1 output to Active Low and Drive High when not active | ||
| 0x15 | 0x20 | FR_CLK_SEL = 1b | Set the internal frame clock to 32768Hz |
| FR_CLK_FINE_TUNE = 00000b | Set clock trim to 0% | ||
| 0x18 | 0x10 | MEAS1_AMB = 0b | Turn off ambient measurement |
| MEAS1_DRVC = 01b | Select LED3_DRV pin for LED Driver C | ||
| MEAS1_DRVB = 00b | Select LED2_DRV pin for LED Driver B | ||
| MEAS1_DRVA = 00b | Select LED1_DRV pin for LED Driver A | ||
| 0x19 | 0x00 | MEAS1_PPG2_PDSEL = 0b | Set PD2_IN input on optical channel 2 |
| MEAS1_PPG1_PDSEL = 0b | Set PD1_IN input on optical channel 1 | ||
| MEAS1_TINT = 00b | Set Measure 1 integration time to 14.6µs | ||
| MEAS1_AVER = 000b | Set Measure 1 average to one sample (no averaging) | ||
| 0x1A | 0x0F | MEAS1_SINC3_SEL = 0b | Use COI3 decimation filter. Turn off SINC3 filter. |
| MEAS1_FILT_SEL = 0b | Set ambient light rejection to central difference method | ||
| MEAS1_LED_RGE = 00b | Set LED current range for 0mA to 32mA | ||
| MEAS1_PPG2_ADC_RGE = 11b | Set PD2 Range to 32µA full scale | ||
| MEAS1_PPG1_ADC_RGE = 11b | Set PD1 Range to 32µA full scale | ||
| 0x1B | 0x50 | MEAS1_PD_SETLNG = 01b | Set 12µs photodiode settling time |
| MEAS1_LED_SETLNG = 01b | Set 12µs LED settling time | ||
| PPG2_DACOFF = 00b | PPG2 DAC offset current set to 0 | ||
| PPG1_DACOFF = 00b | PPG1 DAC offset current set to 0 | ||
| 0x1C | 0x20 | MEAS1_DRVA_PA = 0x20 | Set Drive A current to 4mA |
| 0x1D | 0x00 | MEAS1_DRVB_PA = 0x00 | Set Drive B current to 0mA |
| 0x1E | 0x00 | MEAS1_DRVC_PA = 0x00 | Set Drive C current to 0mA |
| 0x78 | 0x80 | A_FULL_EN1 = 1b | Enable A_FULL_EN status bit to be output on INT1. When A_FULL_BIT is asserted, INT1 is activated. |
Startup Sequence
After configuring the MAX30003 and MAX86171 for synchronized data acquisition, perform the following steps each time the system data acquisition starts to ensure proper temporal correlation between the ECG and PPG data sets:
- Reset PPG FIFO.
- Take PPG out of shutdown mode. The PPG is configured to take a sample each time a synchronization pulse is received from the ECG and waits for the first ECG synchronization pulse to occur.
- Before starting the ECG, perform the following:
- Send an ECG SYNCH command to the SYNCH (0x09) register to resynchronize all ECG internal timing.
- Send a reset command to the FIFO_RST (0x0A) register to reset the ECG FIFO.
- Set the ECG_EN bit in the ECG CNFG_GEN (0x10) register. Immediately after this bit is set, the ECG starts sampling at the data rate that is set in the CNFG_ECG (0x15) register.
PPG Startup
Before starting the ECG, use the commands in Table 6 to set the PPG to sample after each ECG synchronization pulse.
Table 6. PPG Startup Register Command Sequence
| Address | Data | Comment |
|---|---|---|
| 0x0A | OR with 0x10 | Set FLUSH_FIFO = 1b to reset the PPG FIFO. |
| 0x0C | AND with 0xFD | Clear the SHDN bit to take the PPG out of shutdown mode. |
ECG Startup
After the PPG startup commands are sent, start ECG sampling using the commands in Table 7. These commands must be executed in the order listed.
Table 7. ECG Startup Register Command Sequence
| Address | Data | Comment |
|---|---|---|
| 0x09 | 0x000000 | Internal clock synchronization command. |
| 0x0A | 0x000000 | Reset FIFO command. |
| 0x10 | OR with 0x080000 | EN_ECG = 1b to enable ECG sampling. |
When started, the system continuously acquires data at the selected ECG sample rate until the EN_ECG bit in the ECG CNFG_GEN (0x10) register is cleared.
Data Collection and Temporal Correlation
While the system is continuously acquiring data, the ECG and PPG FIFOs need to be read after each data pair is placed in the respective FIFO. It is important that the ECG data FIFO is not read until the PPG completes measurement because the small current signal generated by the PPG photodiode is susceptible to switching transitions on the SPI lines. The PPG FIFO Ready interrupt goes low immediately after the PPG completes measurement. If data is not read after each measurement, it becomes difficult to manage the reading of multiple samples from the FIFOs and to guarantee that there is no SPI activity during the PPG measurement time.
Adjust the ECG and PPG data pairs based on the delay times to make meaningful pulse arrival time (PAT) measurements. The ECG data sample read after a given ECG synchronization pulse at time tSYNCH represents an ECG measurement at time tECG. tECG is the ECG measurement time before the synchronization pulse, which is expressed as tECG = tSYNCH – tECG_DELAY. The PPG data sample read after the same ECG synchronization pulse represents a PPG measurement at time tPPG. tPPG is the measurement time after the synchronization pulse falling edge, which is expressed as tPPG = tSYNCH + tPPG_DELAY.
Figure 5 shows the relationship between tECG and tPPG.
Figure 5. Data pair delay timing.
The time difference between the ECG and PPG data pair is determined by subtracting tECG from tPPG as follows:
tPPG – tECG = tPPG_DELAY + tECG_DELAY
This is the sum of the ECG and PPG delays defined in Table 1 and Table 4.
To time-correlate the ECG and PPG data pair, read from the FIFOs after each measurement at time tSAMPLE. Assume that the ECG timestamp is equal to tSAMPLE. To determine the PPG timestamp, add tSAMPLE and the time-delay sum.
Choose
tECG = tSAMPLE
Then
tPPG = tSAMPLE + tPPG_DELAY + tECG_DELAY
for a given ECG PPG data pair.
Converting Raw ECG Data to ECG Millivolts
Each ECG sample word read from the ECG FIFO consists of 3 data bytes. The lower 6 bits contain tags, which can be used to verify the quality of the data. Assuming that the 3-data-byte word is read into a 3-byte character array called data, the most significant byte is in data[0], and the least significant byte is in data[2], the following C code can be used to convert the raw data word into ADC counts:
data[2] = data[2]>>6; // shift data right 6 bits to remove data tags
ADC_count = data[0] × 1024 + data[1] × 4 + data[2];
If (ADC_count > 131072) ADC_count = ADC_count – 262144;// 2's complement
To convert the ADC count to millivolts, use the following equation:
ECG_mv = 1000 × ADC_count / (217 × Gain)
where Gain is the ECG gain of 20V/V, 40V/V, 80V/V or 160V/V selected by the register 0x15.
Refer to the MAX30003 data sheet for more details on the ECG data-word format.
Converting Raw PPG Data Words to PPG Counts
Each PPG-sample word read from the PPG FIFO consists of 3 data bytes. The upper 5 bits of the most significant byte contain automatic ranging information and are masked with zeros before converting to counts. Assuming that the 3-data-byte word is read into a 3-byte character array called data, the most significant byte is in data[0], and the least significant byte is in data[2], the following line of C code can be used to convert the 3-byte raw data word into PPG counts:
PPG_count = (data[0]&0x07) × 65536 + data[1] × 256 + data[2];
PPG_count is proportional to the amount of light collected from the LED driven by the PPG device during the LED integration time. The absolute magnitude of the counts is dependent on many variables and has no absolute reference.
Because the PPG data is typically recovered as an approximated 1Hz AC signal riding on a large, slowly moving (0.2Hz) background signal, the PPG data is usually displayed with the background signal removed. The easiest way to remove the background signal is to subtract the PPG signal value of sample n from a one second running average of the PPG signal. The running average is centered on sample n (i.e., the average spans from 0.5 seconds before to 0.5 seconds after sample n).
Refer to the MAX86171 data sheet for more details on the PPG data-word format.
PAT Data-Correlation Example
Table 8 shows an example of raw data-pair samples and their corresponding time-corrected correlation for each data sample. The correction assumes ECG sampling at 512sps with the DLPF bypassed and the PPG set for 24µs-settling time and 117µs-integration time. These settings require an ECG-delay adjustment of 20.839ms and a PPG-delay adjustment of 526µs giving a total ECG-to-PPG offset of 21.365ms, which was calculated as follows:
tPPG_DELAY + tECG_DELAY = 0.526ms + 20.839ms = 21.365ms
Data sampled at 512sps results in consecutive samples separated by 1.953125ms. As shown in Table 8, the PPG samples for each data pair are assigned a sample time that is 21.365ms after the ECG time. ECG time is assumed to be n × 1.953125ms, where n is the sample index.
Table 8. PAT Data-Sample-Pair Time-Correlation Example
| Raw Data Pairs | Time-Corected Data Pairs | |||||
|---|---|---|---|---|---|---|
| SAMPLE n | ECG COUNTS | PPG Counts | ECG | PPG | ||
| TIME (ms) | COUNTS | TIME (ms) | COUNTS | |||
| 0 | -308 | 305513 | 0.0000 | -308 | 21.3650 | 305513 |
| 1 | -230 | 305560 | 1.9531 | -230 | 23.3181 | 305560 |
| 2 | -94 | 305542 | 3.9063 | -94 | 25.2713 | 305542 |
| 3 | 38 | 305554 | 5.8594 | 38 | 27.2244 | 305554 |
| 4 | 236 | 305561 | 7.8125 | 236 | 29.1775 | 305561 |
| 5 | 462 | 305567 | 9.7656 | 462 | 31.1306 | 305567 |
| 6 | 606 | 305588 | 11.7188 | 606 | 33.0838 | 305588 |
| 7 | 800 | 305592 | 13.6719 | 800 | 35.0369 | 305592 |
| 8 | 1101 | 305599 | 15.6250 | 1101 | 36.9900 | 305599 |
| 9 | 1358 | 305594 | 17.5781 | 1358 | 38.9431 | 305594 |
| 10 | 1621 | 305589 | 19.5313 | 1621 | 40.8963 | 305589 |
| 11 | 1971 | 305583 | 21.4844 | 1971 | 42.8494 | 305583 |
| 12 | 2255 | 305619 | 23.4375 | 2255 | 44.8025 | 305619 |
| 13 | 2322 | 305622 | 25.3906 | 2322 | 46.7556 | 305622 |
| 14 | 2143 | 305636 | 27.3438 | 2143 | 48.7088 | 305636 |
| 15 | 1780 | 305651 | 29.2969 | 1780 | 50.6619 | 305651 |
| 16 | 1270 | 305647 | 31.2500 | 1270 | 52.6150 | 305647 |
| 17 | 543 | 305645 | 33.2031 | 543 | 54.5681 | 305645 |
| 18 | -273 | 305652 | 35.1563 | -273 | 56.5213 | 305652 |
| 19 | -872 | 305635 | 37.1094 | -872 | 58.4744 | 305635 |
| 20 | -1201 | 305660 | 39.0625 | -1201 | 60.4275 | 305660 |
Conclusion
In a real-world solution of a test subject, Figure 6 shows actual data with wet ECG electrodes placed on the chest to measure Lead II and PPG data taken from a finger on the left hand. The ECG counts have been converted to millivolts, and the PPG counts have been high-pass filtered to remove the DC component of the signal by subtracting each PPG sample from a one-second-wide running average.
Figure 6. ECG and PPG correlated data plot.
There are many different methods to calculate PAT, so the reader must decide on which method best meets their needs. This application note shows hardware and register configurations to obtain ECG and PPG data that is typically time correlated to a standard deviation of less than 5µs.