RF Converters: A Technology That Is Enabling Wideband Radios

Figure 1

   

Converters that can directly synthesize signals in the radio frequency range (RF converters) have matured to a point that they are poised to transform conventional radio designs. With the capabilities to digitize and synthesize instantaneous signal bandwidths as high as 2 GHz or 3 GHz, RF converters can now deliver on the promise of truly wideband radios, enabling radio designers to dramatically reduce the amount of hardware needed to create a radio, and enabling a new level of reconfigurability via software that simply is not possible with conventional radio designs. This article explores the advances in RF converter technology that make this new breed of data acquisition systems and wideband radios possible, and discusses the possibilities that software configurability creates.

Introduction

A design constraint that faces every radio designer is the trade-off of designing for signal bandwidth with the highest possible quality vs. the power consumption of the radio. How the radio designer meets this constraint determines the size and weight of the radio and fundamentally influences the placement of the radio, which includes buildings, towers, poles, underground vehicles, packs, pockets, ears, or glasses. Each radio location has an amount of power available that is commensurate with its location. A building or a tower, for example, will likely have more power available to it than a smartphone in a pocket or a Bluetooth® headset in an ear. In all cases, a fundamental truth exists: the less power a radio takes and the more throughput it is able to deliver per unit of power, the smaller and lighter the radio will be. This has immense consequences, and has been the driver behind much of the innovation in the communications electronics industry over many years.

As semiconductor companies have integrated more functionality and higher performance into the same or smaller size component, the equipment that uses them has been able to deliver on the promise of smaller, more functional, lighter, or all three in some cases. The smaller, lighter equipment that is better, with more functionality, enables placements of this better equipment in locations that were previously prohibited due to some other constraint, such as the amount of real estate needed for a building that is reduced when the unit can go on a tower, the size of a tower radio unit that can be reduced to a pole unit if the weight of the unit is low enough, or a unit that was required to be carried in a vehicle due to its weight can now be carried in a pack.

Today’s environment is filled with legacy installations that require buildings, towers, poles, and vehicles. Driven by the need to connect the people in the world to each other, engineers meet that challenge by designing equipment with the available components at that time, and delivered to us the communications-rich environment we have today; where we can talk, text, IM, photograph, download, upload, and browse nearly anywhere we wish on one of several different networks, including mobile networks wireless LANs, ad hoc short range wireless networks, and others. These all connect to the broadband wired network on which the data is carried by RF cables and eventually by optical fiber.

Figure 1. RF converters enable wideband radios that can service demanding data services like streaming video and gaming.

Enhanced Video Experience

As several studies have shown,1, 2 the demand for data is projected to continue increasing well into the next decade. This is driven by a seemingly insatiable demand for richer data content that needs wider bandwidths. For example, cable television and fiber-to-the-home carriers continue to compete on broadband services to the home by offering higher speed connections and more high definition TV channels. The move to ultrahigh definition (UHD or 4k definition) TV calls for more than twice the capacity of HD TV and requires wider channel bandwidths than are being used today.

In addition, immersive video, which includes virtual reality (VR), as well as gaming and 3D effects like 180° or panoramic viewing with multidimension freedom, all with 4k UHD TV, will demand up to 1 gigabit of bandwidth per user.2 This goes well beyond the already demanding needs of simple 4k UHD TV broadcast and streaming. Online gaming demands symmetrical data bandwidths in the network since latency times are crucial, and this is driving development of much wider bandwidth upstream transmission capability. This need for wider upstream capability is, in turn, causing equipment makers to upgrade their designs to enable symmetrical, wide bandwidth transmissions.

The enhanced capabilities of today’s RF converters are crucial to enabling advances in the delivery of such rich video content. They must be able to create high dynamic range signals with excellent spurious-free performance in order to enable the use of higher order modulation schemes such as 256-QAM, 1024-QAM, and 4k-QAM. These higher order modulation methods are needed to increase the spectral efficiency of each channel, since the installed coaxial cable plant and distribution amplifiers have a finite bandwidth of 1.2 GHz to 1.7 GHz. Higher performance in the head-end transmission equipment extends the usable life of the installed equipment base, easing capital budget constraints and allowing multiple service operators (MSOs) a longer window of time in which to upgrade their equipment and transmission systems.

Multiband, Multimode Test

Today’s smartphones resemble traditional mobile phones even less as more features are packed into them. Many of these features have radios associated with them and, thus, the mobile device of today has upward of five or seven or more radios in it. Each of these radios must be tested when the smartphone is produced, and this presents new challenges to makers of multimode communications testers. There is a need for speed to keep test costs down, despite the number of tests increasing with the number of radios. Building different radio hardware for each radio in the mobile device becomes impractical with regards to size and cost of the tester. With more bands opening or being proposed for mobile services,3 the challenge of testing more and more radios in the mobile device increases.

This challenge can be addressed well by RF converters. In both the transmitter and receiver, RF converters can provide flexibility that can’t be achieved with conventional radios. Wideband RF converters provide the ability to capture and to directly synthesize signals in every band at the same time, enabling simultaneous test of multiple radios in the mobile device. With channelizers built into the RF DAC and RF ADC, those multiple radio signals are efficiently processed in the converters. For example, in Figure 2, 3 channelizers per RF DAC are shown, enabling three different signals and bands to be directly synthesized, combined, and then upconverted digitally with the numerically controlled oscillator (NCO) before being converted to an RF signal by the RF DAC.

In other market segments such as testing equipment for aerospace and defense, the need is increasing for wideband test solutions for pulsed radar and military communications. Due to the number and types of radar, electronic intelligence, electronic warfare equipment, and communications equipment needing test, the test equipment manufacturer must create a flexible instrument with a rich set of features.4 For example, arbitrary waveform generators must be able to create various signals, including linear frequency modulation, pulsed signals, phase coherent signals, and modulated signals across a wide range of output frequencies and bandwidths. Measurement equipment must be equally capable in order to receive such signals when testing the exciter or transmitter. RF converters serve this application well by enabling direct RF synthesis and measurement at RF frequencies. In some cases this can eliminate the need for an up or downconversion, and in other cases can reduce the number needed to a single conversion. This simplifies the hardware and can thus reduce its size, weight, and power requirements. The addition of digital features such as channelizers, interpolators, NCOs, and combiners makes for efficient signal processing on dedicated, low power CMOS technology.

Figure 2. Example of an RF DAC with channelizers.

Software-Defined Radios

RF converters can be a critical enabler in software-defined radios. With the ability to directly synthesize and capture radio frequencies in the multi-GHz range, RF converters simplify the radio architecture by eliminating entire up or downconversion stages, instead implementing them digitally. The removal of the analog conversion stage and the associated mixers, LO synthesizers, and filters reduces the size, weight, and power (SWaP) of a radio, enabling the radio to be situated in more places and operate from smaller power supplies. Such technology makes it possible for the radios to be small and light enough to be hand carried, driven in small ground vehicles, or mounted in various airborne assets such as planes, helicopters, and unmanned aerial vehicles (UAVs).

In addition to enabling better communication across platforms, radio hardware built with RF converters has the potential to be multifunction, as well as multimode and multiband. Because RF converters are now able to reach to the lower radar bands, and in the near future will reach the higher bands, the concept of a single unit that can be used as both a radar and a tactical communications link can become a reality. Such a unit offers clear leverage in terms of field repairs, upgrades, and procurement procedures and costs.

The ability to directly synthesize and capture radar frequencies makes RF converters ideal for phased array radar systems. Because direct RF converter synthesis and capture eliminates so much conventional radio hardware, an individual signal chain is much smaller and lighter. Thus, packing many of these radios into a smaller space is possible. Arrays suitable for ship-mounted or ground-based phased arrays, as well as smaller arrays and units for signal intelligence operations, can be built with a smaller SWaP.

Figure 3. Software-defined radio powered by RF converters enables connected communications across platforms.

The Technology Behind RF Converters

One of the key technology advancements that makes RF converters possible is the continuous march toward finer line CMOS processes. As the gate length and feature size of the basic CMOS transistor becomes smaller, digital gates get faster, smaller, and lower power.6 This allows for significant digital signal processing to be included on chip with the RF converter with reasonable power and area. The inclusion of digital channelizers, modulators, and filters that are software programmable are critical to constructing an efficient and flexible radio. This more efficient DSP also opens the door to use digital processing to help correct analog deficiencies in the converter. On the analog side, each new node provides faster transistors that have better matching per unit area. These improvements are critical for faster high precision converters.

Process technology advancement alone is not sufficient—there have also been some key architectural advancements that make these converters possible. The architecture of choice for RF DACs is the current steering DAC architecture. The performance of this type of DAC is dependent on the matching of the current sources that comprise the DAC. Uncalibrated current source matching is proportional to the square root of the area of the current source.7 The matching per unit area will improve with each technology node. However, even in the most advanced nodes a current source with low enough random mismatch for a high resolution converter would be very large. Having such a large current source would make the converter large and, more critically, the parasitic capacitance of this large current source degrades the high frequency performance of the DAC. A much more attractive solution is to calibrate smaller current sources to achieve the desired level of matching. This can significantly reduce the added parasites from the current source and, thus, allow for the desired linearity performance without compromising the high frequency performance. If done correctly, this calibration can be made very stable across temperature and this allows for the calibration to be done one time. Stable one-time calibration means calibration doesn’t need to be run periodically in the background, which saves operating power and alleviates concerns about spurious products creation due to the calibration running in the background.8

Another architectural choice that assists in meeting the desired converter performance metrics at very high speeds is the choice of switch architecture used to steer the DAC current. The traditional dual-switch structure (Figure 4) has several drawbacks when operated at very high speeds.9, 10 Since the data driven into the dual-switch can stay the same anywhere from one to many clock cycles, the tail node will have a data dependent amount of time to settle. If the clock rate is slow enough for this node to settle within one clock period this is not a problem. However, at very high rates this node will not settle fully in one clock period and thus the data dependent settling time will cause distortion in DAC output. If a quad-switch (Figure 5) is used, the data signals are all returned to zero. This leads to the tail node voltage being independent of data input, which alleviates the problem mentioned above. The quad-switch also allows for the DAC data to be updated on both edges of the clock. This feature can be used to effectively double the DAC sample rate without doubling the clock frequency.11

Figure 4. Example of a dual-switch DAC cell.

Figure 5. Example of a quad-switch DAC cell.

Using a well-designed current source calibration algorithm and a quad-switch current steering cell, in combination with today’s fine line CMOS processes, allows for the design of a DAC that can sample at very high rates with excellent dynamic range. This allows for synthesis of high quality signals across a wide range of frequency. When this wideband DAC is combined with supporting DSP it becomes a very flexible high performance radio transmitter that can be configured to provide signals for all of the different applications mentioned in this article previously.

Future Radios

While the RF converters of today are already enabling radical changes in radio architecture design, they are poised to enable even greater changes in the future. As process technology continues to advance and RF converter design is further optimized, the RF converter’s impact on power consumption and size of a radio will continue to shrink. These opportune technology advances come just in time to enable the next generation of radios, such as emerging 5G wireless base station applications like massive MIMO, as well as large scale phased array radars and beamforming applications. Deep submicron lithography will enable even larger amounts of digital circuitry to be placed on the RF converter die, integrating critical compute-heavy functions like digital predistortion (DPD)13 and crest factor reduction (CFR) algorithms that help to improve power amplifier efficiency and reduce overall system power dramatically. Such integrations will relieve the pressure on power-hungry FPGA logic and move those functions to power-stingy dedicated logic. Other possibilities include integrating the RF converter and its digital engines with RF, microwave, or millimeter wave analog components, further reducing size and further simplifying the radio design, and delivering a bits-to-antenna, system-level approach to radio design. With RF converters, a wide range of opportunities exist. RF converters are technology that is Ahead of What’s Possible.

About the Authors

Daniel E. Fague
Daniel E. Fague is the director of systems application engineering in the High Speed Products Group at Analog Devices. He received his B.S.E.E from Gonzaga University in 1989 and his M.S.E.E. from the University of Califor...
Steven Rose
Steven C. Rose is a Staff Design Engineer in the high-speed products group at Analog Devices. He received his BSEE from the University of Michigan in 1999 and his MSEE from the University of California at Berkeley in 2002....
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Industry Solutions

Resources


Analog Dialogue
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project