signals header
Aerial view of a large data center complex with extensive rooftop cooling units at sunset
Aerial view of a large data center complex with extensive rooftop cooling units at sunset

SIGNALS+ NEWSLETTER SUBSCRIPTION

Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.

By clicking “Subscribe”, you consent to receive marketing communications from Analog Devices, Inc. and its subsidiaries and agree to our Privacy Policy. Unsubscribe any time in your Privacy Settings.

Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.

You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!

Close
Donal McCarthy
Donal McCarthy,

Market Segment Director for Datacenter Power

Author Details
Donal McCarthy
Donal McCarthy holds a B.E.E. from University College Cork, an M.B.A. from Boston College, and a marketing diploma from the Irish Management Institute in Dublin. Donal has held various roles, including design engineer at M/A COM, field sales engineer and marketing roles at Hittite, and marketing management and director positions at Analog Devices.
Close Details

800 VOLTS: POWERING THE FUTURE OF HYPERSCALE DATA CENTERS

March 27, 2026


KEY TAKEAWAYS

  • AI workload demand surges from 120kW to 600kW–1 MW per rack, making the transition to 800V architecture essential to overcome the physical limits of traditional 48V systems.
  • 48V architecture remains highly relevant due to its mature ecosystem, proven reliability, manageable safety profile, and compatibility with existing infrastructure investments.
  • Hot-swap controllers are evolving into a power entry point and first line of defense, providing real-time telemetry, enabling predictive maintenance, and optimizing capacity planning, while improving energy forecasting and proactive failure prevention.

 

Hyperscale AI workloads are rewriting the rules of data center design. Compute density is skyrocketing as operators strive to pack more GPUs into every server rack. A rack that consumed 120kW two years ago will soon demand 600kW, with projections reaching 1MW by the end of the decade1 for cutting-edge racks.

At these power levels, traditional 48V architectures hit physical limits—cabling becomes unwieldy and current surges create inefficiencies. Migrating to 800V reduces current, minimizes losses, and enables sidecar power units, freeing rack space for additional main rack compute trays. This shift is essential for hyperscalers delivering advanced AI training and inference at scale—where training builds AI models using massive datasets, and inference applies those models to deliver real-time insights and outputs.

WHY 48V STILL MATTERS

While ±400V/800V architectures will emerge for ultra-high-power AI racks, 48V backplane distribution will remain highly relevant over the next 5+ years due to its deep ecosystem maturity, manageable safety profile, retrofit compatibility, and alignment with a large number of server and accelerator power envelopes.

48V is already standardized, qualified, and shipping at massive scale (OCP ORv3, hyperscaler custom racks). The existing ecosystem is deep and hyperscalers prioritize known reliability and supply-chain resilience, especially for fleet-scale deployments.

Analog Devices, Inc. (ADI) will continue to serve customers relying on 48V proven infrastructure for cost-effective performance as well as hyperscale data centers requiring 800V.

800V: THE FOUNDATIONAL LAYER FOR THE AI FUTURE

The move to 800V is not just an incremental upgrade; it represents a fundamental redesign of the data center power ecosystem. Increasing the voltage significantly lowers the current needed to deliver the same power. This seemingly simple change has profound strategic implications.

Icon depicts Unlocking Scalability

Unlocking Scalability:
800V architecture enables the delivery of megawatts of power per rack, removing physical barriers that currently limit compute density. This results in more powerful GPUs per rack, faster interconnects, and more powerful AI clusters.

Icon depicts Driving Efficiency

Driving Efficiency:
Higher-voltage (800V DC) power distribution reduces current for a given power level, significantly lowering resistive losses in power delivery conductors. This enables smaller cabling, better power density, and lower distribution thermal load. When combined with fewer conversion stages and DC-native architectures, 800V can reduce infrastructure losses, material usage, and total cost of ownership for high‑power AI data centers.

Icon depicts Enabling Architectural Innovation

Enabling Architectural Innovation:
The 800V model supports a disaggregated power architecture, relocating bulky components like power distribution and battery backup units outside the primary IT rack to the sidecar. This frees up valuable space for additional compute trays in the IT rack.

Technician configuring servers inside a large data center with rows of illuminated server racks

Beyond Power: The Dawn of the Intelligent Data Center

This transition to 800V is driven by the need to support higher power delivery and increasing rack density. As systems scale, higher voltage architectures become a practical necessity, placing greater demands on protection and power‑path management. In this high‑voltage environment, the hot‑swap controller serves as the first line of defense, taking on a more strategic role across the entire rack.

Modern hot‑swap controllers for 800V systems function as advanced protection and data‑acquisition devices, delivering real‑time telemetry for voltage, current, power, and temperature. This goes beyond operational telemetry, providing actionable system‑level insights that can be used to make better‑informed decisions.

  • Predict and Prevent Failures: By analyzing historical power consumption data, failures in components can be identified before they cause catastrophic outages, shifting from a reactive to a predictive maintenance model.
  • Optimize Capacity Planning: : Real-time load profiling provides an accurate picture of energy demand, enabling smarter, rack-level capacity planning and preventing over provisioning. This goes beyond operational telemetry, providing actionable system level insights that can be used to make better informed decisions around.
  • Improve Energy Forecasting: Accurate telemetry feeds into sophisticated models for energy demand forecasting, helping to manage costs. Can support procurement strategy and negotiations for more favorable contract structures.

High-voltage data centers require uninterrupted operation and power reliant processing system operations, including power density: high-voltage control and protection, telemetry and diagnostic supporting reliability, and advanced power monitoring: system diagnostics for predictive maintenance.

HOT SWAP: THE UNSUNG HERO OF HIGH-VOLTAGE SYSTEMS

As voltages increase, so do the risks. Hot-swap technology—long a key part of data center reliability—becomes mission-critical in an 800V environment because of these factors:

  • Safety at Scale: Live tray insertion and removal at 800V introduces risks of arcing and the potential of catastrophic failure. Hot-swap controllers mitigate these hazards by managing inrush currents and isolating faults.
  • Uptime Imperative: Hyperscale racks can cost millions. Downtime equals lost revenue. Hot-swap ensures uninterrupted operation during maintenance.
  • Intelligent Control: Next-generation hot-swap solutions integrate telemetry, enabling predictive diagnostics and real-time monitoring.

ADI leads in high-voltage hot-swap innovation, offering modular solutions that simplify integration and improve reliability. These systems combine robust protection with next-generation high-voltage hot-swap controllers that efficiently manage inrush currents. They include comprehensive telemetry for system diagnostics and advanced sensing to help ensure safe, efficient power delivery in the most demanding environments. By adopting a system view of rack power development, developers can help cloud server providers and system integrators gain new insights and realize savings.

TELEMETRY AND PREDICTIVE INTELLIGENCE

Tomorrow’s hyperscale power systems won’t just switch—they’ll provide insight. Embedded telemetry in hot-swap modules provides:

  • Failure Prediction: Detect anomalies before they disrupt operations.
  • Capacity Planning: Optimize rack utilization and energy distribution.
  • Energy Forecasting: Improve sustainability and cost efficiency.

These capabilities transform power delivery from a passive component into an active contributor to uptime and performance. Hot-swap technology, combined with advanced monitoring and protection, will be central to this transformation. ADI is committed to driving these innovations forward, ensuring data centers stay reliable, scalable, and future-ready..

 

Close‑up view of high‑performance server hardware with blue and purple LED indicators

THE ROAD AHEAD

The move to 800V for hyperscale data centers is not a matter of "if," but "when." The choices we make today regarding data center infrastructure will shape our capacity for future innovation. Those who lead the transition will gain a crucial advantage, enabling them to expand their AI efforts more rapidly and efficiently than their competitors.

Nonetheless, for many, 48V will remain a cornerstone for many applications. Supporting both architectures—and embedding intelligence, safety, and modularity into power delivery—is key to meeting the industry’s evolving demands and our future.

References

1 Sean Graham. “Date Center Vision: How Datacenter Infrastructure will evolve to Support AI and Accelerated Compute”. IDC Research Inc. March 2025