Meeting the Power Challenges of General Lighting Applications

Jan 22 2020

Figure 1

   

Abstract

The proliferation of LED drivers in general lighting applications places new requirements on system hardware, such as reduced component size to fit additional electronics in the same space, improved energy efficiency to perform within the same or lower thermal budget, connected and flexible architectures supporting multiple configurations, and accurate control that preserves LED light characteristics. Read full article.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Product Categories