MAX3983: Designing for 10Gbase-CX4 Transmitter Template Compliance with the MAX3983

Apr 23 2004

Figure 1

   

Abstract

The MAX3983 cable driver/receiver was optimized to achieve maximum cable span without the use of automatic/adaptive equalization techniques. After its release new copper cable interface standards were completed, the most stringent of which are found in the IEEE802.3's 10Gbase-CX4 transmitter output template. This discussion will aid in achieving CX4 compliance using the MAX3983. With the addition of a few passive components, the high performance MAX3983 can easily be adjusted to meet this tight template. Read full article.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products