MAX3610: MAX3610 Synthesizer-Based Crystal Oscillator Enables Low Cost, High-Performance Clock Sources

Mar 22 2004

Figure 1

   

Abstract

This design note describes the characteristics of the MAX3610 reference clock generator, and the methodology for measuring the power supply induced deterministic jitter using a spectrum analyzer. Measurement results are presented for the clock output single side band (SSB) phase noise and the power supply induced determininistic jitter. The crystal resonator parameter, and the measured frequency stability of the MAX3610 with a crystal are given in Section 4 of the document. Read full article.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article