LTspice: Parametric Plots

Aug 6 2013

Figure 1

   

Plotting results in LTspice is as easy as clicking on a node to show voltage, or a component to show current—the trace is then displayed in the waveform viewer. In transient analysis, the horizontal axis defaults to showing time, but you can always change the horizontal axis to show other quantities (such as current) to validate model parameters.

To change the default settings of the X-axis:

  1. Click on a node/component to plot its voltage/current in the waveform viewer.
  2. Move the cursor to the horizontal axis of the waveform viewer (the cursor will turn into a ruler) and right-click.
  3. In the Horizontal Axis dialog, enter an expression for the “Quantity Plotted.
  4. Click OK.

About the Authors

Gabino Alonso
Gabino Alonso is currently the director of strategic marketing for the Power by Linear™ Group. Prior to joining ADI, Gabino held various positions in marketing, engineering, operations, and education at Linear Technology, ...
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Resources

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project