HFAN-02.2.2: Optical Modulation Amplitude and Extinction Ratio

Sep 15 2003

Figure 1

   

Abstract

The purpose of this application note is to define optical modulation amplitude (OMA) and how it relates to other parameters such as extinction ratio and average power. Further, this application note will clarify the trade-offs between specifying OMA versus extinction ratio and explore appropriate specification ranges for each.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article