HFAN-02.0.1: Parasitic Inductance Effects in 10Gbps Fiber Optic Design

Feb 28 2002

Figure 1

   

Abstract

Successful 10Gbps optical module design demands careful attention to the sources and effects ofparasitic inductance. The addition of even 0.1nH of inductance can cause significant degradation to therise/fall times, overshoot/ringing, and jitter in the optical output (for reference, a 0.5mm bond wire addsapproximately 0.4nH).

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article