Chill Out Your Power Supply: Efficiency Through Better Cooling

Jun 5 2026

Figure 1

   

Question:

Could a smarter cooling strategy unlock your power supply’s untapped efficiency potential?

Answer:

Yes, because unmanaged heat quietly undermines efficiency, accelerates component aging, and limits power density. Smart cooling choices, made early in the design, can unlock higher performance, longer lifetime, and more robust power supplies.

Chill Out Your Power Supply: Efficiency Through Better Cooling

Introduction

Heat is one of the primary factors affecting the reliability of electronic systems. In power supplies, the backbone of modern electronics, thermal stress can significantly impact performance and system integrity. These circuits convert electrical energy into stable voltages for applications ranging from consumer devices to aerospace systems. As power density continues to rise with the demand for smaller and more capable designs, thermal management has become a critical design challenge.

Sources of heat include switching transients in power transistors, magnetic losses in inductive components, and leakage currents in semiconductors. If unmanaged, this thermal buildup can lead to degraded electrical performance, reduced mean time between failures (MTBF), and even catastrophic component failure. Effective cooling strategies are therefore essential to maintain efficiency and reliability under varying load and environmental conditions.

This article examines four proven cooling methods, each with distinct characteristics suited to different operational environments and design constraints. By understanding their technical trade-offs, engineers can make informed decisions that balance performance, reliability, cost, and complexity ensuring power supplies operate safely and efficiently.

Sources of Heat in Power Supplies

Heat comes from semiconductor devices like MOSFETs and diodes, which dissipate energy through conduction and switching losses. Magnetic components such as transformers and inductors generate heat due to copper losses in windings and core losses from hysteresis and eddy currents, while resistive elements and control circuitry add minor heat.

  1. MOSFET (switching transistor): generates heat due to conduction losses when current flows through its on-state resistance and switching losses during transitions between on and off states. These losses increase significantly at high frequencies and high currents, making MOSFETs one of the main contributors of heat in SMPS designs.

    Conduction loss:

    Equation 1.

    Where:

    • Irms: rms current through MOSFET
    • RDS(ON): drain-to-source on-state resistance

    Switching loss:

    Equation 2.

    Where:

    • Vds: drain-to-source voltage
    • Id: drain current
    • ton, toff: switching transition times
    • fsw: switching frequency
    • 0.5: assumes linear overlap of voltage and current during switching
  2. Diode (rectifier): generates heat mainly because of its forward voltage drop when current flows through it, causing energy to be dissipated as heat during conduction. In high-speed switching applications, additional losses occur during reverse recovery when stored charge is removed as the diode transitions from forward to reverse bias.

    Equation 3.

    Where:

    • Vf: forward voltage drops (0.7V for Si, 0.3V for Schottky)
    • Iavg: average current through diode
  3. Inductor/transformer: produces heat mainly from copper losses in its windings caused by resistive heating and core losses due to hysteresis and eddy currents in the magnetic material. Both losses grow with higher current, frequency, and flux density, requiring careful material and design choices.

    Copper loss:

    Equation 4.

    Where:

    • Irms: rms current in winding
    • Rwinding: DC resistance of winding

    Core loss (Steinmetz equation):

    Equation 5.

    Where:

    • k: Steinmetz coefficient (material specific)
    • f: frequency (Hz)
    • B: peak flux density (Tesla)
    • α β: Steinmetz exponents (typically α ≈ 1.3 – 1.6 β ≈ 2.0 – 2.8)
    • Vcore: core volume (cm3 or m3)
  4. Capacitors: generate heat through their equivalent series resistance (ESR), which dissipates energy when ripple currents flow through them. This effect is more pronounced in electrolytic capacitors with higher ESR, leading to localized heating in power supply filters.

    Equation 6.

    Where:

    • Iripple: ripple current through capacitor
    • ESR: equivalent series resistance
  5. An integrated circuit (IC): contributes heat to a system through its junction temperature, the temperature at the semiconductor die inside the package. Designers often calculate it using:

    Equation 7.

    Where:

    • Tj: junction temperature (°C)
    • Ta: ambient temperature (°C)
    • θja: thermal resistance from junction to ambient (°C/W)
    • Pd: power dissipation (W)

Higher current, voltage, and switching frequency increase both power losses and component temperatures, making thermal management critical to the design. Minimizing these losses requires careful component selection, optimized circuit design, and effective cooling strategies. Addressing heat generation not only improves efficiency but also ensures longevity of the power supply system.

Cooling Methods in Power Supplies

Natural Convection Cooling

This is a passive cooling method that relies on the buoyancy-driven movement of air. As electronic components heat up, the surrounding air becomes less dense and rises, while cooler air moves in to replace it. This creates continuous airflow around the heat-generating components without the need for mechanical assistance. Figure 1 illustrates how air moves with convection cooling.

Figure 1. Convection cooling in power supply.

The effectiveness of natural convection depends on several factors, including the orientation of the components, the geometry of the enclosure, and the ambient temperature. Heat sinks are commonly used to increase the surface area available for heat dissipation, and their design from fins, materials, and placement plays a critical role in optimizing thermal performance.

Advantages include silent operation, minimal maintenance, and high reliability due to the absence of moving parts. It is ideal for low-power applications or environments where noise and mechanical wear are concerns. Limitations include relatively low heat dissipation capacity and dependence on ambient airflow, which can be insufficient in high-power or densely packed systems.

Forced Air Cooling

A cooling method that enhances heat dissipation by actively moving air across components using fans or blowers. This increases the convective heat transfer coefficient, allowing more efficient removal of heat from surfaces such as heat sinks, transformers, and switching devices. Figure 2 shows how the air flows when using a fan in a power supply.

Figure 2. Forced air cooling in power supply.

From a design perspective, forced air cooling requires careful airflow management to avoid hot spots and ensure uniform cooling. Designers must consider fan placement, airflow direction, ducting, and acoustic noise suppression. Fan speed control and monitoring are also important to balance cooling performance with energy consumption and noise levels.

Pros include scalability for higher power levels, easy implementation, and compatibility with compact designs. Cons include mechanical wear and potential failure points, periodic maintenance, and noise generation. Forced air systems may also be less effective in dusty or humid environments where airflow can be obstructed or contaminated.

Conduction Cooling

The method involves transferring heat directly from components to a heat sink or chassis through physical contact. This method is particularly useful in sealed or rugged environments where airflow is restricted or where dust, moisture, or vibration makes fan-based cooling impractical. Figure 3 illustrates how to implement conduction cooling in a system.

Figure 3. Conduction cooling in power supply.

Thermal interface materials (TIMs) such as thermal pads, pastes, or phase-change materials are used to improve thermal conductivity between surfaces. The efficiency of conduction cooling depends on the thermal resistance of the path, the material properties (for example, copper vs. aluminum), and the surface area available for heat transfer.

Advantages include high reliability, suitability for harsh environments, and elimination of moving parts. Drawbacks include limited cooling capacity compared to active methods and the need for precise mechanical design to ensure effective thermal contact.

Liquid Cooling

A high-performance method uses a circulating coolant to absorb and transport heat away from components. The coolant flows through cold plates or heat exchangers attached to heat sources, and the absorbed heat is then dissipated via a radiator or external cooling system. Figure 4 illustrates a liquid cooling approach.

Figure 4. Liquid cooling method.

Technically, liquid cooling offers superior thermal conductivity and heat capacity compared to air. It enables efficient cooling of high-power components in compact spaces. However, it requires pumps, tubing, reservoirs, and leak-proof connections, making the system more complex and potentially more expensive. Benefits include excellent thermal performance, reduced noise, and suitability for high-density or high-power applications. Challenges include increased costs, potential for leaks, and the need for regular maintenance to ensure system integrity and coolant quality.

Thermal Design Best Practices

Effective thermal design requires a combination of electrical, mechanical, and environmental considerations. Below are key practices to ensure optimal thermal performance.

  • Thermal budgeting and power profiling: Begin with accurate power dissipation estimates for each component under worst-case conditions. Include switching losses, conduction losses, and magnetic losses. Use simulation tools and data sheet values to calculate junction temperatures and ensure thermal margins.
  • PCB layout optimization: Use wide copper planes and thermal vias to spread heat. Figure 5 illustrates how vias can be used to spread heat. Place high-power components near heat sinks or thermal paths. Avoid placing heat-sensitive components near heat sources. Consider multilayer boards with internal heat spreading layers.
    Figure 5. Heat spreading into PCB with and without thermal vias.
  • Heat sink selection and mounting: Choose heat sinks based on thermal resistance, airflow compatibility, and mounting constraints. Consider fin geometry, orientation, and surface treatment (for example, anodizing) to enhance heat dissipation.
  • Airflow management: Design airflow paths to be smooth and laminar. Avoid sharp turns, obstructions, or recirculation zones. Use computational fluid dynamics (CFD) tools to simulate airflow and optimize ducting. Ensure intake and exhaust vents are properly sized and positioned.
  • Active cooling control: Implement dynamic fan control using temperature feedback. Use pulse-width modulation (PWM) or voltage control to adjust fan speed based on thermal load. Include fault detection for fan failure and thermal alarms for overtemperature conditions.
  • Environmental considerations: Account for ambient temperature, altitude (affects air density), humidity, and contamination. Use conformal coatings or sealed enclosures in harsh environments. Consider derating components for high-altitude or high-temperature operation.

Common Pitfalls in Thermal Design

Thermal design errors are often subtle but can significantly impact system reliability and performance. One of the most common mistakes is underestimating heat generation, especially under peak load or worst-case environmental conditions. Designers may rely on typical operating values and overlook transient spikes or cumulative heat buildup, leading to thermal overload. Another frequent issue is improper application of TIMs. Uneven or excessive applications can trap air, increase thermal resistance, and reduce the effectiveness of conduction cooling. Similarly, inadequate airflow planning, such as poor fan placement or obstructed vents, can result in recirculation zones and hot spots, compromising forced air cooling efficiency.

Component placement also plays a critical role in thermal behavior. Placing heat-sensitive components too close to high-power devices can expose them to excessive heat, affecting performance or causing premature failure. Long-term reliability is often neglected; fans degrade, TIMs dry out, and dust accumulation can block airflow, all of which reduce cooling effectiveness over time. Skipping thermal simulation and real-world testing is another pitfall, and relying solely on data sheet values or theoretical models can lead to inaccurate predictions. Finally, misjudging environmental factors such as altitude, humidity, or enclosure sealing can result in unexpected thermal challenges. Addressing these pitfalls early in the design process helps ensure robust power supply design.

ADI Controllers for Thermal Management

Analog Devices offers a robust portfolio of thermal management solutions tailored for different power supplies or systems across a wide range of cooling methods. These controllers and integrated circuits provide precise control over temperature regulation, fan operation, and thermoelectric cooling, enabling engineers to design systems that are both efficient and reliable.

Intelligent Fan Controller

The MAX31785 is a six-channel intelligent fan controller designed for high-density systems such as servers, telecom equipment, and industrial power supplies. It supports PWM control and closed-loop RPM control, enabling precise regulation of fan speed based on real-time temperature feedback. With six independent PWM outputs, it can control multiple fans simultaneously, while its I2C/SMBus interface allows seamless communication with host systems. The device can support up to 12 tachometer inputs—two per fan—which is considered a sophisticated and highly desirable feature in modern systems. Figure 6 shows the evaluation board of the MAX31785 with a fan attached for testing.

Figure 6. The MAX31785 evaluation kit.

The controller monitors temperature via up to six remote thermal diodes and one internal temperature sensor and includes fault detection and alert generation for fan failures or thermal anomalies. Its flexible fan speed profiles help optimize both acoustic performance and thermal efficiency, making it ideal for forced air cooling systems where dynamic airflow control is essential to maintain system reliability and minimize noise.

TEC Controller for Precision Cooling

The ADN8834 is a patented high-efficiency single inductor thermoelectric cooler (TEC) controller optimized for precision temperature control in conduction-cooled systems such as optical modules and laser diodes. The single inductor stands out as a space-saving and cost-effective solution, especially when compared to conventional designs that require two inductors. It integrates a buck controller capable of driving TECs with up to 1.5A current and includes a built-in proportional integral differential (PID) control loop for accurate thermal regulation. It also supports temperature monitoring using thermistors or diode sensors and operates with low noise, making it suitable for sensitive analog systems. Its compact footprint and programmable PID parameters allow for fine-tuned thermal response in space-constrained designs. Figure 7 illustrates how the controller is integrated into the TEC system.

Figure 7. TEC system.

Thermal Simulation Tools

Simulation tools are vital for predicting heat flow, optimizing cooling strategies, and validating designs before prototyping. Ansys Icepak offers advanced CFD modeling for airflow and heat transfer, ideal for high-density electronics. COMSOL Multiphysics® enables coupled physics simulations, making it suitable for systems where thermal behavior interacts with electrical or mechanical domains. SolidWorks Flow Simulation integrates directly with computer-aided design (CAD), allowing quick thermal analysis of enclosures and mechanical assemblies. Mentor Graphics® FloTHERM™ specializes in PCB and system-level thermal modeling, widely used in telecom and aerospace. These tools help engineers identify thermal bottlenecks early, reduce design iterations, and ensure compliance with reliability standards.

Conclusion

Effective cooling is essential for the safe and efficient operation of power supplies. Each cooling method from natural convection, forced air, conduction, and liquid cooling offers unique advantages and trade-offs. Natural convection is simple and silent but limited in capacity. Forced air cooling is scalable and effective but introduces mechanical complexity. Conduction cooling is rugged and reliable, ideal for sealed environments, while liquid cooling delivers unmatched performance for high-power applications at the cost of system complexity.

By understanding the technical principles and limitations, applying thermal design best practices, avoiding common pitfalls, and leveraging simulation tools, engineers can make informed decisions tailored to their application requirements. ADI supports these efforts with a comprehensive portfolio of thermal management controllers, enabling precise and reliable cooling across a wide range of system applications.

About the Authors

Hermogenes Escala
Hermogenes Escala is an applications engineer at Analog Devices, Inc., supporting the EMEA Central Applications Center (CAC). With a strong focus on switch-mode power supplies (SMPS) and power management, Hermo brings a
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Product Categories