A Five-Channel (Three +V and Two -V) Hot-Swap Reference Design

Mar 31 2023

Figure 1

   

This five-channel circuit provides hot-swap functions for three positive-voltage circuits and for two negative-voltage circuits, though it employs only a single MAX5927A four-channel hot-swap controller. The Figure 1 circuit meets the following load and power-sequencing requirements:

  • Ch1 = +3.3V at 2A (circuit breaker at ≥ 3A)
  • Ch2 = +5V at 1.6A (circuit breaker at ≥ 2.4A)
  • Ch3 = +12V at 2A (circuit breaker at ≥ 3A)
  • Ch4 = -12V at 150mA (no circuit-breaker action)
  • Ch5 = -5V at 50mA (no circuit-breaker action)
  • Startup timing is such that channels 2 (+5V) and 3 (+12V) begin to turn on as soon as active-low CARD_PRESENT goes low. STAT2 and STAT3 go active-high 10.8ms after active-low CARD_PRESENT goes low.
  • Channel 1 (+3.3V) turn-on is delayed by 11.8ms from channels 2 and 3. STAT1 goes high 10.8ms after channel 1 begins to turn on.
  • Turn-on of channels 4 (-12V) and 5 (-5V) is delayed by 27.8ms from channels 2 and 3. STAT4 goes high 10.8ms after channels 4 and 5 begin to turn on.
  • Latching fault management. If any of channels 1 through 3 experiences a fault, all channels will

Figure 1. This five-channel hot-swap circuit controls three positive-voltage and two negative-voltage channels

Figure 1. This five-channel hot-swap circuit controls three positive-voltage and two negative-voltage channels

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Resources


Video
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project